summaryrefslogtreecommitdiffstats
blob: 0f1f85e22dbb54c1322b4e4f68780dcd92995947 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
/*
 * Copyright (C) 2013 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef _LIBMEMTRACK_MEMTRACK_H_
#define _LIBMEMTRACK_MEMTRACK_H_

#include <sys/types.h>
#include <stddef.h>
#include <cutils/compiler.h>

#ifdef __cplusplus
extern "C" {
#endif

/**
 * struct memtrack_proc
 *
 * an opaque handle to the memory stats on a process.
 * Created with memtrack_proc_new, destroyed by
 * memtrack_proc_destroy.  Can be reused multiple times with
 * memtrack_proc_get.
 */
struct memtrack_proc;

/**
 * memtrack_init
 *
 * Must be called once before calling any other functions.  After this function
 * is called, everything else is thread-safe.
 *
 * Returns 0 on success, -errno on error.
 */
int memtrack_init(void);

/**
 * memtrack_proc_new
 *
 * Return a new handle to hold process memory stats.
 *
 * Returns NULL on error.
 */
struct memtrack_proc *memtrack_proc_new(void);

/**
 * memtrack_proc_destroy
 *
 * Free all memory associated with a process memory stats handle.
 */
void memtrack_proc_destroy(struct memtrack_proc *p);

/**
 * memtrack_proc_get
 *
 * Fill a process memory stats handle with data about the given pid.  Can be
 * called on a handle that was just allocated with memtrack_proc_new,
 * or on a handle that has been previously passed to memtrack_proc_get
 * to replace the data with new data on the same or another process.  It is
 * expected that the second call on the same handle should not require
 * allocating any new memory.
 *
 * Returns 0 on success, -errno on error.
 */
int memtrack_proc_get(struct memtrack_proc *p, pid_t pid);

/**
 * memtrack_proc_graphics_total
 *
 * Return total amount of memory that has been allocated for use as window
 * buffers.  Does not differentiate between memory that has already been
 * accounted for by reading /proc/pid/smaps and memory that has not been
 * accounted for.
 *
 * Returns non-negative size in bytes on success, -errno on error.
 */
ssize_t memtrack_proc_graphics_total(struct memtrack_proc *p);

/**
 * memtrack_proc_graphics_pss
 *
 * Return total amount of memory that has been allocated for use as window
 * buffers, but has not already been accounted for by reading /proc/pid/smaps.
 * Memory that is shared across processes may already be divided by the
 * number of processes that share it (preferred), or may be charged in full to
 * every process that shares it, depending on the capabilities of the driver.
 *
 * Returns non-negative size in bytes on success, -errno on error.
 */
ssize_t memtrack_proc_graphics_pss(struct memtrack_proc *p);

/**
 * memtrack_proc_gl_total
 *
 * Same as memtrack_proc_graphics_total, but counts GL memory (which
 * should not overlap with graphics memory) instead of graphics memory.
 *
 * Returns non-negative size in bytes on success, -errno on error.
 */
ssize_t memtrack_proc_gl_total(struct memtrack_proc *p);

/**
 * memtrack_proc_gl_pss
 *
 * Same as memtrack_proc_graphics_total, but counts GL memory (which
 * should not overlap with graphics memory) instead of graphics memory.
 *
 * Returns non-negative size in bytes on success, -errno on error.
 */
ssize_t memtrack_proc_gl_pss(struct memtrack_proc *p);

/**
 * memtrack_proc_gl_total
 *
 * Same as memtrack_proc_graphics_total, but counts miscellaneous memory
 * not tracked by gl or graphics calls above.
 *
 * Returns non-negative size in bytes on success, -errno on error.
 */
ssize_t memtrack_proc_other_total(struct memtrack_proc *p);

/**
 * memtrack_proc_gl_pss
 *
 * Same as memtrack_proc_graphics_total, but counts miscellaneous memory
 * not tracked by gl or graphics calls above.
 *
 * Returns non-negative size in bytes on success, -errno on error.
 */
ssize_t memtrack_proc_other_pss(struct memtrack_proc *p);

#ifdef __cplusplus
}
#endif

#endif