summaryrefslogtreecommitdiffstats
blob: 5d0873ac42a6d847a6aeb86094e55fed3de06aec (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
/*
 * Copyright (C) 2011 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef SYSTEM_CORE_INCLUDE_ANDROID_CAMERA_H
#define SYSTEM_CORE_INCLUDE_ANDROID_CAMERA_H

#include <stdint.h>
#include <sys/cdefs.h>
#include <sys/types.h>
#include <cutils/native_handle.h>
#include <hardware/hardware.h>
#include <hardware/gralloc.h>

__BEGIN_DECLS

/**
 * A set of bit masks for specifying how the received preview frames are
 * handled before the previewCallback() call.
 *
 * The least significant 3 bits of an "int" value are used for this purpose:
 *
 * ..... 0 0 0
 *       ^ ^ ^
 *       | | |---------> determine whether the callback is enabled or not
 *       | |-----------> determine whether the callback is one-shot or not
 *       |-------------> determine whether the frame is copied out or not
 *
 * WARNING: When a frame is sent directly without copying, it is the frame
 * receiver's responsiblity to make sure that the frame data won't get
 * corrupted by subsequent preview frames filled by the camera. This flag is
 * recommended only when copying out data brings significant performance price
 * and the handling/processing of the received frame data is always faster than
 * the preview frame rate so that data corruption won't occur.
 *
 * For instance,
 * 1. 0x00 disables the callback. In this case, copy out and one shot bits
 *    are ignored.
 * 2. 0x01 enables a callback without copying out the received frames. A
 *    typical use case is the Camcorder application to avoid making costly
 *    frame copies.
 * 3. 0x05 is enabling a callback with frame copied out repeatedly. A typical
 *    use case is the Camera application.
 * 4. 0x07 is enabling a callback with frame copied out only once. A typical
 *    use case is the Barcode scanner application.
 */

enum {
    CAMERA_FRAME_CALLBACK_FLAG_ENABLE_MASK = 0x01,
    CAMERA_FRAME_CALLBACK_FLAG_ONE_SHOT_MASK = 0x02,
    CAMERA_FRAME_CALLBACK_FLAG_COPY_OUT_MASK = 0x04,
    /** Typical use cases */
    CAMERA_FRAME_CALLBACK_FLAG_NOOP = 0x00,
    CAMERA_FRAME_CALLBACK_FLAG_CAMCORDER = 0x01,
    CAMERA_FRAME_CALLBACK_FLAG_CAMERA = 0x05,
    CAMERA_FRAME_CALLBACK_FLAG_BARCODE_SCANNER = 0x07
};

/** msgType in notifyCallback and dataCallback functions */
enum {
    CAMERA_MSG_ERROR = 0x0001,            // notifyCallback
    CAMERA_MSG_SHUTTER = 0x0002,          // notifyCallback
    CAMERA_MSG_FOCUS = 0x0004,            // notifyCallback
    CAMERA_MSG_ZOOM = 0x0008,             // notifyCallback
    CAMERA_MSG_PREVIEW_FRAME = 0x0010,    // dataCallback
    CAMERA_MSG_VIDEO_FRAME = 0x0020,      // data_timestamp_callback
    CAMERA_MSG_POSTVIEW_FRAME = 0x0040,   // dataCallback
    CAMERA_MSG_RAW_IMAGE = 0x0080,        // dataCallback
    CAMERA_MSG_COMPRESSED_IMAGE = 0x0100, // dataCallback
    CAMERA_MSG_RAW_IMAGE_NOTIFY = 0x0200, // dataCallback
    // Preview frame metadata. This can be combined with
    // CAMERA_MSG_PREVIEW_FRAME in dataCallback. For example, the apps can
    // request FRAME and METADATA. Or the apps can request only FRAME or only
    // METADATA.
    CAMERA_MSG_PREVIEW_METADATA = 0x0400, // dataCallback
    // Notify on autofocus start and stop. This is useful in continuous
    // autofocus - FOCUS_MODE_CONTINUOUS_VIDEO and FOCUS_MODE_CONTINUOUS_PICTURE.
    CAMERA_MSG_FOCUS_MOVE = 0x0800,       // notifyCallback
    CAMERA_MSG_ALL_MSGS = 0xFFFF
};

/** cmdType in sendCommand functions */
enum {
    CAMERA_CMD_START_SMOOTH_ZOOM = 1,
    CAMERA_CMD_STOP_SMOOTH_ZOOM = 2,

    /**
     * Set the clockwise rotation of preview display (setPreviewDisplay) in
     * degrees. This affects the preview frames and the picture displayed after
     * snapshot. This method is useful for portrait mode applications. Note
     * that preview display of front-facing cameras is flipped horizontally
     * before the rotation, that is, the image is reflected along the central
     * vertical axis of the camera sensor. So the users can see themselves as
     * looking into a mirror.
     *
     * This does not affect the order of byte array of
     * CAMERA_MSG_PREVIEW_FRAME, CAMERA_MSG_VIDEO_FRAME,
     * CAMERA_MSG_POSTVIEW_FRAME, CAMERA_MSG_RAW_IMAGE, or
     * CAMERA_MSG_COMPRESSED_IMAGE. This is allowed to be set during preview
     * since API level 14.
     */
    CAMERA_CMD_SET_DISPLAY_ORIENTATION = 3,

    /**
     * cmdType to disable/enable shutter sound. In sendCommand passing arg1 =
     * 0 will disable, while passing arg1 = 1 will enable the shutter sound.
     */
    CAMERA_CMD_ENABLE_SHUTTER_SOUND = 4,

    /* cmdType to play recording sound */
    CAMERA_CMD_PLAY_RECORDING_SOUND = 5,

    /**
     * Start the face detection. This should be called after preview is started.
     * The camera will notify the listener of CAMERA_MSG_FACE and the detected
     * faces in the preview frame. The detected faces may be the same as the
     * previous ones. Apps should call CAMERA_CMD_STOP_FACE_DETECTION to stop
     * the face detection. This method is supported if CameraParameters
     * KEY_MAX_NUM_HW_DETECTED_FACES or KEY_MAX_NUM_SW_DETECTED_FACES is
     * bigger than 0. Hardware and software face detection should not be running
     * at the same time. If the face detection has started, apps should not send
     * this again.
     *
     * In hardware face detection mode, CameraParameters KEY_WHITE_BALANCE,
     * KEY_FOCUS_AREAS and KEY_METERING_AREAS have no effect.
     *
     * arg1 is the face detection type. It can be CAMERA_FACE_DETECTION_HW or
     * CAMERA_FACE_DETECTION_SW. If the type of face detection requested is not
     * supported, the HAL must return BAD_VALUE.
     */
    CAMERA_CMD_START_FACE_DETECTION = 6,

    /**
     * Stop the face detection.
     */
    CAMERA_CMD_STOP_FACE_DETECTION = 7,

    /**
     * Enable/disable focus move callback (CAMERA_MSG_FOCUS_MOVE). Passing
     * arg1 = 0 will disable, while passing arg1 = 1 will enable the callback.
     */
    CAMERA_CMD_ENABLE_FOCUS_MOVE_MSG = 8,

    /**
     * Ping camera service to see if camera hardware is released.
     *
     * When any camera method returns error, the client can use ping command
     * to see if the camera has been taken away by other clients. If the result
     * is NO_ERROR, it means the camera hardware is not released. If the result
     * is not NO_ERROR, the camera has been released and the existing client
     * can silently finish itself or show a dialog.
     */
    CAMERA_CMD_PING = 9,

    /**
     * Configure the number of video buffers used for recording. The intended
     * video buffer count for recording is passed as arg1, which must be
     * greater than 0. This command must be sent before recording is started.
     * This command returns INVALID_OPERATION error if it is sent after video
     * recording is started, or the command is not supported at all. This
     * command also returns a BAD_VALUE error if the intended video buffer
     * count is non-positive or too big to be realized.
     */
    CAMERA_CMD_SET_VIDEO_BUFFER_COUNT = 10,

    /**
     * Configure an explicit format to use for video recording metadata mode.
     * This can be used to switch the format from the
     * default IMPLEMENTATION_DEFINED gralloc format to some other
     * device-supported format, and the default dataspace from the BT_709 color
     * space to some other device-supported dataspace. arg1 is the HAL pixel
     * format, and arg2 is the HAL dataSpace. This command returns
     * INVALID_OPERATION error if it is sent after video recording is started,
     * or the command is not supported at all.
     *
     * If the gralloc format is set to a format other than
     * IMPLEMENTATION_DEFINED, then HALv3 devices will use gralloc usage flags
     * of SW_READ_OFTEN.
     */
    CAMERA_CMD_SET_VIDEO_FORMAT = 11
};

/** camera fatal errors */
enum {
    CAMERA_ERROR_UNKNOWN = 1,
    /**
     * Camera was released because another client has connected to the camera.
     * The original client should call Camera::disconnect immediately after
     * getting this notification. Otherwise, the camera will be released by
     * camera service in a short time. The client should not call any method
     * (except disconnect and sending CAMERA_CMD_PING) after getting this.
     */
    CAMERA_ERROR_RELEASED = 2,
    CAMERA_ERROR_SERVER_DIED = 100
};

enum {
    /** The facing of the camera is opposite to that of the screen. */
    CAMERA_FACING_BACK = 0,
    /** The facing of the camera is the same as that of the screen. */
    CAMERA_FACING_FRONT = 1,
    /**
     * The facing of the camera is not fixed relative to the screen.
     * The cameras with this facing are external cameras, e.g. USB cameras.
     */
    CAMERA_FACING_EXTERNAL = 2
};

enum {
    /** Hardware face detection. It does not use much CPU. */
    CAMERA_FACE_DETECTION_HW = 0,
    /**
     * Software face detection. It uses some CPU. Applications must use
     * Camera.setPreviewTexture for preview in this mode.
     */
    CAMERA_FACE_DETECTION_SW = 1
};

/**
 * The information of a face from camera face detection.
 */
typedef struct camera_face {
    /**
     * Bounds of the face [left, top, right, bottom]. (-1000, -1000) represents
     * the top-left of the camera field of view, and (1000, 1000) represents the
     * bottom-right of the field of view. The width and height cannot be 0 or
     * negative. This is supported by both hardware and software face detection.
     *
     * The direction is relative to the sensor orientation, that is, what the
     * sensor sees. The direction is not affected by the rotation or mirroring
     * of CAMERA_CMD_SET_DISPLAY_ORIENTATION.
     */
    int32_t rect[4];

    /**
     * The confidence level of the face. The range is 1 to 100. 100 is the
     * highest confidence. This is supported by both hardware and software
     * face detection.
     */
    int32_t score;

    /**
     * An unique id per face while the face is visible to the tracker. If
     * the face leaves the field-of-view and comes back, it will get a new
     * id. If the value is 0, id is not supported.
     */
    int32_t id;

    /**
     * The coordinates of the center of the left eye. The range is -1000 to
     * 1000. -2000, -2000 if this is not supported.
     */
    int32_t left_eye[2];

    /**
     * The coordinates of the center of the right eye. The range is -1000 to
     * 1000. -2000, -2000 if this is not supported.
     */
    int32_t right_eye[2];

    /**
     * The coordinates of the center of the mouth. The range is -1000 to 1000.
     * -2000, -2000 if this is not supported.
     */
    int32_t mouth[2];

} camera_face_t;

/**
 * The metadata of the frame data.
 */
typedef struct camera_frame_metadata {
    /**
     * The number of detected faces in the frame.
     */
    int32_t number_of_faces;

    /**
     * An array of the detected faces. The length is number_of_faces.
     */
    camera_face_t *faces;
} camera_frame_metadata_t;

__END_DECLS

#endif /* SYSTEM_CORE_INCLUDE_ANDROID_CAMERA_H */