summaryrefslogtreecommitdiffstats
blob: be86ae42b1ad1fedf5363407bbaec27a39035ae6 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
/*
 * Copyright (C) 2011 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef SYSTEM_CORE_INCLUDE_ANDROID_GRAPHICS_H
#define SYSTEM_CORE_INCLUDE_ANDROID_GRAPHICS_H

#include <stdint.h>

#ifdef __cplusplus
extern "C" {
#endif

/*
 * If the HAL needs to create service threads to handle graphics related
 * tasks, these threads need to run at HAL_PRIORITY_URGENT_DISPLAY priority
 * if they can block the main rendering thread in any way.
 *
 * the priority of the current thread can be set with:
 *
 *      #include <sys/resource.h>
 *      setpriority(PRIO_PROCESS, 0, HAL_PRIORITY_URGENT_DISPLAY);
 *
 */

#define HAL_PRIORITY_URGENT_DISPLAY     (-8)

/**
 * pixel format definitions
 */

enum {
    /*
     * "linear" color pixel formats:
     *
     * The pixel formats below contain sRGB data but are otherwise treated
     * as linear formats, i.e.: no special operation is performed when
     * reading or writing into a buffer in one of these formats
     */
    HAL_PIXEL_FORMAT_RGBA_8888          = 1,
    HAL_PIXEL_FORMAT_RGBX_8888          = 2,
    HAL_PIXEL_FORMAT_RGB_888            = 3,
    HAL_PIXEL_FORMAT_RGB_565            = 4,
    HAL_PIXEL_FORMAT_BGRA_8888          = 5,

    /*
     * sRGB color pixel formats:
     *
     * The red, green and blue components are stored in sRGB space, and converted
     * to linear space when read, using the standard sRGB to linear equation:
     *
     * Clinear = Csrgb / 12.92                  for Csrgb <= 0.04045
     *         = (Csrgb + 0.055 / 1.055)^2.4    for Csrgb >  0.04045
     *
     * When written the inverse transformation is performed:
     *
     * Csrgb = 12.92 * Clinear                  for Clinear <= 0.0031308
     *       = 1.055 * Clinear^(1/2.4) - 0.055  for Clinear >  0.0031308
     *
     *
     *  The alpha component, if present, is always stored in linear space and
     *  is left unmodified when read or written.
     *
     */
    HAL_PIXEL_FORMAT_sRGB_A_8888        = 0xC,
    HAL_PIXEL_FORMAT_sRGB_X_8888        = 0xD,

    /*
     * 0x100 - 0x1FF
     *
     * This range is reserved for pixel formats that are specific to the HAL
     * implementation.  Implementations can use any value in this range to
     * communicate video pixel formats between their HAL modules.  These formats
     * must not have an alpha channel.  Additionally, an EGLimage created from a
     * gralloc buffer of one of these formats must be supported for use with the
     * GL_OES_EGL_image_external OpenGL ES extension.
     */

    /*
     * Android YUV format:
     *
     * This format is exposed outside of the HAL to software decoders and
     * applications.  EGLImageKHR must support it in conjunction with the
     * OES_EGL_image_external extension.
     *
     * YV12 is a 4:2:0 YCrCb planar format comprised of a WxH Y plane followed
     * by (W/2) x (H/2) Cr and Cb planes.
     *
     * This format assumes
     * - an even width
     * - an even height
     * - a horizontal stride multiple of 16 pixels
     * - a vertical stride equal to the height
     *
     *   y_size = stride * height
     *   c_stride = ALIGN(stride/2, 16)
     *   c_size = c_stride * height/2
     *   size = y_size + c_size * 2
     *   cr_offset = y_size
     *   cb_offset = y_size + c_size
     *
     */
    HAL_PIXEL_FORMAT_YV12   = 0x32315659, // YCrCb 4:2:0 Planar


    /*
     * Android Y8 format:
     *
     * This format is exposed outside of the HAL to the framework.
     * The expected gralloc usage flags are SW_* and HW_CAMERA_*,
     * and no other HW_ flags will be used.
     *
     * Y8 is a YUV planar format comprised of a WxH Y plane,
     * with each pixel being represented by 8 bits.
     *
     * It is equivalent to just the Y plane from YV12.
     *
     * This format assumes
     * - an even width
     * - an even height
     * - a horizontal stride multiple of 16 pixels
     * - a vertical stride equal to the height
     *
     *   size = stride * height
     *
     */
    HAL_PIXEL_FORMAT_Y8     = 0x20203859,

    /*
     * Android Y16 format:
     *
     * This format is exposed outside of the HAL to the framework.
     * The expected gralloc usage flags are SW_* and HW_CAMERA_*,
     * and no other HW_ flags will be used.
     *
     * Y16 is a YUV planar format comprised of a WxH Y plane,
     * with each pixel being represented by 16 bits.
     *
     * It is just like Y8, but has double the bits per pixel (little endian).
     *
     * This format assumes
     * - an even width
     * - an even height
     * - a horizontal stride multiple of 16 pixels
     * - a vertical stride equal to the height
     * - strides are specified in pixels, not in bytes
     *
     *   size = stride * height * 2
     *
     */
    HAL_PIXEL_FORMAT_Y16    = 0x20363159,

    /*
     * Android RAW sensor format:
     *
     * This format is exposed outside of the HAL to applications.
     *
     * RAW_SENSOR is a single-channel 16-bit format, typically representing raw
     * Bayer-pattern images from an image sensor, with minimal processing.
     *
     * The exact pixel layout of the data in the buffer is sensor-dependent, and
     * needs to be queried from the camera device.
     *
     * Generally, not all 16 bits are used; more common values are 10 or 12
     * bits. All parameters to interpret the raw data (black and white points,
     * color space, etc) must be queried from the camera device.
     *
     * This format assumes
     * - an even width
     * - an even height
     * - a horizontal stride multiple of 16 pixels (32 bytes).
     */
    HAL_PIXEL_FORMAT_RAW_SENSOR = 0x20,

    /*
     * Android binary blob graphics buffer format:
     *
     * This format is used to carry task-specific data which does not have a
     * standard image structure. The details of the format are left to the two
     * endpoints.
     *
     * A typical use case is for transporting JPEG-compressed images from the
     * Camera HAL to the framework or to applications.
     *
     * Buffers of this format must have a height of 1, and width equal to their
     * size in bytes.
     */
    HAL_PIXEL_FORMAT_BLOB = 0x21,

    /*
     * Android format indicating that the choice of format is entirely up to the
     * device-specific Gralloc implementation.
     *
     * The Gralloc implementation should examine the usage bits passed in when
     * allocating a buffer with this format, and it should derive the pixel
     * format from those usage flags.  This format will never be used with any
     * of the GRALLOC_USAGE_SW_* usage flags.
     *
     * If a buffer of this format is to be used as an OpenGL ES texture, the
     * framework will assume that sampling the texture will always return an
     * alpha value of 1.0 (i.e. the buffer contains only opaque pixel values).
     *
     */
    HAL_PIXEL_FORMAT_IMPLEMENTATION_DEFINED = 0x22,

    /*
     * Android flexible YCbCr formats
     *
     * This format allows platforms to use an efficient YCbCr/YCrCb buffer
     * layout, while still describing the buffer layout in a way accessible to
     * the CPU in a device-independent manner.  While called YCbCr, it can be
     * used to describe formats with either chromatic ordering, as well as
     * whole planar or semiplanar layouts.
     *
     * struct android_ycbcr (below) is the the struct used to describe it.
     *
     * This format must be accepted by the gralloc module when
     * USAGE_HW_CAMERA_WRITE and USAGE_SW_READ_* are set.
     *
     * This format is locked for use by gralloc's (*lock_ycbcr) method, and
     * locking with the (*lock) method will return an error.
     */
    HAL_PIXEL_FORMAT_YCbCr_420_888 = 0x23,

    /* Legacy formats (deprecated), used by ImageFormat.java */
    HAL_PIXEL_FORMAT_YCbCr_422_SP       = 0x10, // NV16
    HAL_PIXEL_FORMAT_YCrCb_420_SP       = 0x11, // NV21
    HAL_PIXEL_FORMAT_YCbCr_422_I        = 0x14, // YUY2
};

/*
 * Structure for describing YCbCr formats for consumption by applications.
 * This is used with HAL_PIXEL_FORMAT_YCbCr_*_888.
 *
 * Buffer chroma subsampling is defined in the format.
 * e.g. HAL_PIXEL_FORMAT_YCbCr_420_888 has subsampling 4:2:0.
 *
 * Buffers must have a 8 bit depth.
 *
 * @y, @cb, and @cr point to the first byte of their respective planes.
 *
 * Stride describes the distance in bytes from the first value of one row of
 * the image to the first value of the next row.  It includes the width of the
 * image plus padding.
 * @ystride is the stride of the luma plane.
 * @cstride is the stride of the chroma planes.
 *
 * @chroma_step is the distance in bytes from one chroma pixel value to the
 * next.  This is 2 bytes for semiplanar (because chroma values are interleaved
 * and each chroma value is one byte) and 1 for planar.
 */

struct android_ycbcr {
    void *y;
    void *cb;
    void *cr;
    size_t ystride;
    size_t cstride;
    size_t chroma_step;

    /** reserved for future use, set to 0 by gralloc's (*lock_ycbcr)() */
    uint32_t reserved[8];
};

/**
 * Transformation definitions
 *
 * IMPORTANT NOTE:
 * HAL_TRANSFORM_ROT_90 is applied CLOCKWISE and AFTER HAL_TRANSFORM_FLIP_{H|V}.
 *
 */

enum {
    /* flip source image horizontally (around the vertical axis) */
    HAL_TRANSFORM_FLIP_H    = 0x01,
    /* flip source image vertically (around the horizontal axis)*/
    HAL_TRANSFORM_FLIP_V    = 0x02,
    /* rotate source image 90 degrees clockwise */
    HAL_TRANSFORM_ROT_90    = 0x04,
    /* rotate source image 180 degrees */
    HAL_TRANSFORM_ROT_180   = 0x03,
    /* rotate source image 270 degrees clockwise */
    HAL_TRANSFORM_ROT_270   = 0x07,
    /* don't use. see system/window.h */
    HAL_TRANSFORM_RESERVED  = 0x08,
};

#ifdef __cplusplus
}
#endif

#endif /* SYSTEM_CORE_INCLUDE_ANDROID_GRAPHICS_H */