1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
591
592
593
594
595
596
597
598
599
600
601
602
603
604
605
606
607
608
609
610
611
612
613
614
|
/*
* Copyright (C) 2011 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef SYSTEM_CORE_INCLUDE_ANDROID_WINDOW_H
#define SYSTEM_CORE_INCLUDE_ANDROID_WINDOW_H
#include <stdint.h>
#include <sys/cdefs.h>
#include <system/graphics.h>
#include <cutils/native_handle.h>
__BEGIN_DECLS
/*****************************************************************************/
#define ANDROID_NATIVE_MAKE_CONSTANT(a,b,c,d) \
(((unsigned)(a)<<24)|((unsigned)(b)<<16)|((unsigned)(c)<<8)|(unsigned)(d))
#define ANDROID_NATIVE_WINDOW_MAGIC \
ANDROID_NATIVE_MAKE_CONSTANT('_','w','n','d')
#define ANDROID_NATIVE_BUFFER_MAGIC \
ANDROID_NATIVE_MAKE_CONSTANT('_','b','f','r')
// ---------------------------------------------------------------------------
typedef const native_handle_t* buffer_handle_t;
// ---------------------------------------------------------------------------
typedef struct android_native_rect_t
{
int32_t left;
int32_t top;
int32_t right;
int32_t bottom;
} android_native_rect_t;
// ---------------------------------------------------------------------------
typedef struct android_native_base_t
{
/* a magic value defined by the actual EGL native type */
int magic;
/* the sizeof() of the actual EGL native type */
int version;
void* reserved[4];
/* reference-counting interface */
void (*incRef)(struct android_native_base_t* base);
void (*decRef)(struct android_native_base_t* base);
} android_native_base_t;
typedef struct ANativeWindowBuffer
{
#ifdef __cplusplus
ANativeWindowBuffer() {
common.magic = ANDROID_NATIVE_BUFFER_MAGIC;
common.version = sizeof(ANativeWindowBuffer);
memset(common.reserved, 0, sizeof(common.reserved));
}
// Implement the methods that sp<ANativeWindowBuffer> expects so that it
// can be used to automatically refcount ANativeWindowBuffer's.
void incStrong(const void* id) const {
common.incRef(const_cast<android_native_base_t*>(&common));
}
void decStrong(const void* id) const {
common.decRef(const_cast<android_native_base_t*>(&common));
}
#endif
struct android_native_base_t common;
int width;
int height;
int stride;
int format;
int usage;
void* reserved[2];
buffer_handle_t handle;
void* reserved_proc[8];
} ANativeWindowBuffer_t;
// Old typedef for backwards compatibility.
typedef ANativeWindowBuffer_t android_native_buffer_t;
// ---------------------------------------------------------------------------
/* attributes queriable with query() */
enum {
NATIVE_WINDOW_WIDTH = 0,
NATIVE_WINDOW_HEIGHT = 1,
NATIVE_WINDOW_FORMAT = 2,
/* The minimum number of buffers that must remain un-dequeued after a buffer
* has been queued. This value applies only if set_buffer_count was used to
* override the number of buffers and if a buffer has since been queued.
* Users of the set_buffer_count ANativeWindow method should query this
* value before calling set_buffer_count. If it is necessary to have N
* buffers simultaneously dequeued as part of the steady-state operation,
* and this query returns M then N+M buffers should be requested via
* native_window_set_buffer_count.
*
* Note that this value does NOT apply until a single buffer has been
* queued. In particular this means that it is possible to:
*
* 1. Query M = min undequeued buffers
* 2. Set the buffer count to N + M
* 3. Dequeue all N + M buffers
* 4. Cancel M buffers
* 5. Queue, dequeue, queue, dequeue, ad infinitum
*/
NATIVE_WINDOW_MIN_UNDEQUEUED_BUFFERS = 3,
/* Check whether queueBuffer operations on the ANativeWindow send the buffer
* to the window compositor. The query sets the returned 'value' argument
* to 1 if the ANativeWindow DOES send queued buffers directly to the window
* compositor and 0 if the buffers do not go directly to the window
* compositor.
*
* This can be used to determine whether protected buffer content should be
* sent to the ANativeWindow. Note, however, that a result of 1 does NOT
* indicate that queued buffers will be protected from applications or users
* capturing their contents. If that behavior is desired then some other
* mechanism (e.g. the GRALLOC_USAGE_PROTECTED flag) should be used in
* conjunction with this query.
*/
NATIVE_WINDOW_QUEUES_TO_WINDOW_COMPOSER = 4,
/* Get the concrete type of a ANativeWindow. See below for the list of
* possible return values.
*
* This query should not be used outside the Android framework and will
* likely be removed in the near future.
*/
NATIVE_WINDOW_CONCRETE_TYPE = 5,
/*
* Default width and height of the ANativeWindow, these are the dimensions
* of the window irrespective of the NATIVE_WINDOW_SET_BUFFERS_DIMENSIONS
* call.
*/
NATIVE_WINDOW_DEFAULT_WIDTH = 6,
NATIVE_WINDOW_DEFAULT_HEIGHT = 7,
/*
* transformation that will most-likely be applied to buffers. This is only
* a hint, the actual transformation applied might be different.
*
* INTENDED USE:
*
* The transform hint can be used by a producer, for instance the GLES
* driver, to pre-rotate the rendering such that the final transformation
* in the composer is identity. This can be very useful when used in
* conjunction with the h/w composer HAL, in situations where it
* cannot handle arbitrary rotations.
*
* 1. Before dequeuing a buffer, the GL driver (or any other ANW client)
* queries the ANW for NATIVE_WINDOW_TRANSFORM_HINT.
*
* 2. The GL driver overrides the width and height of the ANW to
* account for NATIVE_WINDOW_TRANSFORM_HINT. This is done by querying
* NATIVE_WINDOW_DEFAULT_{WIDTH | HEIGHT}, swapping the dimensions
* according to NATIVE_WINDOW_TRANSFORM_HINT and calling
* native_window_set_buffers_dimensions().
*
* 3. The GL driver dequeues a buffer of the new pre-rotated size.
*
* 4. The GL driver renders to the buffer such that the image is
* already transformed, that is applying NATIVE_WINDOW_TRANSFORM_HINT
* to the rendering.
*
* 5. The GL driver calls native_window_set_transform to apply
* inverse transformation to the buffer it just rendered.
* In order to do this, the GL driver needs
* to calculate the inverse of NATIVE_WINDOW_TRANSFORM_HINT, this is
* done easily:
*
* int hintTransform, inverseTransform;
* query(..., NATIVE_WINDOW_TRANSFORM_HINT, &hintTransform);
* inverseTransform = hintTransform;
* if (hintTransform & HAL_TRANSFORM_ROT_90)
* inverseTransform ^= HAL_TRANSFORM_ROT_180;
*
*
* 6. The GL driver queues the pre-transformed buffer.
*
* 7. The composer combines the buffer transform with the display
* transform. If the buffer transform happens to cancel out the
* display transform then no rotation is needed.
*
*/
NATIVE_WINDOW_TRANSFORM_HINT = 8,
};
/* valid operations for the (*perform)() hook */
enum {
NATIVE_WINDOW_SET_USAGE = 0,
NATIVE_WINDOW_CONNECT = 1, /* deprecated */
NATIVE_WINDOW_DISCONNECT = 2, /* deprecated */
NATIVE_WINDOW_SET_CROP = 3,
NATIVE_WINDOW_SET_BUFFER_COUNT = 4,
NATIVE_WINDOW_SET_BUFFERS_GEOMETRY = 5, /* deprecated */
NATIVE_WINDOW_SET_BUFFERS_TRANSFORM = 6,
NATIVE_WINDOW_SET_BUFFERS_TIMESTAMP = 7,
NATIVE_WINDOW_SET_BUFFERS_DIMENSIONS = 8,
NATIVE_WINDOW_SET_BUFFERS_FORMAT = 9,
NATIVE_WINDOW_SET_SCALING_MODE = 10,
NATIVE_WINDOW_LOCK = 11, /* private */
NATIVE_WINDOW_UNLOCK_AND_POST = 12, /* private */
NATIVE_WINDOW_API_CONNECT = 13, /* private */
NATIVE_WINDOW_API_DISCONNECT = 14, /* private */
};
/* parameter for NATIVE_WINDOW_[API_][DIS]CONNECT */
enum {
/* Buffers will be queued by EGL via eglSwapBuffers after being filled using
* OpenGL ES.
*/
NATIVE_WINDOW_API_EGL = 1,
/* Buffers will be queued after being filled using the CPU
*/
NATIVE_WINDOW_API_CPU = 2,
/* Buffers will be queued by Stagefright after being filled by a video
* decoder. The video decoder can either be a software or hardware decoder.
*/
NATIVE_WINDOW_API_MEDIA = 3,
/* Buffers will be queued by the the camera HAL.
*/
NATIVE_WINDOW_API_CAMERA = 4,
};
/* parameter for NATIVE_WINDOW_SET_BUFFERS_TRANSFORM */
enum {
/* flip source image horizontally */
NATIVE_WINDOW_TRANSFORM_FLIP_H = HAL_TRANSFORM_FLIP_H ,
/* flip source image vertically */
NATIVE_WINDOW_TRANSFORM_FLIP_V = HAL_TRANSFORM_FLIP_V,
/* rotate source image 90 degrees clock-wise */
NATIVE_WINDOW_TRANSFORM_ROT_90 = HAL_TRANSFORM_ROT_90,
/* rotate source image 180 degrees */
NATIVE_WINDOW_TRANSFORM_ROT_180 = HAL_TRANSFORM_ROT_180,
/* rotate source image 270 degrees clock-wise */
NATIVE_WINDOW_TRANSFORM_ROT_270 = HAL_TRANSFORM_ROT_270,
};
/* parameter for NATIVE_WINDOW_SET_SCALING_MODE */
enum {
/* the window content is not updated (frozen) until a buffer of
* the window size is received (enqueued)
*/
NATIVE_WINDOW_SCALING_MODE_FREEZE = 0,
/* the buffer is scaled in both dimensions to match the window size */
NATIVE_WINDOW_SCALING_MODE_SCALE_TO_WINDOW = 1,
};
/* values returned by the NATIVE_WINDOW_CONCRETE_TYPE query */
enum {
NATIVE_WINDOW_FRAMEBUFFER = 0, /* FramebufferNativeWindow */
NATIVE_WINDOW_SURFACE = 1, /* Surface */
NATIVE_WINDOW_SURFACE_TEXTURE_CLIENT = 2, /* SurfaceTextureClient */
};
/* parameter for NATIVE_WINDOW_SET_BUFFERS_TIMESTAMP
*
* Special timestamp value to indicate that timestamps should be auto-generated
* by the native window when queueBuffer is called. This is equal to INT64_MIN,
* defined directly to avoid problems with C99/C++ inclusion of stdint.h.
*/
static const int64_t NATIVE_WINDOW_TIMESTAMP_AUTO = (-9223372036854775807LL-1);
struct ANativeWindow
{
#ifdef __cplusplus
ANativeWindow()
: flags(0), minSwapInterval(0), maxSwapInterval(0), xdpi(0), ydpi(0)
{
common.magic = ANDROID_NATIVE_WINDOW_MAGIC;
common.version = sizeof(ANativeWindow);
memset(common.reserved, 0, sizeof(common.reserved));
}
/* Implement the methods that sp<ANativeWindow> expects so that it
can be used to automatically refcount ANativeWindow's. */
void incStrong(const void* id) const {
common.incRef(const_cast<android_native_base_t*>(&common));
}
void decStrong(const void* id) const {
common.decRef(const_cast<android_native_base_t*>(&common));
}
#endif
struct android_native_base_t common;
/* flags describing some attributes of this surface or its updater */
const uint32_t flags;
/* min swap interval supported by this updated */
const int minSwapInterval;
/* max swap interval supported by this updated */
const int maxSwapInterval;
/* horizontal and vertical resolution in DPI */
const float xdpi;
const float ydpi;
/* Some storage reserved for the OEM's driver. */
intptr_t oem[4];
/*
* Set the swap interval for this surface.
*
* Returns 0 on success or -errno on error.
*/
int (*setSwapInterval)(struct ANativeWindow* window,
int interval);
/*
* hook called by EGL to acquire a buffer. After this call, the buffer
* is not locked, so its content cannot be modified.
* this call may block if no buffers are available.
*
* Returns 0 on success or -errno on error.
*/
int (*dequeueBuffer)(struct ANativeWindow* window,
struct ANativeWindowBuffer** buffer);
/*
* hook called by EGL to lock a buffer. This MUST be called before modifying
* the content of a buffer. The buffer must have been acquired with
* dequeueBuffer first.
*
* Returns 0 on success or -errno on error.
*/
int (*lockBuffer)(struct ANativeWindow* window,
struct ANativeWindowBuffer* buffer);
/*
* hook called by EGL when modifications to the render buffer are done.
* This unlocks and post the buffer.
*
* Buffers MUST be queued in the same order than they were dequeued.
*
* Returns 0 on success or -errno on error.
*/
int (*queueBuffer)(struct ANativeWindow* window,
struct ANativeWindowBuffer* buffer);
/*
* hook used to retrieve information about the native window.
*
* Returns 0 on success or -errno on error.
*/
int (*query)(const struct ANativeWindow* window,
int what, int* value);
/*
* hook used to perform various operations on the surface.
* (*perform)() is a generic mechanism to add functionality to
* ANativeWindow while keeping backward binary compatibility.
*
* DO NOT CALL THIS HOOK DIRECTLY. Instead, use the helper functions
* defined below.
*
* (*perform)() returns -ENOENT if the 'what' parameter is not supported
* by the surface's implementation.
*
* The valid operations are:
* NATIVE_WINDOW_SET_USAGE
* NATIVE_WINDOW_CONNECT (deprecated)
* NATIVE_WINDOW_DISCONNECT (deprecated)
* NATIVE_WINDOW_SET_CROP
* NATIVE_WINDOW_SET_BUFFER_COUNT
* NATIVE_WINDOW_SET_BUFFERS_GEOMETRY (deprecated)
* NATIVE_WINDOW_SET_BUFFERS_TRANSFORM
* NATIVE_WINDOW_SET_BUFFERS_TIMESTAMP
* NATIVE_WINDOW_SET_BUFFERS_DIMENSIONS
* NATIVE_WINDOW_SET_BUFFERS_FORMAT
* NATIVE_WINDOW_SET_SCALING_MODE
* NATIVE_WINDOW_LOCK (private)
* NATIVE_WINDOW_UNLOCK_AND_POST (private)
* NATIVE_WINDOW_API_CONNECT (private)
* NATIVE_WINDOW_API_DISCONNECT (private)
*
*/
int (*perform)(struct ANativeWindow* window,
int operation, ... );
/*
* hook used to cancel a buffer that has been dequeued.
* No synchronization is performed between dequeue() and cancel(), so
* either external synchronization is needed, or these functions must be
* called from the same thread.
*/
int (*cancelBuffer)(struct ANativeWindow* window,
struct ANativeWindowBuffer* buffer);
void* reserved_proc[2];
};
/* Backwards compatibility: use ANativeWindow (struct ANativeWindow in C).
* android_native_window_t is deprecated.
*/
typedef struct ANativeWindow ANativeWindow;
typedef struct ANativeWindow android_native_window_t;
/*
* native_window_set_usage(..., usage)
* Sets the intended usage flags for the next buffers
* acquired with (*lockBuffer)() and on.
* By default (if this function is never called), a usage of
* GRALLOC_USAGE_HW_RENDER | GRALLOC_USAGE_HW_TEXTURE
* is assumed.
* Calling this function will usually cause following buffers to be
* reallocated.
*/
static inline int native_window_set_usage(
struct ANativeWindow* window, int usage)
{
return window->perform(window, NATIVE_WINDOW_SET_USAGE, usage);
}
/* deprecated. Always returns 0. Don't call. */
static inline int native_window_connect(
struct ANativeWindow* window, int api) {
return 0;
}
/* deprecated. Always returns 0. Don't call. */
static inline int native_window_disconnect(
struct ANativeWindow* window, int api) {
return 0;
}
/*
* native_window_set_crop(..., crop)
* Sets which region of the next queued buffers needs to be considered.
* A buffer's crop region is scaled to match the surface's size.
*
* The specified crop region applies to all buffers queued after it is called.
*
* if 'crop' is NULL, subsequently queued buffers won't be cropped.
*
* An error is returned if for instance the crop region is invalid,
* out of the buffer's bound or if the window is invalid.
*/
static inline int native_window_set_crop(
struct ANativeWindow* window,
android_native_rect_t const * crop)
{
return window->perform(window, NATIVE_WINDOW_SET_CROP, crop);
}
/*
* native_window_set_buffer_count(..., count)
* Sets the number of buffers associated with this native window.
*/
static inline int native_window_set_buffer_count(
struct ANativeWindow* window,
size_t bufferCount)
{
return window->perform(window, NATIVE_WINDOW_SET_BUFFER_COUNT, bufferCount);
}
/*
* native_window_set_buffers_geometry(..., int w, int h, int format)
* All buffers dequeued after this call will have the dimensions and format
* specified. A successful call to this function has the same effect as calling
* native_window_set_buffers_size and native_window_set_buffers_format.
*
* XXX: This function is deprecated. The native_window_set_buffers_dimensions
* and native_window_set_buffers_format functions should be used instead.
*/
static inline int native_window_set_buffers_geometry(
struct ANativeWindow* window,
int w, int h, int format)
{
return window->perform(window, NATIVE_WINDOW_SET_BUFFERS_GEOMETRY,
w, h, format);
}
/*
* native_window_set_buffers_dimensions(..., int w, int h)
* All buffers dequeued after this call will have the dimensions specified.
* In particular, all buffers will have a fixed-size, independent form the
* native-window size. They will be scaled according to the scaling mode
* (see native_window_set_scaling_mode) upon window composition.
*
* If w and h are 0, the normal behavior is restored. That is, dequeued buffers
* following this call will be sized to match the window's size.
*
* Calling this function will reset the window crop to a NULL value, which
* disables cropping of the buffers.
*/
static inline int native_window_set_buffers_dimensions(
struct ANativeWindow* window,
int w, int h)
{
return window->perform(window, NATIVE_WINDOW_SET_BUFFERS_DIMENSIONS,
w, h);
}
/*
* native_window_set_buffers_format(..., int format)
* All buffers dequeued after this call will have the format specified.
*
* If the specified format is 0, the default buffer format will be used.
*/
static inline int native_window_set_buffers_format(
struct ANativeWindow* window,
int format)
{
return window->perform(window, NATIVE_WINDOW_SET_BUFFERS_FORMAT, format);
}
/*
* native_window_set_buffers_transform(..., int transform)
* All buffers queued after this call will be displayed transformed according
* to the transform parameter specified.
*/
static inline int native_window_set_buffers_transform(
struct ANativeWindow* window,
int transform)
{
return window->perform(window, NATIVE_WINDOW_SET_BUFFERS_TRANSFORM,
transform);
}
/*
* native_window_set_buffers_timestamp(..., int64_t timestamp)
* All buffers queued after this call will be associated with the timestamp
* parameter specified. If the timestamp is set to NATIVE_WINDOW_TIMESTAMP_AUTO
* (the default), timestamps will be generated automatically when queueBuffer is
* called. The timestamp is measured in nanoseconds, and is normally monotonically
* increasing. The timestamp should be unaffected by time-of-day adjustments,
* and for a camera should be strictly monotonic but for a media player may be
* reset when the position is set.
*/
static inline int native_window_set_buffers_timestamp(
struct ANativeWindow* window,
int64_t timestamp)
{
return window->perform(window, NATIVE_WINDOW_SET_BUFFERS_TIMESTAMP,
timestamp);
}
/*
* native_window_set_scaling_mode(..., int mode)
* All buffers queued after this call will be associated with the scaling mode
* specified.
*/
static inline int native_window_set_scaling_mode(
struct ANativeWindow* window,
int mode)
{
return window->perform(window, NATIVE_WINDOW_SET_SCALING_MODE,
mode);
}
/*
* native_window_api_connect(..., int api)
* connects an API to this window. only one API can be connected at a time.
* Returns -EINVAL if for some reason the window cannot be connected, which
* can happen if it's connected to some other API.
*/
static inline int native_window_api_connect(
struct ANativeWindow* window, int api)
{
return window->perform(window, NATIVE_WINDOW_API_CONNECT, api);
}
/*
* native_window_api_disconnect(..., int api)
* disconnect the API from this window.
* An error is returned if for instance the window wasn't connected in the
* first place.
*/
static inline int native_window_api_disconnect(
struct ANativeWindow* window, int api)
{
return window->perform(window, NATIVE_WINDOW_API_DISCONNECT, api);
}
__END_DECLS
#endif /* SYSTEM_CORE_INCLUDE_ANDROID_WINDOW_H */
|