summaryrefslogtreecommitdiffstats
blob: 41ca2e1a31f16f440503b9c3f1aa4487cff4284e (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
/*
 * Copyright (C) 2015 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef LIBZIPARCHIVE_ZIPWRITER_H_
#define LIBZIPARCHIVE_ZIPWRITER_H_

#include <cstdio>
#include <ctime>
#include <zlib.h>

#include <memory>
#include <string>
#include <vector>

#include "android-base/macros.h"
#include "utils/Compat.h"

/**
 * Writes a Zip file via a stateful interface.
 *
 * Example:
 *
 *   FILE* file = fopen("path/to/zip.zip", "wb");
 *
 *   ZipWriter writer(file);
 *
 *   writer.StartEntry("test.txt", ZipWriter::kCompress | ZipWriter::kAlign);
 *   writer.WriteBytes(buffer, bufferLen);
 *   writer.WriteBytes(buffer2, bufferLen2);
 *   writer.FinishEntry();
 *
 *   writer.StartEntry("empty.txt", 0);
 *   writer.FinishEntry();
 *
 *   writer.Finish();
 *
 *   fclose(file);
 */
class ZipWriter {
public:
  enum {
    /**
     * Flag to compress the zip entry using deflate.
     */
    kCompress = 0x01,

    /**
     * Flag to align the zip entry data on a 32bit boundary. Useful for
     * mmapping the data at runtime.
     */
    kAlign32 = 0x02,
  };

  /**
   * A struct representing a zip file entry.
   */
  struct FileEntry {
    std::string path;
    uint16_t compression_method;
    uint32_t crc32;
    uint32_t compressed_size;
    uint32_t uncompressed_size;
    uint16_t last_mod_time;
    uint16_t last_mod_date;
    uint32_t local_file_header_offset;
  };

  static const char* ErrorCodeString(int32_t error_code);

  /**
   * Create a ZipWriter that will write into a FILE stream. The file should be opened with
   * open mode of "wb" or "w+b". ZipWriter does not take ownership of the file stream. The
   * caller is responsible for closing the file.
   */
  explicit ZipWriter(FILE* f);

  // Move constructor.
  ZipWriter(ZipWriter&& zipWriter);

  // Move assignment.
  ZipWriter& operator=(ZipWriter&& zipWriter);

  /**
   * Starts a new zip entry with the given path and flags.
   * Flags can be a bitwise OR of ZipWriter::kCompress and ZipWriter::kAlign.
   * Subsequent calls to WriteBytes(const void*, size_t) will add data to this entry.
   * Returns 0 on success, and an error value < 0 on failure.
   */
  int32_t StartEntry(const char* path, size_t flags);

  /**
   * Starts a new zip entry with the given path and flags, where the
   * entry will be aligned to the given alignment.
   * Flags can only be ZipWriter::kCompress. Using the flag ZipWriter::kAlign32
   * will result in an error.
   * Subsequent calls to WriteBytes(const void*, size_t) will add data to this entry.
   * Returns 0 on success, and an error value < 0 on failure.
   */
  int32_t StartAlignedEntry(const char* path, size_t flags, uint32_t alignment);

  /**
   * Same as StartEntry(const char*, size_t), but sets a last modified time for the entry.
   */
  int32_t StartEntryWithTime(const char* path, size_t flags, time_t time);

  /**
   * Same as StartAlignedEntry(const char*, size_t), but sets a last modified time for the entry.
   */
  int32_t StartAlignedEntryWithTime(const char* path, size_t flags, time_t time,
                                    uint32_t alignment);

  /**
   * Writes bytes to the zip file for the previously started zip entry.
   * Returns 0 on success, and an error value < 0 on failure.
   */
  int32_t WriteBytes(const void* data, size_t len);

  /**
   * Finish a zip entry started with StartEntry(const char*, size_t) or
   * StartEntryWithTime(const char*, size_t, time_t). This must be called before
   * any new zip entries are started, or before Finish() is called.
   * Returns 0 on success, and an error value < 0 on failure.
   */
  int32_t FinishEntry();

  /**
   * Discards the last-written entry. Can only be called after an entry has been written using
   * FinishEntry().
   * Returns 0 on success, and an error value < 0 on failure.
   */
  int32_t DiscardLastEntry();

  /**
   * Sets `out_entry` to the last entry written after a call to FinishEntry().
   * Returns 0 on success, and an error value < 0 if no entries have been written.
   */
  int32_t GetLastEntry(FileEntry* out_entry);

  /**
   * Writes the Central Directory Headers and flushes the zip file stream.
   * Returns 0 on success, and an error value < 0 on failure.
   */
  int32_t Finish();

private:
  DISALLOW_COPY_AND_ASSIGN(ZipWriter);

  int32_t HandleError(int32_t error_code);
  int32_t PrepareDeflate();
  int32_t StoreBytes(FileEntry* file, const void* data, size_t len);
  int32_t CompressBytes(FileEntry* file, const void* data, size_t len);
  int32_t FlushCompressedBytes(FileEntry* file);

  enum class State {
    kWritingZip,
    kWritingEntry,
    kDone,
    kError,
  };

  FILE* file_;
  off64_t current_offset_;
  State state_;
  std::vector<FileEntry> files_;
  FileEntry current_file_entry_;

  std::unique_ptr<z_stream, void(*)(z_stream*)> z_stream_;
  std::vector<uint8_t> buffer_;
};

#endif /* LIBZIPARCHIVE_ZIPWRITER_H_ */