1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
|
/*
* Copyright (C) 2015 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#include "action.h"
#include <android-base/chrono_utils.h>
#include <android-base/logging.h>
#include <android-base/properties.h>
#include <android-base/strings.h>
#include "util.h"
using android::base::Join;
namespace android {
namespace init {
Result<Success> RunBuiltinFunction(const BuiltinFunction& function,
const std::vector<std::string>& args,
const std::string& context) {
auto builtin_arguments = BuiltinArguments(context);
builtin_arguments.args.resize(args.size());
builtin_arguments.args[0] = args[0];
for (std::size_t i = 1; i < args.size(); ++i) {
if (!expand_props(args[i], &builtin_arguments.args[i])) {
return Error() << "cannot expand '" << args[i] << "'";
}
}
return function(builtin_arguments);
}
Command::Command(BuiltinFunction f, bool execute_in_subcontext,
const std::vector<std::string>& args, int line)
: func_(std::move(f)), execute_in_subcontext_(execute_in_subcontext), args_(args), line_(line) {}
Result<Success> Command::InvokeFunc(Subcontext* subcontext) const {
if (subcontext) {
if (execute_in_subcontext_) {
return subcontext->Execute(args_);
}
auto expanded_args = subcontext->ExpandArgs(args_);
if (!expanded_args) {
return expanded_args.error();
}
return RunBuiltinFunction(func_, *expanded_args, subcontext->context());
}
return RunBuiltinFunction(func_, args_, kInitContext);
}
std::string Command::BuildCommandString() const {
return Join(args_, ' ');
}
Action::Action(bool oneshot, Subcontext* subcontext, const std::string& filename, int line,
const std::string& event_trigger,
const std::map<std::string, std::string>& property_triggers)
: property_triggers_(property_triggers),
event_trigger_(event_trigger),
oneshot_(oneshot),
subcontext_(subcontext),
filename_(filename),
line_(line) {}
const KeywordFunctionMap* Action::function_map_ = nullptr;
Result<Success> Action::AddCommand(const std::vector<std::string>& args, int line) {
if (!function_map_) {
return Error() << "no function map available";
}
auto function = function_map_->FindFunction(args);
if (!function) return Error() << function.error();
commands_.emplace_back(function->second, function->first, args, line);
return Success();
}
void Action::AddCommand(BuiltinFunction f, const std::vector<std::string>& args, int line) {
commands_.emplace_back(f, false, args, line);
}
std::size_t Action::NumCommands() const {
return commands_.size();
}
void Action::ExecuteOneCommand(std::size_t command) const {
// We need a copy here since some Command execution may result in
// changing commands_ vector by importing .rc files through parser
Command cmd = commands_[command];
ExecuteCommand(cmd);
}
void Action::ExecuteAllCommands() const {
for (const auto& c : commands_) {
ExecuteCommand(c);
}
}
void Action::ExecuteCommand(const Command& command) const {
android::base::Timer t;
auto result = command.InvokeFunc(subcontext_);
auto duration = t.duration();
// There are many legacy paths in rootdir/init.rc that will virtually never exist on a new
// device, such as '/sys/class/leds/jogball-backlight/brightness'. As of this writing, there
// are 198 such failures on bullhead. Instead of spamming the log reporting them, we do not
// report such failures unless we're running at the DEBUG log level.
bool report_failure = !result.has_value();
if (report_failure && android::base::GetMinimumLogSeverity() > android::base::DEBUG &&
result.error_errno() == ENOENT) {
report_failure = false;
}
// Any action longer than 50ms will be warned to user as slow operation
if (report_failure || duration > 50ms ||
android::base::GetMinimumLogSeverity() <= android::base::DEBUG) {
std::string trigger_name = BuildTriggersString();
std::string cmd_str = command.BuildCommandString();
LOG(INFO) << "Command '" << cmd_str << "' action=" << trigger_name << " (" << filename_
<< ":" << command.line() << ") took " << duration.count() << "ms and "
<< (result ? "succeeded" : "failed: " + result.error_string());
}
}
// This function checks that all property triggers are satisfied, that is
// for each (name, value) in property_triggers_, check that the current
// value of the property 'name' == value.
//
// It takes an optional (name, value) pair, which if provided must
// be present in property_triggers_; it skips the check of the current
// property value for this pair.
bool Action::CheckPropertyTriggers(const std::string& name,
const std::string& value) const {
if (property_triggers_.empty()) {
return true;
}
bool found = name.empty();
for (const auto& [trigger_name, trigger_value] : property_triggers_) {
if (trigger_name == name) {
if (trigger_value != "*" && trigger_value != value) {
return false;
} else {
found = true;
}
} else {
std::string prop_val = android::base::GetProperty(trigger_name, "");
if (prop_val.empty() || (trigger_value != "*" && trigger_value != prop_val)) {
return false;
}
}
}
return found;
}
bool Action::CheckEvent(const EventTrigger& event_trigger) const {
return event_trigger == event_trigger_ && CheckPropertyTriggers();
}
bool Action::CheckEvent(const PropertyChange& property_change) const {
const auto& [name, value] = property_change;
return event_trigger_.empty() && CheckPropertyTriggers(name, value);
}
bool Action::CheckEvent(const BuiltinAction& builtin_action) const {
return this == builtin_action;
}
std::string Action::BuildTriggersString() const {
std::vector<std::string> triggers;
for (const auto& [trigger_name, trigger_value] : property_triggers_) {
triggers.emplace_back(trigger_name + '=' + trigger_value);
}
if (!event_trigger_.empty()) {
triggers.emplace_back(event_trigger_);
}
return Join(triggers, " && ");
}
void Action::DumpState() const {
std::string trigger_name = BuildTriggersString();
LOG(INFO) << "on " << trigger_name;
for (const auto& c : commands_) {
std::string cmd_str = c.BuildCommandString();
LOG(INFO) << " " << cmd_str;
}
}
} // namespace init
} // namespace android
|