summaryrefslogtreecommitdiffstats
blob: a91cd1dd109883ab7529b8997e23201c408fe9d3 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
// Copyright (C) 2016 The Android Open Source Project
//
// Licensed under the Apache License, Version 2.0 (the "License");
// you may not use this file except in compliance with the License.
// You may obtain a copy of the License at
//
//      http://www.apache.org/licenses/LICENSE-2.0
//
// Unless required by applicable law or agreed to in writing, software
// distributed under the License is distributed on an "AS IS" BASIS,
// WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
// See the License for the specific language governing permissions and
// limitations under the License.

#include "capabilities.h"

#include <sys/prctl.h>

#include <map>
#include <memory>

#include <android-base/logging.h>
#include <android-base/macros.h>

#define CAP_MAP_ENTRY(cap) { #cap, CAP_##cap }

namespace android {
namespace init {

static const std::map<std::string, int> cap_map = {
    CAP_MAP_ENTRY(CHOWN),
    CAP_MAP_ENTRY(DAC_OVERRIDE),
    CAP_MAP_ENTRY(DAC_READ_SEARCH),
    CAP_MAP_ENTRY(FOWNER),
    CAP_MAP_ENTRY(FSETID),
    CAP_MAP_ENTRY(KILL),
    CAP_MAP_ENTRY(SETGID),
    CAP_MAP_ENTRY(SETUID),
    CAP_MAP_ENTRY(SETPCAP),
    CAP_MAP_ENTRY(LINUX_IMMUTABLE),
    CAP_MAP_ENTRY(NET_BIND_SERVICE),
    CAP_MAP_ENTRY(NET_BROADCAST),
    CAP_MAP_ENTRY(NET_ADMIN),
    CAP_MAP_ENTRY(NET_RAW),
    CAP_MAP_ENTRY(IPC_LOCK),
    CAP_MAP_ENTRY(IPC_OWNER),
    CAP_MAP_ENTRY(SYS_MODULE),
    CAP_MAP_ENTRY(SYS_RAWIO),
    CAP_MAP_ENTRY(SYS_CHROOT),
    CAP_MAP_ENTRY(SYS_PTRACE),
    CAP_MAP_ENTRY(SYS_PACCT),
    CAP_MAP_ENTRY(SYS_ADMIN),
    CAP_MAP_ENTRY(SYS_BOOT),
    CAP_MAP_ENTRY(SYS_NICE),
    CAP_MAP_ENTRY(SYS_RESOURCE),
    CAP_MAP_ENTRY(SYS_TIME),
    CAP_MAP_ENTRY(SYS_TTY_CONFIG),
    CAP_MAP_ENTRY(MKNOD),
    CAP_MAP_ENTRY(LEASE),
    CAP_MAP_ENTRY(AUDIT_WRITE),
    CAP_MAP_ENTRY(AUDIT_CONTROL),
    CAP_MAP_ENTRY(SETFCAP),
    CAP_MAP_ENTRY(MAC_OVERRIDE),
    CAP_MAP_ENTRY(MAC_ADMIN),
    CAP_MAP_ENTRY(SYSLOG),
    CAP_MAP_ENTRY(WAKE_ALARM),
    CAP_MAP_ENTRY(BLOCK_SUSPEND),
    CAP_MAP_ENTRY(AUDIT_READ),
};

static_assert(CAP_LAST_CAP == CAP_AUDIT_READ, "CAP_LAST_CAP is not CAP_AUDIT_READ");

static bool ComputeCapAmbientSupported() {
#if defined(__ANDROID__)
    return prctl(PR_CAP_AMBIENT, PR_CAP_AMBIENT_IS_SET, CAP_CHOWN, 0, 0) >= 0;
#else
    return true;
#endif
}

static unsigned int ComputeLastValidCap() {
#if defined(__ANDROID__)
    // Android does not support kernels < 3.8. 'CAP_WAKE_ALARM' has been present since 3.0, see
    // http://lxr.free-electrons.com/source/include/linux/capability.h?v=3.0#L360.
    unsigned int last_valid_cap = CAP_WAKE_ALARM;
    for (; prctl(PR_CAPBSET_READ, last_valid_cap, 0, 0, 0) >= 0; ++last_valid_cap);

    // |last_valid_cap| will be the first failing value.
    return last_valid_cap - 1;
#else
    return CAP_LAST_CAP;
#endif
}

static bool DropBoundingSet(const CapSet& to_keep) {
    unsigned int last_valid_cap = GetLastValidCap();
    // When dropping the bounding set, attempt to drop capabilities reported at
    // run-time, not at compile-time.
    // If the run-time kernel is older than the compile-time headers, this
    // avoids dropping an invalid capability. If the run-time kernel is newer
    // than the headers, this guarantees all capabilities (even those unknown at
    // compile time) will be dropped.
    for (size_t cap = 0; cap <= last_valid_cap; ++cap) {
        if (cap < to_keep.size() && to_keep.test(cap)) {
            // No need to drop this capability.
            continue;
        }
        if (cap_drop_bound(cap) == -1) {
            PLOG(ERROR) << "cap_drop_bound(" << cap << ") failed";
            return false;
        }
    }
    return true;
}

static bool SetProcCaps(const CapSet& to_keep, bool add_setpcap) {
    ScopedCaps caps(cap_init());

    cap_clear(caps.get());
    cap_value_t value[1];
    for (size_t cap = 0; cap < to_keep.size(); ++cap) {
        if (to_keep.test(cap)) {
            value[0] = cap;
            if (cap_set_flag(caps.get(), CAP_INHERITABLE, arraysize(value), value, CAP_SET) != 0 ||
                cap_set_flag(caps.get(), CAP_PERMITTED, arraysize(value), value, CAP_SET) != 0) {
                PLOG(ERROR) << "cap_set_flag(INHERITABLE|PERMITTED, " << cap << ") failed";
                return false;
            }
        }
    }

    if (add_setpcap) {
        value[0] = CAP_SETPCAP;
        if (cap_set_flag(caps.get(), CAP_PERMITTED, arraysize(value), value, CAP_SET) != 0 ||
            cap_set_flag(caps.get(), CAP_EFFECTIVE, arraysize(value), value, CAP_SET) != 0) {
            PLOG(ERROR) << "cap_set_flag(PERMITTED|EFFECTIVE, " << CAP_SETPCAP << ") failed";
            return false;
        }
    }

    if (cap_set_proc(caps.get()) != 0) {
        PLOG(ERROR) << "cap_set_proc(" << to_keep.to_ulong() << ") failed";
        return false;
    }
    return true;
}

static bool SetAmbientCaps(const CapSet& to_raise) {
#if defined(__ANDROID__)
    for (size_t cap = 0; cap < to_raise.size(); ++cap) {
        if (to_raise.test(cap)) {
            if (prctl(PR_CAP_AMBIENT, PR_CAP_AMBIENT_RAISE, cap, 0, 0) != 0) {
                PLOG(ERROR) << "prctl(PR_CAP_AMBIENT, PR_CAP_AMBIENT_RAISE, " << cap << ") failed";
                return false;
            }
        }
    }
#endif
    return true;
}

int LookupCap(const std::string& cap_name) {
    auto e = cap_map.find(cap_name);
    if (e != cap_map.end()) {
        return e->second;
    } else {
        return -1;
    }
}

bool CapAmbientSupported() {
    static bool cap_ambient_supported = ComputeCapAmbientSupported();
    return cap_ambient_supported;
}

unsigned int GetLastValidCap() {
    static unsigned int last_valid_cap = ComputeLastValidCap();
    return last_valid_cap;
}

bool SetCapsForExec(const CapSet& to_keep) {
    // Need to keep SETPCAP to drop bounding set below.
    bool add_setpcap = true;
    if (!SetProcCaps(to_keep, add_setpcap)) {
        LOG(ERROR) << "failed to apply initial capset";
        return false;
    }

    if (!DropBoundingSet(to_keep)) {
        return false;
    }

    // If SETPCAP wasn't specifically requested, drop it now.
    add_setpcap = false;
    if (!SetProcCaps(to_keep, add_setpcap)) {
        LOG(ERROR) << "failed to apply final capset";
        return false;
    }

    // Add the capabilities to the ambient set so that they are preserved across
    // execve(2).
    // See http://man7.org/linux/man-pages/man7/capabilities.7.html.
    return SetAmbientCaps(to_keep);
}

bool DropInheritableCaps() {
    ScopedCaps caps(cap_get_proc());
    if (cap_clear_flag(caps.get(), CAP_INHERITABLE) == -1) {
        PLOG(ERROR) << "cap_clear_flag(INHERITABLE) failed";
        return false;
    }
    if (cap_set_proc(caps.get()) != 0) {
        PLOG(ERROR) << "cap_set_proc() failed";
        return false;
    }
    return true;
}

}  // namespace init
}  // namespace android