summaryrefslogtreecommitdiffstats
blob: ed4a7398a79573392d241947da31c66838989743 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
/*
 * Copyright (C) 2007 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include "devices.h"

#include <errno.h>
#include <fnmatch.h>
#include <sys/sysmacros.h>
#include <unistd.h>

#include <memory>

#include <android-base/logging.h>
#include <android-base/stringprintf.h>
#include <android-base/strings.h>
#include <private/android_filesystem_config.h>
#include <selinux/android.h>
#include <selinux/selinux.h>

#include "selinux.h"
#include "util.h"

#ifdef _INIT_INIT_H
#error "Do not include init.h in files used by ueventd or watchdogd; it will expose init's globals"
#endif

using android::base::Basename;
using android::base::Dirname;
using android::base::Readlink;
using android::base::Realpath;
using android::base::StartsWith;
using android::base::StringPrintf;

namespace android {
namespace init {

/* Given a path that may start with a PCI device, populate the supplied buffer
 * with the PCI domain/bus number and the peripheral ID and return 0.
 * If it doesn't start with a PCI device, or there is some error, return -1 */
static bool FindPciDevicePrefix(const std::string& path, std::string* result) {
    result->clear();

    if (!StartsWith(path, "/devices/pci")) return false;

    /* Beginning of the prefix is the initial "pci" after "/devices/" */
    std::string::size_type start = 9;

    /* End of the prefix is two path '/' later, capturing the domain/bus number
     * and the peripheral ID. Example: pci0000:00/0000:00:1f.2 */
    auto end = path.find('/', start);
    if (end == std::string::npos) return false;

    end = path.find('/', end + 1);
    if (end == std::string::npos) return false;

    auto length = end - start;
    if (length <= 4) {
        // The minimum string that will get to this check is 'pci/', which is malformed,
        // so return false
        return false;
    }

    *result = path.substr(start, length);
    return true;
}

/* Given a path that may start with a virtual block device, populate
 * the supplied buffer with the virtual block device ID and return 0.
 * If it doesn't start with a virtual block device, or there is some
 * error, return -1 */
static bool FindVbdDevicePrefix(const std::string& path, std::string* result) {
    result->clear();

    if (!StartsWith(path, "/devices/vbd-")) return false;

    /* Beginning of the prefix is the initial "vbd-" after "/devices/" */
    std::string::size_type start = 13;

    /* End of the prefix is one path '/' later, capturing the
       virtual block device ID. Example: 768 */
    auto end = path.find('/', start);
    if (end == std::string::npos) return false;

    auto length = end - start;
    if (length == 0) return false;

    *result = path.substr(start, length);
    return true;
}

Permissions::Permissions(const std::string& name, mode_t perm, uid_t uid, gid_t gid)
    : name_(name), perm_(perm), uid_(uid), gid_(gid), prefix_(false), wildcard_(false) {
    // Set 'prefix_' or 'wildcard_' based on the below cases:
    //
    // 1) No '*' in 'name' -> Neither are set and Match() checks a given path for strict
    //    equality with 'name'
    //
    // 2) '*' only appears as the last character in 'name' -> 'prefix'_ is set to true and
    //    Match() checks if 'name' is a prefix of a given path.
    //
    // 3) '*' appears elsewhere -> 'wildcard_' is set to true and Match() uses fnmatch()
    //    with FNM_PATHNAME to compare 'name' to a given path.

    auto wildcard_position = name_.find('*');
    if (wildcard_position != std::string::npos) {
        if (wildcard_position == name_.length() - 1) {
            prefix_ = true;
            name_.pop_back();
        } else {
            wildcard_ = true;
        }
    }
}

bool Permissions::Match(const std::string& path) const {
    if (prefix_) return StartsWith(path, name_);
    if (wildcard_) return fnmatch(name_.c_str(), path.c_str(), FNM_PATHNAME) == 0;
    return path == name_;
}

bool SysfsPermissions::MatchWithSubsystem(const std::string& path,
                                          const std::string& subsystem) const {
    std::string path_basename = Basename(path);
    if (name().find(subsystem) != std::string::npos) {
        if (Match("/sys/class/" + subsystem + "/" + path_basename)) return true;
        if (Match("/sys/bus/" + subsystem + "/devices/" + path_basename)) return true;
    }
    return Match(path);
}

void SysfsPermissions::SetPermissions(const std::string& path) const {
    std::string attribute_file = path + "/" + attribute_;
    LOG(VERBOSE) << "fixup " << attribute_file << " " << uid() << " " << gid() << " " << std::oct
                 << perm();

    if (access(attribute_file.c_str(), F_OK) == 0) {
        if (chown(attribute_file.c_str(), uid(), gid()) != 0) {
            PLOG(ERROR) << "chown(" << attribute_file << ", " << uid() << ", " << gid()
                        << ") failed";
        }
        if (chmod(attribute_file.c_str(), perm()) != 0) {
            PLOG(ERROR) << "chmod(" << attribute_file << ", " << perm() << ") failed";
        }
    }
}

// Given a path that may start with a platform device, find the parent platform device by finding a
// parent directory with a 'subsystem' symlink that points to the platform bus.
// If it doesn't start with a platform device, return false
bool DeviceHandler::FindPlatformDevice(std::string path, std::string* platform_device_path) const {
    platform_device_path->clear();

    // Uevents don't contain the mount point, so we need to add it here.
    path.insert(0, sysfs_mount_point_);

    std::string directory = Dirname(path);

    while (directory != "/" && directory != ".") {
        std::string subsystem_link_path;
        if (Realpath(directory + "/subsystem", &subsystem_link_path) &&
            subsystem_link_path == sysfs_mount_point_ + "/bus/platform") {
            // We need to remove the mount point that we added above before returning.
            directory.erase(0, sysfs_mount_point_.size());
            *platform_device_path = directory;
            return true;
        }

        auto last_slash = path.rfind('/');
        if (last_slash == std::string::npos) return false;

        path.erase(last_slash);
        directory = Dirname(path);
    }

    return false;
}

void DeviceHandler::FixupSysPermissions(const std::string& upath,
                                        const std::string& subsystem) const {
    // upaths omit the "/sys" that paths in this list
    // contain, so we prepend it...
    std::string path = "/sys" + upath;

    for (const auto& s : sysfs_permissions_) {
        if (s.MatchWithSubsystem(path, subsystem)) s.SetPermissions(path);
    }

    if (!skip_restorecon_ && access(path.c_str(), F_OK) == 0) {
        LOG(VERBOSE) << "restorecon_recursive: " << path;
        if (selinux_android_restorecon(path.c_str(), SELINUX_ANDROID_RESTORECON_RECURSE) != 0) {
            PLOG(ERROR) << "selinux_android_restorecon(" << path << ") failed";
        }
    }
}

std::tuple<mode_t, uid_t, gid_t> DeviceHandler::GetDevicePermissions(
    const std::string& path, const std::vector<std::string>& links) const {
    // Search the perms list in reverse so that ueventd.$hardware can override ueventd.rc.
    for (auto it = dev_permissions_.crbegin(); it != dev_permissions_.crend(); ++it) {
        if (it->Match(path) || std::any_of(links.cbegin(), links.cend(),
                                           [it](const auto& link) { return it->Match(link); })) {
            return {it->perm(), it->uid(), it->gid()};
        }
    }
    /* Default if nothing found. */
    return {0600, 0, 0};
}

void DeviceHandler::MakeDevice(const std::string& path, bool block, int major, int minor,
                               const std::vector<std::string>& links) const {
    auto[mode, uid, gid] = GetDevicePermissions(path, links);
    mode |= (block ? S_IFBLK : S_IFCHR);

    std::string secontext;
    if (!SelabelLookupFileContextBestMatch(path, links, mode, &secontext)) {
        PLOG(ERROR) << "Device '" << path << "' not created; cannot find SELinux label";
        return;
    }
    if (!secontext.empty()) {
        setfscreatecon(secontext.c_str());
    }

    dev_t dev = makedev(major, minor);
    /* Temporarily change egid to avoid race condition setting the gid of the
     * device node. Unforunately changing the euid would prevent creation of
     * some device nodes, so the uid has to be set with chown() and is still
     * racy. Fixing the gid race at least fixed the issue with system_server
     * opening dynamic input devices under the AID_INPUT gid. */
    if (setegid(gid)) {
        PLOG(ERROR) << "setegid(" << gid << ") for " << path << " device failed";
        goto out;
    }
    /* If the node already exists update its SELinux label to handle cases when
     * it was created with the wrong context during coldboot procedure. */
    if (mknod(path.c_str(), mode, dev) && (errno == EEXIST) && !secontext.empty()) {
        char* fcon = nullptr;
        int rc = lgetfilecon(path.c_str(), &fcon);
        if (rc < 0) {
            PLOG(ERROR) << "Cannot get SELinux label on '" << path << "' device";
            goto out;
        }

        bool different = fcon != secontext;
        freecon(fcon);

        if (different && lsetfilecon(path.c_str(), secontext.c_str())) {
            PLOG(ERROR) << "Cannot set '" << secontext << "' SELinux label on '" << path
                        << "' device";
        }
    }

out:
    chown(path.c_str(), uid, -1);
    if (setegid(AID_ROOT)) {
        PLOG(FATAL) << "setegid(AID_ROOT) failed";
    }

    if (!secontext.empty()) {
        setfscreatecon(nullptr);
    }
}

// replaces any unacceptable characters with '_', the
// length of the resulting string is equal to the input string
void SanitizePartitionName(std::string* string) {
    const char* accept =
        "abcdefghijklmnopqrstuvwxyz"
        "ABCDEFGHIJKLMNOPQRSTUVWXYZ"
        "0123456789"
        "_-.";

    if (!string) return;

    std::string::size_type pos = 0;
    while ((pos = string->find_first_not_of(accept, pos)) != std::string::npos) {
        (*string)[pos] = '_';
    }
}

std::vector<std::string> DeviceHandler::GetBlockDeviceSymlinks(const Uevent& uevent) const {
    std::string device;
    std::string type;

    if (FindPlatformDevice(uevent.path, &device)) {
        // Skip /devices/platform or /devices/ if present
        static const std::string devices_platform_prefix = "/devices/platform/";
        static const std::string devices_prefix = "/devices/";

        if (StartsWith(device, devices_platform_prefix)) {
            device = device.substr(devices_platform_prefix.length());
        } else if (StartsWith(device, devices_prefix)) {
            device = device.substr(devices_prefix.length());
        }

        type = "platform";
    } else if (FindPciDevicePrefix(uevent.path, &device)) {
        type = "pci";
    } else if (FindVbdDevicePrefix(uevent.path, &device)) {
        type = "vbd";
    } else {
        return {};
    }

    std::vector<std::string> links;

    LOG(VERBOSE) << "found " << type << " device " << device;

    auto link_path = "/dev/block/" + type + "/" + device;

    if (!uevent.partition_name.empty()) {
        std::string partition_name_sanitized(uevent.partition_name);
        SanitizePartitionName(&partition_name_sanitized);
        if (partition_name_sanitized != uevent.partition_name) {
            LOG(VERBOSE) << "Linking partition '" << uevent.partition_name << "' as '"
                         << partition_name_sanitized << "'";
        }
        links.emplace_back(link_path + "/by-name/" + partition_name_sanitized);
        // Adds symlink: /dev/block/by-name/<partition_name>.
        if (boot_devices_.find(device) != boot_devices_.end()) {
            links.emplace_back("/dev/block/by-name/" + partition_name_sanitized);
        }
    }

    auto last_slash = uevent.path.rfind('/');
    links.emplace_back(link_path + "/" + uevent.path.substr(last_slash + 1));

    return links;
}

void DeviceHandler::HandleDevice(const std::string& action, const std::string& devpath, bool block,
                                 int major, int minor, const std::vector<std::string>& links) const {
    if (action == "add") {
        MakeDevice(devpath, block, major, minor, links);
        for (const auto& link : links) {
            if (!mkdir_recursive(Dirname(link), 0755)) {
                PLOG(ERROR) << "Failed to create directory " << Dirname(link);
            }

            if (symlink(devpath.c_str(), link.c_str())) {
                if (errno != EEXIST) {
                    PLOG(ERROR) << "Failed to symlink " << devpath << " to " << link;
                } else if (std::string link_path;
                           Readlink(link, &link_path) && link_path != devpath) {
                    PLOG(ERROR) << "Failed to symlink " << devpath << " to " << link
                                << ", which already links to: " << link_path;
                }
            }
        }
    }

    if (action == "remove") {
        for (const auto& link : links) {
            std::string link_path;
            if (Readlink(link, &link_path) && link_path == devpath) {
                unlink(link.c_str());
            }
        }
        unlink(devpath.c_str());
    }
}

void DeviceHandler::HandleDeviceEvent(const Uevent& uevent) {
    if (uevent.action == "add" || uevent.action == "change" || uevent.action == "online") {
        FixupSysPermissions(uevent.path, uevent.subsystem);
    }

    // if it's not a /dev device, nothing to do
    if (uevent.major < 0 || uevent.minor < 0) return;

    std::string devpath;
    std::vector<std::string> links;
    bool block = false;

    if (uevent.subsystem == "block") {
        block = true;
        devpath = "/dev/block/" + Basename(uevent.path);

        if (StartsWith(uevent.path, "/devices")) {
            links = GetBlockDeviceSymlinks(uevent);
        }
    } else if (const auto subsystem =
                   std::find(subsystems_.cbegin(), subsystems_.cend(), uevent.subsystem);
               subsystem != subsystems_.cend()) {
        devpath = subsystem->ParseDevPath(uevent);
    } else if (uevent.subsystem == "usb") {
        if (!uevent.device_name.empty()) {
            devpath = "/dev/" + uevent.device_name;
        } else {
            // This imitates the file system that would be created
            // if we were using devfs instead.
            // Minors are broken up into groups of 128, starting at "001"
            int bus_id = uevent.minor / 128 + 1;
            int device_id = uevent.minor % 128 + 1;
            devpath = StringPrintf("/dev/bus/usb/%03d/%03d", bus_id, device_id);
        }
    } else if (StartsWith(uevent.subsystem, "usb")) {
        // ignore other USB events
        return;
    } else {
        devpath = "/dev/" + Basename(uevent.path);
    }

    mkdir_recursive(Dirname(devpath), 0755);

    HandleDevice(uevent.action, devpath, block, uevent.major, uevent.minor, links);
}

DeviceHandler::DeviceHandler(std::vector<Permissions> dev_permissions,
                             std::vector<SysfsPermissions> sysfs_permissions,
                             std::vector<Subsystem> subsystems, std::set<std::string> boot_devices,
                             bool skip_restorecon)
    : dev_permissions_(std::move(dev_permissions)),
      sysfs_permissions_(std::move(sysfs_permissions)),
      subsystems_(std::move(subsystems)),
      boot_devices_(std::move(boot_devices)),
      skip_restorecon_(skip_restorecon),
      sysfs_mount_point_("/sys") {}

DeviceHandler::DeviceHandler()
    : DeviceHandler(std::vector<Permissions>{}, std::vector<SysfsPermissions>{},
                    std::vector<Subsystem>{}, std::set<std::string>{}, false) {}

}  // namespace init
}  // namespace android