1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
|
/*
* Copyright (C) 2007 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef _INIT_DEVICES_H
#define _INIT_DEVICES_H
#include <sys/stat.h>
#include <sys/types.h>
#include <algorithm>
#include <set>
#include <string>
#include <vector>
#include <android-base/file.h>
#include <selinux/label.h>
#include "uevent.h"
namespace android {
namespace init {
class Permissions {
public:
Permissions(const std::string& name, mode_t perm, uid_t uid, gid_t gid);
bool Match(const std::string& path) const;
mode_t perm() const { return perm_; }
uid_t uid() const { return uid_; }
gid_t gid() const { return gid_; }
protected:
const std::string& name() const { return name_; }
private:
std::string name_;
mode_t perm_;
uid_t uid_;
gid_t gid_;
bool prefix_;
bool wildcard_;
};
class SysfsPermissions : public Permissions {
public:
SysfsPermissions(const std::string& name, const std::string& attribute, mode_t perm, uid_t uid,
gid_t gid)
: Permissions(name, perm, uid, gid), attribute_(attribute) {}
bool MatchWithSubsystem(const std::string& path, const std::string& subsystem) const;
void SetPermissions(const std::string& path) const;
private:
const std::string attribute_;
};
class Subsystem {
public:
friend class SubsystemParser;
Subsystem() {}
Subsystem(std::string name) : name_(std::move(name)) {}
// Returns the full path for a uevent of a device that is a member of this subsystem,
// according to the rules parsed from ueventd.rc
std::string ParseDevPath(const Uevent& uevent) const {
std::string devname = devname_source_ == DevnameSource::DEVNAME_UEVENT_DEVNAME
? uevent.device_name
: android::base::Basename(uevent.path);
return dir_name_ + "/" + devname;
}
bool operator==(const std::string& string_name) const { return name_ == string_name; }
private:
enum class DevnameSource {
DEVNAME_UEVENT_DEVNAME,
DEVNAME_UEVENT_DEVPATH,
};
std::string name_;
std::string dir_name_ = "/dev";
DevnameSource devname_source_;
};
class DeviceHandler {
public:
friend class DeviceHandlerTester;
DeviceHandler();
DeviceHandler(std::vector<Permissions> dev_permissions,
std::vector<SysfsPermissions> sysfs_permissions, std::vector<Subsystem> subsystems,
std::set<std::string> boot_devices, bool skip_restorecon);
~DeviceHandler(){};
void HandleDeviceEvent(const Uevent& uevent);
std::vector<std::string> GetBlockDeviceSymlinks(const Uevent& uevent) const;
void set_skip_restorecon(bool value) { skip_restorecon_ = value; }
private:
bool FindPlatformDevice(std::string path, std::string* platform_device_path) const;
std::tuple<mode_t, uid_t, gid_t> GetDevicePermissions(
const std::string& path, const std::vector<std::string>& links) const;
void MakeDevice(const std::string& path, bool block, int major, int minor,
const std::vector<std::string>& links) const;
void HandleDevice(const std::string& action, const std::string& devpath, bool block, int major,
int minor, const std::vector<std::string>& links) const;
void FixupSysPermissions(const std::string& upath, const std::string& subsystem) const;
std::vector<Permissions> dev_permissions_;
std::vector<SysfsPermissions> sysfs_permissions_;
std::vector<Subsystem> subsystems_;
std::set<std::string> boot_devices_;
bool skip_restorecon_;
std::string sysfs_mount_point_;
};
// Exposed for testing
void SanitizePartitionName(std::string* string);
} // namespace init
} // namespace android
#endif
|