1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
|
/*
* Copyright (C) 2017 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#include "init_first_stage.h"
#include <stdlib.h>
#include <unistd.h>
#include <chrono>
#include <memory>
#include <set>
#include <string>
#include <vector>
#include <android-base/chrono_utils.h>
#include <android-base/file.h>
#include <android-base/logging.h>
#include <android-base/strings.h>
#include "devices.h"
#include "fs_mgr.h"
#include "fs_mgr_avb.h"
#include "uevent.h"
#include "uevent_listener.h"
#include "util.h"
using android::base::Timer;
namespace android {
namespace init {
// Class Declarations
// ------------------
class FirstStageMount {
public:
FirstStageMount();
virtual ~FirstStageMount() = default;
// The factory method to create either FirstStageMountVBootV1 or FirstStageMountVBootV2
// based on device tree configurations.
static std::unique_ptr<FirstStageMount> Create();
bool DoFirstStageMount(); // Mounts fstab entries read from device tree.
bool InitDevices();
protected:
ListenerAction HandleBlockDevice(const std::string& name, const Uevent&);
bool InitRequiredDevices();
bool InitVerityDevice(const std::string& verity_device);
bool MountPartitions();
virtual ListenerAction UeventCallback(const Uevent& uevent);
// Pure virtual functions.
virtual bool GetRequiredDevices() = 0;
virtual bool SetUpDmVerity(fstab_rec* fstab_rec) = 0;
bool need_dm_verity_;
std::unique_ptr<fstab, decltype(&fs_mgr_free_fstab)> device_tree_fstab_;
std::vector<fstab_rec*> mount_fstab_recs_;
std::set<std::string> required_devices_partition_names_;
DeviceHandler device_handler_;
UeventListener uevent_listener_;
};
class FirstStageMountVBootV1 : public FirstStageMount {
public:
FirstStageMountVBootV1() = default;
~FirstStageMountVBootV1() override = default;
protected:
bool GetRequiredDevices() override;
bool SetUpDmVerity(fstab_rec* fstab_rec) override;
};
class FirstStageMountVBootV2 : public FirstStageMount {
public:
friend void SetInitAvbVersionInRecovery();
FirstStageMountVBootV2();
~FirstStageMountVBootV2() override = default;
protected:
ListenerAction UeventCallback(const Uevent& uevent) override;
bool GetRequiredDevices() override;
bool SetUpDmVerity(fstab_rec* fstab_rec) override;
bool InitAvbHandle();
std::string device_tree_vbmeta_parts_;
FsManagerAvbUniquePtr avb_handle_;
ByNameSymlinkMap by_name_symlink_map_;
};
// Static Functions
// ----------------
static inline bool IsDtVbmetaCompatible() {
return is_android_dt_value_expected("vbmeta/compatible", "android,vbmeta");
}
static bool inline IsRecoveryMode() {
return access("/sbin/recovery", F_OK) == 0;
}
// Class Definitions
// -----------------
FirstStageMount::FirstStageMount()
: need_dm_verity_(false), device_tree_fstab_(fs_mgr_read_fstab_dt(), fs_mgr_free_fstab) {
if (!device_tree_fstab_) {
LOG(INFO) << "Failed to read fstab from device tree";
return;
}
// Stores device_tree_fstab_->recs[] into mount_fstab_recs_ (vector<fstab_rec*>)
// for easier manipulation later, e.g., range-base for loop.
for (int i = 0; i < device_tree_fstab_->num_entries; i++) {
mount_fstab_recs_.push_back(&device_tree_fstab_->recs[i]);
}
}
std::unique_ptr<FirstStageMount> FirstStageMount::Create() {
if (IsDtVbmetaCompatible()) {
return std::make_unique<FirstStageMountVBootV2>();
} else {
return std::make_unique<FirstStageMountVBootV1>();
}
}
bool FirstStageMount::DoFirstStageMount() {
// Nothing to mount.
if (mount_fstab_recs_.empty()) return true;
if (!InitDevices()) return false;
if (!MountPartitions()) return false;
return true;
}
bool FirstStageMount::InitDevices() {
return GetRequiredDevices() && InitRequiredDevices();
}
// Creates devices with uevent->partition_name matching one in the member variable
// required_devices_partition_names_. Found partitions will then be removed from it
// for the subsequent member function to check which devices are NOT created.
bool FirstStageMount::InitRequiredDevices() {
if (required_devices_partition_names_.empty()) {
return true;
}
if (need_dm_verity_) {
const std::string dm_path = "/devices/virtual/misc/device-mapper";
bool found = false;
auto dm_callback = [this, &dm_path, &found](const Uevent& uevent) {
if (uevent.path == dm_path) {
device_handler_.HandleDeviceEvent(uevent);
found = true;
return ListenerAction::kStop;
}
return ListenerAction::kContinue;
};
uevent_listener_.RegenerateUeventsForPath("/sys" + dm_path, dm_callback);
if (!found) {
LOG(INFO) << "device-mapper device not found in /sys, waiting for its uevent";
Timer t;
uevent_listener_.Poll(dm_callback, 10s);
LOG(INFO) << "Wait for device-mapper returned after " << t;
}
if (!found) {
LOG(ERROR) << "device-mapper device not found after polling timeout";
return false;
}
}
auto uevent_callback = [this](const Uevent& uevent) { return UeventCallback(uevent); };
uevent_listener_.RegenerateUevents(uevent_callback);
// UeventCallback() will remove found partitions from required_devices_partition_names_.
// So if it isn't empty here, it means some partitions are not found.
if (!required_devices_partition_names_.empty()) {
LOG(INFO) << __PRETTY_FUNCTION__
<< ": partition(s) not found in /sys, waiting for their uevent(s): "
<< android::base::Join(required_devices_partition_names_, ", ");
Timer t;
uevent_listener_.Poll(uevent_callback, 10s);
LOG(INFO) << "Wait for partitions returned after " << t;
}
if (!required_devices_partition_names_.empty()) {
LOG(ERROR) << __PRETTY_FUNCTION__ << ": partition(s) not found after polling timeout: "
<< android::base::Join(required_devices_partition_names_, ", ");
return false;
}
return true;
}
ListenerAction FirstStageMount::HandleBlockDevice(const std::string& name, const Uevent& uevent) {
// Matches partition name to create device nodes.
// Both required_devices_partition_names_ and uevent->partition_name have A/B
// suffix when A/B is used.
auto iter = required_devices_partition_names_.find(name);
if (iter != required_devices_partition_names_.end()) {
LOG(VERBOSE) << __PRETTY_FUNCTION__ << ": found partition: " << *iter;
required_devices_partition_names_.erase(iter);
device_handler_.HandleDeviceEvent(uevent);
if (required_devices_partition_names_.empty()) {
return ListenerAction::kStop;
} else {
return ListenerAction::kContinue;
}
}
return ListenerAction::kContinue;
}
ListenerAction FirstStageMount::UeventCallback(const Uevent& uevent) {
// Ignores everything that is not a block device.
if (uevent.subsystem != "block") {
return ListenerAction::kContinue;
}
if (!uevent.partition_name.empty()) {
return HandleBlockDevice(uevent.partition_name, uevent);
} else {
size_t base_idx = uevent.path.rfind('/');
if (base_idx != std::string::npos) {
return HandleBlockDevice(uevent.path.substr(base_idx + 1), uevent);
}
}
// Not found a partition or find an unneeded partition, continue to find others.
return ListenerAction::kContinue;
}
// Creates "/dev/block/dm-XX" for dm-verity by running coldboot on /sys/block/dm-XX.
bool FirstStageMount::InitVerityDevice(const std::string& verity_device) {
const std::string device_name(basename(verity_device.c_str()));
const std::string syspath = "/sys/block/" + device_name;
bool found = false;
auto verity_callback = [&device_name, &verity_device, this, &found](const Uevent& uevent) {
if (uevent.device_name == device_name) {
LOG(VERBOSE) << "Creating dm-verity device : " << verity_device;
device_handler_.HandleDeviceEvent(uevent);
found = true;
return ListenerAction::kStop;
}
return ListenerAction::kContinue;
};
uevent_listener_.RegenerateUeventsForPath(syspath, verity_callback);
if (!found) {
LOG(INFO) << "dm-verity device not found in /sys, waiting for its uevent";
Timer t;
uevent_listener_.Poll(verity_callback, 10s);
LOG(INFO) << "wait for dm-verity device returned after " << t;
}
if (!found) {
LOG(ERROR) << "dm-verity device not found after polling timeout";
return false;
}
return true;
}
bool FirstStageMount::MountPartitions() {
for (auto fstab_rec : mount_fstab_recs_) {
if (!SetUpDmVerity(fstab_rec)) {
PLOG(ERROR) << "Failed to setup verity for '" << fstab_rec->mount_point << "'";
return false;
}
if (fs_mgr_do_mount_one(fstab_rec)) {
PLOG(ERROR) << "Failed to mount '" << fstab_rec->mount_point << "'";
return false;
}
}
return true;
}
bool FirstStageMountVBootV1::GetRequiredDevices() {
std::string verity_loc_device;
need_dm_verity_ = false;
for (auto fstab_rec : mount_fstab_recs_) {
// Don't allow verifyatboot in the first stage.
if (fs_mgr_is_verifyatboot(fstab_rec)) {
LOG(ERROR) << "Partitions can't be verified at boot";
return false;
}
// Checks for verified partitions.
if (fs_mgr_is_verified(fstab_rec)) {
need_dm_verity_ = true;
}
// Checks if verity metadata is on a separate partition. Note that it is
// not partition specific, so there must be only one additional partition
// that carries verity state.
if (fstab_rec->verity_loc) {
if (verity_loc_device.empty()) {
verity_loc_device = fstab_rec->verity_loc;
} else if (verity_loc_device != fstab_rec->verity_loc) {
LOG(ERROR) << "More than one verity_loc found: " << verity_loc_device << ", "
<< fstab_rec->verity_loc;
return false;
}
}
}
// Includes the partition names of fstab records and verity_loc_device (if any).
// Notes that fstab_rec->blk_device has A/B suffix updated by fs_mgr when A/B is used.
for (auto fstab_rec : mount_fstab_recs_) {
required_devices_partition_names_.emplace(basename(fstab_rec->blk_device));
}
if (!verity_loc_device.empty()) {
required_devices_partition_names_.emplace(basename(verity_loc_device.c_str()));
}
return true;
}
bool FirstStageMountVBootV1::SetUpDmVerity(fstab_rec* fstab_rec) {
if (fs_mgr_is_verified(fstab_rec)) {
int ret = fs_mgr_setup_verity(fstab_rec, false /* wait_for_verity_dev */);
switch (ret) {
case FS_MGR_SETUP_VERITY_SKIPPED:
case FS_MGR_SETUP_VERITY_DISABLED:
LOG(INFO) << "Verity disabled/skipped for '" << fstab_rec->mount_point << "'";
return true;
case FS_MGR_SETUP_VERITY_SUCCESS:
// The exact block device name (fstab_rec->blk_device) is changed to
// "/dev/block/dm-XX". Needs to create it because ueventd isn't started in init
// first stage.
return InitVerityDevice(fstab_rec->blk_device);
default:
return false;
}
}
return true; // Returns true to mount the partition.
}
// FirstStageMountVBootV2 constructor.
// Gets the vbmeta partitions from device tree.
// /{
// firmware {
// android {
// vbmeta {
// compatible = "android,vbmeta";
// parts = "vbmeta,boot,system,vendor"
// };
// };
// };
// }
FirstStageMountVBootV2::FirstStageMountVBootV2() : avb_handle_(nullptr) {
if (!read_android_dt_file("vbmeta/parts", &device_tree_vbmeta_parts_)) {
PLOG(ERROR) << "Failed to read vbmeta/parts from device tree";
return;
}
}
bool FirstStageMountVBootV2::GetRequiredDevices() {
need_dm_verity_ = false;
// fstab_rec->blk_device has A/B suffix.
for (auto fstab_rec : mount_fstab_recs_) {
if (fs_mgr_is_avb(fstab_rec)) {
need_dm_verity_ = true;
}
required_devices_partition_names_.emplace(basename(fstab_rec->blk_device));
}
// libavb verifies AVB metadata on all verified partitions at once.
// e.g., The device_tree_vbmeta_parts_ will be "vbmeta,boot,system,vendor"
// for libavb to verify metadata, even if there is only /vendor in the
// above mount_fstab_recs_.
if (need_dm_verity_) {
if (device_tree_vbmeta_parts_.empty()) {
LOG(ERROR) << "Missing vbmeta parts in device tree";
return false;
}
std::vector<std::string> partitions = android::base::Split(device_tree_vbmeta_parts_, ",");
std::string ab_suffix = fs_mgr_get_slot_suffix();
for (const auto& partition : partitions) {
// required_devices_partition_names_ is of type std::set so it's not an issue
// to emplace a partition twice. e.g., /vendor might be in both places:
// - device_tree_vbmeta_parts_ = "vbmeta,boot,system,vendor"
// - mount_fstab_recs_: /vendor_a
required_devices_partition_names_.emplace(partition + ab_suffix);
}
}
return true;
}
ListenerAction FirstStageMountVBootV2::UeventCallback(const Uevent& uevent) {
// Check if this uevent corresponds to one of the required partitions and store its symlinks if
// so, in order to create FsManagerAvbHandle later.
// Note that the parent callback removes partitions from the list of required partitions
// as it finds them, so this must happen first.
if (!uevent.partition_name.empty() &&
required_devices_partition_names_.find(uevent.partition_name) !=
required_devices_partition_names_.end()) {
// GetBlockDeviceSymlinks() will return three symlinks at most, depending on
// the content of uevent. by-name symlink will be at [0] if uevent->partition_name
// is not empty. e.g.,
// - /dev/block/platform/soc.0/f9824900.sdhci/by-name/modem
// - /dev/block/platform/soc.0/f9824900.sdhci/by-num/p1
// - /dev/block/platform/soc.0/f9824900.sdhci/mmcblk0p1
std::vector<std::string> links = device_handler_.GetBlockDeviceSymlinks(uevent);
if (!links.empty()) {
auto[it, inserted] = by_name_symlink_map_.emplace(uevent.partition_name, links[0]);
if (!inserted) {
LOG(ERROR) << "Partition '" << uevent.partition_name
<< "' already existed in the by-name symlink map with a value of '"
<< it->second << "', new value '" << links[0] << "' will be ignored.";
}
}
}
return FirstStageMount::UeventCallback(uevent);
}
bool FirstStageMountVBootV2::SetUpDmVerity(fstab_rec* fstab_rec) {
if (fs_mgr_is_avb(fstab_rec)) {
if (!InitAvbHandle()) return false;
SetUpAvbHashtreeResult hashtree_result =
avb_handle_->SetUpAvbHashtree(fstab_rec, false /* wait_for_verity_dev */);
switch (hashtree_result) {
case SetUpAvbHashtreeResult::kDisabled:
return true; // Returns true to mount the partition.
case SetUpAvbHashtreeResult::kSuccess:
// The exact block device name (fstab_rec->blk_device) is changed to
// "/dev/block/dm-XX". Needs to create it because ueventd isn't started in init
// first stage.
return InitVerityDevice(fstab_rec->blk_device);
default:
return false;
}
}
return true; // Returns true to mount the partition.
}
bool FirstStageMountVBootV2::InitAvbHandle() {
if (avb_handle_) return true; // Returns true if the handle is already initialized.
if (by_name_symlink_map_.empty()) {
LOG(ERROR) << "by_name_symlink_map_ is empty";
return false;
}
avb_handle_ = FsManagerAvbHandle::Open(std::move(by_name_symlink_map_));
by_name_symlink_map_.clear(); // Removes all elements after the above std::move().
if (!avb_handle_) {
PLOG(ERROR) << "Failed to open FsManagerAvbHandle";
return false;
}
// Sets INIT_AVB_VERSION here for init to set ro.boot.avb_version in the second stage.
setenv("INIT_AVB_VERSION", avb_handle_->avb_version().c_str(), 1);
return true;
}
// Public functions
// ----------------
// Mounts partitions specified by fstab in device tree.
bool DoFirstStageMount() {
// Skips first stage mount if we're in recovery mode.
if (IsRecoveryMode()) {
LOG(INFO) << "First stage mount skipped (recovery mode)";
return true;
}
// Firstly checks if device tree fstab entries are compatible.
if (!is_android_dt_value_expected("fstab/compatible", "android,fstab")) {
LOG(INFO) << "First stage mount skipped (missing/incompatible fstab in device tree)";
return true;
}
std::unique_ptr<FirstStageMount> handle = FirstStageMount::Create();
if (!handle) {
LOG(ERROR) << "Failed to create FirstStageMount";
return false;
}
return handle->DoFirstStageMount();
}
void SetInitAvbVersionInRecovery() {
if (!IsRecoveryMode()) {
LOG(INFO) << "Skipped setting INIT_AVB_VERSION (not in recovery mode)";
return;
}
if (!IsDtVbmetaCompatible()) {
LOG(INFO) << "Skipped setting INIT_AVB_VERSION (not vbmeta compatible)";
return;
}
// Initializes required devices for the subsequent FsManagerAvbHandle::Open()
// to verify AVB metadata on all partitions in the verified chain.
// We only set INIT_AVB_VERSION when the AVB verification succeeds, i.e., the
// Open() function returns a valid handle.
// We don't need to mount partitions here in recovery mode.
FirstStageMountVBootV2 avb_first_mount;
if (!avb_first_mount.InitDevices()) {
LOG(ERROR) << "Failed to init devices for INIT_AVB_VERSION";
return;
}
FsManagerAvbUniquePtr avb_handle =
FsManagerAvbHandle::Open(std::move(avb_first_mount.by_name_symlink_map_));
if (!avb_handle) {
PLOG(ERROR) << "Failed to open FsManagerAvbHandle for INIT_AVB_VERSION";
return;
}
setenv("INIT_AVB_VERSION", avb_handle->avb_version().c_str(), 1);
}
} // namespace init
} // namespace android
|