1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
|
/*
* Copyright (C) 2018 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#include "modalias_handler.h"
#include <fnmatch.h>
#include <sys/syscall.h>
#include <algorithm>
#include <functional>
#include <string>
#include <vector>
#include <android-base/chrono_utils.h>
#include <android-base/logging.h>
#include <android-base/unique_fd.h>
#include "parser.h"
namespace android {
namespace init {
Result<Success> ModaliasHandler::ParseDepCallback(std::vector<std::string>&& args) {
std::vector<std::string> deps;
// Set first item as our modules path
std::string::size_type pos = args[0].find(':');
if (pos != std::string::npos) {
deps.emplace_back(args[0].substr(0, pos));
} else {
return Error() << "dependency lines must start with name followed by ':'";
}
// Remaining items are dependencies of our module
for (auto arg = args.begin() + 1; arg != args.end(); ++arg) {
deps.push_back(*arg);
}
// Key is striped module name to match names in alias file
std::size_t start = args[0].find_last_of("/");
std::size_t end = args[0].find(".ko:");
if ((end - start) <= 1) return Error() << "malformed dependency line";
auto mod_name = args[0].substr(start + 1, (end - start) - 1);
// module names can have '-', but their file names will have '_'
std::replace(mod_name.begin(), mod_name.end(), '-', '_');
this->module_deps_[mod_name] = deps;
return Success();
}
Result<Success> ModaliasHandler::ParseAliasCallback(std::vector<std::string>&& args) {
auto it = args.begin();
const std::string& type = *it++;
if (type != "alias") {
return Error() << "we only handle alias lines, got: " << type;
}
if (args.size() != 3) {
return Error() << "alias lines must have 3 entries";
}
std::string& alias = *it++;
std::string& module_name = *it++;
this->module_aliases_.emplace_back(alias, module_name);
return Success();
}
ModaliasHandler::ModaliasHandler() {
using namespace std::placeholders;
static const std::string base_paths[] = {
"/vendor/lib/modules/",
"/lib/modules/",
"/odm/lib/modules/",
};
Parser alias_parser;
auto alias_callback = std::bind(&ModaliasHandler::ParseAliasCallback, this, _1);
alias_parser.AddSingleLineParser("alias", alias_callback);
for (const auto& base_path : base_paths) alias_parser.ParseConfig(base_path + "modules.alias");
Parser dep_parser;
auto dep_callback = std::bind(&ModaliasHandler::ParseDepCallback, this, _1);
dep_parser.AddSingleLineParser("", dep_callback);
for (const auto& base_path : base_paths) dep_parser.ParseConfig(base_path + "modules.dep");
}
Result<Success> ModaliasHandler::Insmod(const std::string& path_name, const std::string& args) {
base::unique_fd fd(
TEMP_FAILURE_RETRY(open(path_name.c_str(), O_RDONLY | O_NOFOLLOW | O_CLOEXEC)));
if (fd == -1) return ErrnoError() << "Could not open module '" << path_name << "'";
int ret = syscall(__NR_finit_module, fd.get(), args.c_str(), 0);
if (ret != 0) {
if (errno == EEXIST) {
// Module already loaded
return Success();
}
return ErrnoError() << "Failed to insmod '" << path_name << "' with args '" << args << "'";
}
LOG(INFO) << "Loaded kernel module " << path_name;
return Success();
}
Result<Success> ModaliasHandler::InsmodWithDeps(const std::string& module_name,
const std::string& args) {
if (module_name.empty()) {
return Error() << "Need valid module name";
}
auto it = module_deps_.find(module_name);
if (it == module_deps_.end()) {
return Error() << "Module '" << module_name << "' not in dependency file";
}
auto& dependencies = it->second;
// load module dependencies in reverse order
for (auto dep = dependencies.rbegin(); dep != dependencies.rend() - 1; ++dep) {
if (auto result = Insmod(*dep, ""); !result) return result;
}
// load target module itself with args
return Insmod(dependencies[0], args);
}
void ModaliasHandler::HandleModaliasEvent(const Uevent& uevent) {
if (uevent.modalias.empty()) return;
for (const auto& [alias, module] : module_aliases_) {
if (fnmatch(alias.c_str(), uevent.modalias.c_str(), 0) != 0) continue; // Keep looking
LOG(DEBUG) << "Loading kernel module '" << module << "' for alias '" << uevent.modalias
<< "'";
if (auto result = InsmodWithDeps(module, ""); !result) {
LOG(ERROR) << "Cannot load module: " << result.error();
// try another one since there may be another match
continue;
}
// loading was successful
return;
}
}
} // namespace init
} // namespace android
|