1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
|
/*
* Copyright (C) 2017 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
// This file contains classes for returning a successful result along with an optional
// arbitrarily typed return value or for returning a failure result along with an optional string
// indicating why the function failed.
// There are 3 classes that implement this functionality and one additional helper type.
//
// Result<T> either contains a member of type T that can be accessed using similar semantics as
// std::optional<T> or it contains a ResultError describing an error, which can be accessed via
// Result<T>::error().
//
// ResultError is a type that contains both a std::string describing the error and a copy of errno
// from when the error occurred. ResultError can be used in an ostream directly to print its
// string value.
//
// Success is a typedef that aids in creating Result<T> that do not contain a return value.
// Result<Success> is the correct return type for a function that either returns successfully or
// returns an error value. Returning Success() from a function that returns Result<Success> is the
// correct way to indicate that a function without a return type has completed successfully.
//
// A successful Result<T> is constructed implicitly from any type that can be implicitly converted
// to T or from the constructor arguments for T. This allows you to return a type T directly from
// a function that returns Result<T>.
//
// Error and ErrnoError are used to construct a Result<T> that has failed. The Error class takes
// an ostream as an input and are implicitly cast to a Result<T> containing that failure.
// ErrnoError() is a helper function to create an Error class that appends ": " + strerror(errno)
// to the end of the failure string to aid in interacting with C APIs. Alternatively, an errno
// value can be directly specified via the Error() constructor.
//
// ResultError can be used in the ostream when using Error to construct a Result<T>. In this case,
// the string that the ResultError takes is passed through the stream normally, but the errno is
// passed to the Result<T>. This can be used to pass errno from a failing C function up multiple
// callers.
//
// ResultError can also directly construct a Result<T>. This is particularly useful if you have a
// function that return Result<T> but you have a Result<U> and want to return its error. In this
// case, you can return the .error() from the Result<U> to construct the Result<T>.
// An example of how to use these is below:
// Result<U> CalculateResult(const T& input) {
// U output;
// if (!SomeOtherCppFunction(input, &output)) {
// return Error() << "SomeOtherCppFunction(" << input << ") failed";
// }
// if (!c_api_function(output)) {
// return ErrnoError() << "c_api_function(" << output << ") failed";
// }
// return output;
// }
//
// auto output = CalculateResult(input);
// if (!output) return Error() << "CalculateResult failed: " << output.error();
// UseOutput(*output);
#ifndef _INIT_RESULT_H
#define _INIT_RESULT_H
#include <errno.h>
#include <sstream>
#include <string>
#include <variant>
namespace android {
namespace init {
struct ResultError {
template <typename T>
ResultError(T&& error_string, int error_errno)
: error_string(std::forward<T>(error_string)), error_errno(error_errno) {}
std::string error_string;
int error_errno;
};
inline std::ostream& operator<<(std::ostream& os, const ResultError& t) {
os << t.error_string;
return os;
}
inline std::ostream& operator<<(std::ostream& os, ResultError&& t) {
os << std::move(t.error_string);
return os;
}
class Error {
public:
Error() : errno_(0), append_errno_(false) {}
Error(int errno_to_append) : errno_(errno_to_append), append_errno_(true) {}
template <typename T>
Error&& operator<<(T&& t) {
ss_ << std::forward<T>(t);
return std::move(*this);
}
Error&& operator<<(const ResultError& result_error) {
ss_ << result_error.error_string;
errno_ = result_error.error_errno;
return std::move(*this);
}
Error&& operator<<(ResultError&& result_error) {
ss_ << std::move(result_error.error_string);
errno_ = result_error.error_errno;
return std::move(*this);
}
const std::string str() const {
std::string str = ss_.str();
if (append_errno_) {
if (str.empty()) {
return strerror(errno_);
}
return str + ": " + strerror(errno_);
}
return str;
}
int get_errno() const { return errno_; }
Error(const Error&) = delete;
Error(Error&&) = delete;
Error& operator=(const Error&) = delete;
Error& operator=(Error&&) = delete;
private:
std::stringstream ss_;
int errno_;
bool append_errno_;
};
inline Error ErrnoError() {
return Error(errno);
}
template <typename T>
class Result {
public:
Result() {}
template <typename U, typename... V,
typename = std::enable_if_t<!(std::is_same_v<std::decay_t<U>, Result<T>> &&
sizeof...(V) == 0)>>
Result(U&& result, V&&... results)
: contents_(std::in_place_index_t<0>(), std::forward<U>(result),
std::forward<V>(results)...) {}
Result(Error&& error) : contents_(std::in_place_index_t<1>(), error.str(), error.get_errno()) {}
Result(const ResultError& result_error)
: contents_(std::in_place_index_t<1>(), result_error.error_string,
result_error.error_errno) {}
Result(ResultError&& result_error)
: contents_(std::in_place_index_t<1>(), std::move(result_error.error_string),
result_error.error_errno) {}
bool has_value() const { return contents_.index() == 0; }
T& value() & { return std::get<0>(contents_); }
const T& value() const & { return std::get<0>(contents_); }
T&& value() && { return std::get<0>(std::move(contents_)); }
const T&& value() const && { return std::get<0>(std::move(contents_)); }
const ResultError& error() const & { return std::get<1>(contents_); }
ResultError&& error() && { return std::get<1>(std::move(contents_)); }
const ResultError&& error() const && { return std::get<1>(std::move(contents_)); }
const std::string& error_string() const & { return std::get<1>(contents_).error_string; }
std::string&& error_string() && { return std::get<1>(std::move(contents_)).error_string; }
const std::string&& error_string() const && {
return std::get<1>(std::move(contents_)).error_string;
}
int error_errno() const { return std::get<1>(contents_).error_errno; }
explicit operator bool() const { return has_value(); }
T& operator*() & { return value(); }
const T& operator*() const & { return value(); }
T&& operator*() && { return std::move(value()); }
const T&& operator*() const && { return std::move(value()); }
T* operator->() { return &value(); }
const T* operator->() const { return &value(); }
private:
std::variant<T, ResultError> contents_;
};
using Success = std::monostate;
} // namespace init
} // namespace android
#endif
|