1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
|
/*
* Copyright (C) 2017 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#include "subcontext.h"
#include <fcntl.h>
#include <poll.h>
#include <sys/socket.h>
#include <unistd.h>
#include <android-base/file.h>
#include <android-base/logging.h>
#include <android-base/strings.h>
#include <selinux/android.h>
#include "action.h"
#include "util.h"
#if defined(__ANDROID__)
#include "property_service.h"
#include "selinux.h"
#else
#include "host_init_stubs.h"
#endif
using android::base::GetExecutablePath;
using android::base::Join;
using android::base::Socketpair;
using android::base::Split;
using android::base::StartsWith;
using android::base::unique_fd;
namespace android {
namespace init {
const std::string kInitContext = "u:r:init:s0";
const std::string kVendorContext = "u:r:vendor_init:s0";
const char* const paths_and_secontexts[2][2] = {
{"/vendor", kVendorContext.c_str()},
{"/odm", kVendorContext.c_str()},
};
namespace {
constexpr size_t kBufferSize = 4096;
Result<std::string> ReadMessage(int socket) {
char buffer[kBufferSize] = {};
auto result = TEMP_FAILURE_RETRY(recv(socket, buffer, sizeof(buffer), 0));
if (result <= 0) {
return ErrnoError();
}
return std::string(buffer, result);
}
template <typename T>
Result<Success> SendMessage(int socket, const T& message) {
std::string message_string;
if (!message.SerializeToString(&message_string)) {
return Error() << "Unable to serialize message";
}
if (message_string.size() > kBufferSize) {
return Error() << "Serialized message too long to send";
}
if (auto result =
TEMP_FAILURE_RETRY(send(socket, message_string.c_str(), message_string.size(), 0));
result != static_cast<long>(message_string.size())) {
return ErrnoError() << "send() failed to send message contents";
}
return Success();
}
std::vector<std::pair<std::string, std::string>> properties_to_set;
uint32_t SubcontextPropertySet(const std::string& name, const std::string& value) {
properties_to_set.emplace_back(name, value);
return 0;
}
class SubcontextProcess {
public:
SubcontextProcess(const KeywordFunctionMap* function_map, std::string context, int init_fd)
: function_map_(function_map), context_(std::move(context)), init_fd_(init_fd){};
void MainLoop();
private:
void RunCommand(const SubcontextCommand::ExecuteCommand& execute_command,
SubcontextReply* reply) const;
void ExpandArgs(const SubcontextCommand::ExpandArgsCommand& expand_args_command,
SubcontextReply* reply) const;
const KeywordFunctionMap* function_map_;
const std::string context_;
const int init_fd_;
};
void SubcontextProcess::RunCommand(const SubcontextCommand::ExecuteCommand& execute_command,
SubcontextReply* reply) const {
// Need to use ArraySplice instead of this code.
auto args = std::vector<std::string>();
for (const auto& string : execute_command.args()) {
args.emplace_back(string);
}
auto map_result = function_map_->FindFunction(args);
Result<Success> result;
if (!map_result) {
result = Error() << "Cannot find command: " << map_result.error();
} else {
result = RunBuiltinFunction(map_result->second, args, context_);
}
for (const auto& [name, value] : properties_to_set) {
auto property = reply->add_properties_to_set();
property->set_name(name);
property->set_value(value);
}
properties_to_set.clear();
if (result) {
reply->set_success(true);
} else {
auto* failure = reply->mutable_failure();
failure->set_error_string(result.error_string());
failure->set_error_errno(result.error_errno());
}
}
void SubcontextProcess::ExpandArgs(const SubcontextCommand::ExpandArgsCommand& expand_args_command,
SubcontextReply* reply) const {
for (const auto& arg : expand_args_command.args()) {
auto expanded_prop = std::string{};
if (!expand_props(arg, &expanded_prop)) {
auto* failure = reply->mutable_failure();
failure->set_error_string("Failed to expand '" + arg + "'");
failure->set_error_errno(0);
return;
} else {
auto* expand_args_reply = reply->mutable_expand_args_reply();
expand_args_reply->add_expanded_args(expanded_prop);
}
}
}
void SubcontextProcess::MainLoop() {
pollfd ufd[1];
ufd[0].events = POLLIN;
ufd[0].fd = init_fd_;
while (true) {
ufd[0].revents = 0;
int nr = TEMP_FAILURE_RETRY(poll(ufd, arraysize(ufd), -1));
if (nr == 0) continue;
if (nr < 0) {
PLOG(FATAL) << "poll() of subcontext socket failed, continuing";
}
auto init_message = ReadMessage(init_fd_);
if (!init_message) {
LOG(FATAL) << "Could not read message from init: " << init_message.error();
}
auto subcontext_command = SubcontextCommand();
if (!subcontext_command.ParseFromString(*init_message)) {
LOG(FATAL) << "Unable to parse message from init";
}
auto reply = SubcontextReply();
switch (subcontext_command.command_case()) {
case SubcontextCommand::kExecuteCommand: {
RunCommand(subcontext_command.execute_command(), &reply);
break;
}
case SubcontextCommand::kExpandArgsCommand: {
ExpandArgs(subcontext_command.expand_args_command(), &reply);
break;
}
default:
LOG(FATAL) << "Unknown message type from init: "
<< subcontext_command.command_case();
}
if (auto result = SendMessage(init_fd_, reply); !result) {
LOG(FATAL) << "Failed to send message to init: " << result.error();
}
}
}
} // namespace
int SubcontextMain(int argc, char** argv, const KeywordFunctionMap* function_map) {
if (argc < 4) LOG(FATAL) << "Fewer than 4 args specified to subcontext (" << argc << ")";
auto context = std::string(argv[2]);
auto init_fd = std::atoi(argv[3]);
SelabelInitialize();
property_set = SubcontextPropertySet;
auto subcontext_process = SubcontextProcess(function_map, context, init_fd);
subcontext_process.MainLoop();
return 0;
}
void Subcontext::Fork() {
unique_fd subcontext_socket;
if (!Socketpair(AF_UNIX, SOCK_SEQPACKET | SOCK_CLOEXEC, 0, &socket_, &subcontext_socket)) {
LOG(FATAL) << "Could not create socket pair to communicate to subcontext";
return;
}
auto result = fork();
if (result == -1) {
LOG(FATAL) << "Could not fork subcontext";
} else if (result == 0) {
socket_.reset();
// We explicitly do not use O_CLOEXEC here, such that we can reference this FD by number
// in the subcontext process after we exec.
int child_fd = dup(subcontext_socket);
if (child_fd < 0) {
PLOG(FATAL) << "Could not dup child_fd";
}
if (setexeccon(context_.c_str()) < 0) {
PLOG(FATAL) << "Could not set execcon for '" << context_ << "'";
}
auto init_path = GetExecutablePath();
auto child_fd_string = std::to_string(child_fd);
const char* args[] = {init_path.c_str(), "subcontext", context_.c_str(),
child_fd_string.c_str(), nullptr};
execv(init_path.data(), const_cast<char**>(args));
PLOG(FATAL) << "Could not execv subcontext init";
} else {
subcontext_socket.reset();
pid_ = result;
LOG(INFO) << "Forked subcontext for '" << context_ << "' with pid " << pid_;
}
}
void Subcontext::Restart() {
LOG(ERROR) << "Restarting subcontext '" << context_ << "'";
if (pid_) {
kill(pid_, SIGKILL);
}
pid_ = 0;
socket_.reset();
Fork();
}
Result<SubcontextReply> Subcontext::TransmitMessage(const SubcontextCommand& subcontext_command) {
if (auto result = SendMessage(socket_, subcontext_command); !result) {
Restart();
return ErrnoError() << "Failed to send message to subcontext";
}
auto subcontext_message = ReadMessage(socket_);
if (!subcontext_message) {
Restart();
return Error() << "Failed to receive result from subcontext: " << subcontext_message.error();
}
auto subcontext_reply = SubcontextReply{};
if (!subcontext_reply.ParseFromString(*subcontext_message)) {
Restart();
return Error() << "Unable to parse message from subcontext";
}
return subcontext_reply;
}
Result<Success> Subcontext::Execute(const std::vector<std::string>& args) {
auto subcontext_command = SubcontextCommand();
std::copy(
args.begin(), args.end(),
RepeatedPtrFieldBackInserter(subcontext_command.mutable_execute_command()->mutable_args()));
auto subcontext_reply = TransmitMessage(subcontext_command);
if (!subcontext_reply) {
return subcontext_reply.error();
}
for (const auto& property : subcontext_reply->properties_to_set()) {
ucred cr = {.pid = pid_, .uid = 0, .gid = 0};
std::string error;
if (HandlePropertySet(property.name(), property.value(), context_, cr, &error) != 0) {
LOG(ERROR) << "Subcontext init could not set '" << property.name() << "' to '"
<< property.value() << "': " << error;
}
}
if (subcontext_reply->reply_case() == SubcontextReply::kFailure) {
auto& failure = subcontext_reply->failure();
return ResultError(failure.error_string(), failure.error_errno());
}
if (subcontext_reply->reply_case() != SubcontextReply::kSuccess) {
return Error() << "Unexpected message type from subcontext: "
<< subcontext_reply->reply_case();
}
return Success();
}
Result<std::vector<std::string>> Subcontext::ExpandArgs(const std::vector<std::string>& args) {
auto subcontext_command = SubcontextCommand{};
std::copy(args.begin(), args.end(),
RepeatedPtrFieldBackInserter(
subcontext_command.mutable_expand_args_command()->mutable_args()));
auto subcontext_reply = TransmitMessage(subcontext_command);
if (!subcontext_reply) {
return subcontext_reply.error();
}
if (subcontext_reply->reply_case() == SubcontextReply::kFailure) {
auto& failure = subcontext_reply->failure();
return ResultError(failure.error_string(), failure.error_errno());
}
if (subcontext_reply->reply_case() != SubcontextReply::kExpandArgsReply) {
return Error() << "Unexpected message type from subcontext: "
<< subcontext_reply->reply_case();
}
auto& reply = subcontext_reply->expand_args_reply();
auto expanded_args = std::vector<std::string>{};
for (const auto& string : reply.expanded_args()) {
expanded_args.emplace_back(string);
}
return expanded_args;
}
static std::vector<Subcontext> subcontexts;
static bool shutting_down;
std::vector<Subcontext>* InitializeSubcontexts() {
if (SelinuxHasVendorInit()) {
for (const auto& [path_prefix, secontext] : paths_and_secontexts) {
subcontexts.emplace_back(path_prefix, secontext);
}
}
return &subcontexts;
}
bool SubcontextChildReap(pid_t pid) {
for (auto& subcontext : subcontexts) {
if (subcontext.pid() == pid) {
if (!shutting_down) {
subcontext.Restart();
}
return true;
}
}
return false;
}
void SubcontextTerminate() {
shutting_down = true;
for (auto& subcontext : subcontexts) {
kill(subcontext.pid(), SIGTERM);
}
}
} // namespace init
} // namespace android
|