summaryrefslogtreecommitdiffstats
blob: 680944546aba18bc9cd6d7283cee3fdd35cdf24b (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
/*
 * Copyright (C) 2010 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include "ueventd.h"

#include <ctype.h>
#include <fcntl.h>
#include <signal.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <sys/wait.h>

#include <set>
#include <thread>

#include <android-base/chrono_utils.h>
#include <android-base/logging.h>
#include <android-base/properties.h>
#include <fstab/fstab.h>
#include <selinux/android.h>
#include <selinux/selinux.h>

#include "devices.h"
#include "firmware_handler.h"
#include "log.h"
#include "selinux.h"
#include "uevent_listener.h"
#include "ueventd_parser.h"
#include "util.h"

// At a high level, ueventd listens for uevent messages generated by the kernel through a netlink
// socket.  When ueventd receives such a message it handles it by taking appropriate actions,
// which can typically be creating a device node in /dev, setting file permissions, setting selinux
// labels, etc.
// Ueventd also handles loading of firmware that the kernel requests, and creates symlinks for block
// and character devices.

// When ueventd starts, it regenerates uevents for all currently registered devices by traversing
// /sys and writing 'add' to each 'uevent' file that it finds.  This causes the kernel to generate
// and resend uevent messages for all of the currently registered devices.  This is done, because
// ueventd would not have been running when these devices were registered and therefore was unable
// to receive their uevent messages and handle them appropriately.  This process is known as
// 'cold boot'.

// 'init' currently waits synchronously on the cold boot process of ueventd before it continues
// its boot process.  For this reason, cold boot should be as quick as possible.  One way to achieve
// a speed up here is to parallelize the handling of ueventd messages, which consume the bulk of the
// time during cold boot.

// Handling of uevent messages has two unique properties:
// 1) It can be done in isolation; it doesn't need to read or write any status once it is started.
// 2) It uses setegid() and setfscreatecon() so either care (aka locking) must be taken to ensure
//    that no file system operations are done while the uevent process has an abnormal egid or
//    fscreatecon or this handling must happen in a separate process.
// Given the above two properties, it is best to fork() subprocesses to handle the uevents.  This
// reduces the overhead and complexity that would be required in a solution with threads and locks.
// In testing, a racy multithreaded solution has the same performance as the fork() solution, so
// there is no reason to deal with the complexity of the former.

// One other important caveat during the boot process is the handling of SELinux restorecon.
// Since many devices have child devices, calling selinux_android_restorecon() recursively for each
// device when its uevent is handled, results in multiple restorecon operations being done on a
// given file.  It is more efficient to simply do restorecon recursively on /sys during cold boot,
// than to do restorecon on each device as its uevent is handled.  This only applies to cold boot;
// once that has completed, restorecon is done for each device as its uevent is handled.

// With all of the above considered, the cold boot process has the below steps:
// 1) ueventd regenerates uevents by doing the /sys traversal and listens to the netlink socket for
//    the generated uevents.  It writes these uevents into a queue represented by a vector.
//
// 2) ueventd forks 'n' separate uevent handler subprocesses and has each of them to handle the
//    uevents in the queue based on a starting offset (their process number) and a stride (the total
//    number of processes).  Note that no IPC happens at this point and only const functions from
//    DeviceHandler should be called from this context.
//
// 3) In parallel to the subprocesses handling the uevents, the main thread of ueventd calls
//    selinux_android_restorecon() recursively on /sys/class, /sys/block, and /sys/devices.
//
// 4) Once the restorecon operation finishes, the main thread calls waitpid() to wait for all
//    subprocess handlers to complete and exit.  Once this happens, it marks coldboot as having
//    completed.
//
// At this point, ueventd is single threaded, poll()'s and then handles any future uevents.

// Lastly, it should be noted that uevents that occur during the coldboot process are handled
// without issue after the coldboot process completes.  This is because the uevent listener is
// paused while the uevent handler and restorecon actions take place.  Once coldboot completes,
// the uevent listener resumes in polling mode and will handle the uevents that occurred during
// coldboot.

namespace android {
namespace init {

class ColdBoot {
  public:
    ColdBoot(UeventListener& uevent_listener, DeviceHandler& device_handler)
        : uevent_listener_(uevent_listener),
          device_handler_(device_handler),
          num_handler_subprocesses_(std::thread::hardware_concurrency() ?: 4) {}

    void Run();

  private:
    void UeventHandlerMain(unsigned int process_num, unsigned int total_processes);
    void RegenerateUevents();
    void ForkSubProcesses();
    void DoRestoreCon();
    void WaitForSubProcesses();

    UeventListener& uevent_listener_;
    DeviceHandler& device_handler_;

    unsigned int num_handler_subprocesses_;
    std::vector<Uevent> uevent_queue_;

    std::set<pid_t> subprocess_pids_;
};

void ColdBoot::UeventHandlerMain(unsigned int process_num, unsigned int total_processes) {
    for (unsigned int i = process_num; i < uevent_queue_.size(); i += total_processes) {
        auto& uevent = uevent_queue_[i];
        device_handler_.HandleDeviceEvent(uevent);
    }
    _exit(EXIT_SUCCESS);
}

void ColdBoot::RegenerateUevents() {
    uevent_listener_.RegenerateUevents([this](const Uevent& uevent) {
        HandleFirmwareEvent(uevent);

        uevent_queue_.emplace_back(std::move(uevent));
        return ListenerAction::kContinue;
    });
}

void ColdBoot::ForkSubProcesses() {
    for (unsigned int i = 0; i < num_handler_subprocesses_; ++i) {
        auto pid = fork();
        if (pid < 0) {
            PLOG(FATAL) << "fork() failed!";
        }

        if (pid == 0) {
            UeventHandlerMain(i, num_handler_subprocesses_);
        }

        subprocess_pids_.emplace(pid);
    }
}

void ColdBoot::DoRestoreCon() {
    selinux_android_restorecon("/sys", SELINUX_ANDROID_RESTORECON_RECURSE);
    device_handler_.set_skip_restorecon(false);
}

void ColdBoot::WaitForSubProcesses() {
    // Treat subprocesses that crash or get stuck the same as if ueventd itself has crashed or gets
    // stuck.
    //
    // When a subprocess crashes, we fatally abort from ueventd.  init will restart ueventd when
    // init reaps it, and the cold boot process will start again.  If this continues to fail, then
    // since ueventd is marked as a critical service, init will reboot to recovery.
    //
    // When a subprocess gets stuck, keep ueventd spinning waiting for it.  init has a timeout for
    // cold boot and will reboot to the bootloader if ueventd does not complete in time.
    while (!subprocess_pids_.empty()) {
        int status;
        pid_t pid = TEMP_FAILURE_RETRY(waitpid(-1, &status, 0));
        if (pid == -1) {
            PLOG(ERROR) << "waitpid() failed";
            continue;
        }

        auto it = std::find(subprocess_pids_.begin(), subprocess_pids_.end(), pid);
        if (it == subprocess_pids_.end()) continue;

        if (WIFEXITED(status)) {
            if (WEXITSTATUS(status) == EXIT_SUCCESS) {
                subprocess_pids_.erase(it);
            } else {
                LOG(FATAL) << "subprocess exited with status " << WEXITSTATUS(status);
            }
        } else if (WIFSIGNALED(status)) {
            LOG(FATAL) << "subprocess killed by signal " << WTERMSIG(status);
        }
    }
}

void ColdBoot::Run() {
    android::base::Timer cold_boot_timer;

    RegenerateUevents();

    ForkSubProcesses();

    DoRestoreCon();

    WaitForSubProcesses();

    close(open(COLDBOOT_DONE, O_WRONLY | O_CREAT | O_CLOEXEC, 0000));
    LOG(INFO) << "Coldboot took " << cold_boot_timer.duration().count() / 1000.0f << " seconds";
}

int ueventd_main(int argc, char** argv) {
    /*
     * init sets the umask to 077 for forked processes. We need to
     * create files with exact permissions, without modification by
     * the umask.
     */
    umask(000);

    InitKernelLogging(argv);

    LOG(INFO) << "ueventd started!";

    SelinuxSetupKernelLogging();
    SelabelInitialize();

    DeviceHandler device_handler;
    UeventListener uevent_listener;

    {
        // Keep the current product name base configuration so we remain backwards compatible and
        // allow it to override everything.
        // TODO: cleanup platform ueventd.rc to remove vendor specific device node entries (b/34968103)
        auto hardware = android::base::GetProperty("ro.hardware", "");

        auto ueventd_configuration =
                ParseConfig({"/ueventd.rc", "/vendor/ueventd.rc", "/odm/ueventd.rc", hardware});

        device_handler = DeviceHandler{std::move(ueventd_configuration.dev_permissions),
                                       std::move(ueventd_configuration.sysfs_permissions),
                                       std::move(ueventd_configuration.subsystems),
                                       fs_mgr_get_boot_devices(), true};

        firmware_directories = ueventd_configuration.firmware_directories;
    }

    if (access(COLDBOOT_DONE, F_OK) != 0) {
        ColdBoot cold_boot(uevent_listener, device_handler);
        cold_boot.Run();
    }

    // We use waitpid() in ColdBoot, so we can't ignore SIGCHLD until now.
    signal(SIGCHLD, SIG_IGN);
    // Reap and pending children that exited between the last call to waitpid() and setting SIG_IGN
    // for SIGCHLD above.
    while (waitpid(-1, nullptr, WNOHANG) > 0) {
    }

    uevent_listener.Poll([&device_handler](const Uevent& uevent) {
        HandleFirmwareEvent(uevent);
        device_handler.HandleDeviceEvent(uevent);
        return ListenerAction::kContinue;
    });

    return 0;
}

}  // namespace init
}  // namespace android