1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
|
/*
* Copyright (C) 2014 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef _BACKTRACE_BACKTRACE_MAP_H
#define _BACKTRACE_BACKTRACE_MAP_H
#include <stdint.h>
#include <sys/types.h>
#ifdef _WIN32
// MINGW does not define these constants.
#define PROT_NONE 0
#define PROT_READ 0x1
#define PROT_WRITE 0x2
#define PROT_EXEC 0x4
#else
#include <sys/mman.h>
#endif
#include <deque>
#include <string>
#include <vector>
// Special flag to indicate a map is in /dev/. However, a map in
// /dev/ashmem/... does not set this flag.
static constexpr int PROT_DEVICE_MAP = 0x8000;
struct backtrace_map_t {
uintptr_t start = 0;
uintptr_t end = 0;
uintptr_t offset = 0;
uintptr_t load_bias = 0;
int flags = 0;
std::string name;
};
class BacktraceMap {
public:
// If uncached is true, then parse the current process map as of the call.
// Passing a map created with uncached set to true to Backtrace::Create()
// is unsupported.
static BacktraceMap* Create(pid_t pid, bool uncached = false);
// Same as above, but is compatible with the new unwinder.
static BacktraceMap* CreateNew(pid_t pid, bool uncached = false);
static BacktraceMap* Create(pid_t pid, const std::vector<backtrace_map_t>& maps);
virtual ~BacktraceMap();
// Fill in the map data structure for the given address.
virtual void FillIn(uintptr_t addr, backtrace_map_t* map);
// The flags returned are the same flags as used by the mmap call.
// The values are PROT_*.
int GetFlags(uintptr_t pc) {
backtrace_map_t map;
FillIn(pc, &map);
if (IsValid(map)) {
return map.flags;
}
return PROT_NONE;
}
bool IsReadable(uintptr_t pc) { return GetFlags(pc) & PROT_READ; }
bool IsWritable(uintptr_t pc) { return GetFlags(pc) & PROT_WRITE; }
bool IsExecutable(uintptr_t pc) { return GetFlags(pc) & PROT_EXEC; }
// In order to use the iterators on this object, a caller must
// call the LockIterator and UnlockIterator function to guarantee
// that the data does not change while it's being used.
virtual void LockIterator() {}
virtual void UnlockIterator() {}
typedef std::deque<backtrace_map_t>::iterator iterator;
iterator begin() { return maps_.begin(); }
iterator end() { return maps_.end(); }
typedef std::deque<backtrace_map_t>::const_iterator const_iterator;
const_iterator begin() const { return maps_.begin(); }
const_iterator end() const { return maps_.end(); }
virtual bool Build();
static inline bool IsValid(const backtrace_map_t& map) {
return map.end > 0;
}
protected:
BacktraceMap(pid_t pid);
virtual bool ParseLine(const char* line, backtrace_map_t* map);
std::deque<backtrace_map_t> maps_;
pid_t pid_;
};
class ScopedBacktraceMapIteratorLock {
public:
explicit ScopedBacktraceMapIteratorLock(BacktraceMap* map) : map_(map) {
map->LockIterator();
}
~ScopedBacktraceMapIteratorLock() {
map_->UnlockIterator();
}
private:
BacktraceMap* map_;
};
#endif // _BACKTRACE_BACKTRACE_MAP_H
|