summaryrefslogtreecommitdiffstats
blob: c9580af046263dd824ca23e79e8b06a39b8d8788 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
/*
 * Copyright (C) 2017 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef __TRACE_DEV_INC
#define __TRACE_DEV_INC

#define LOG_TAG "cutils-trace"

#include <errno.h>
#include <fcntl.h>
#include <limits.h>
#include <pthread.h>
#include <stdatomic.h>
#include <stdlib.h>
#include <string.h>
#include <sys/types.h>

#include <cutils/compiler.h>
#include <cutils/properties.h>
#include <cutils/trace.h>
#include <log/log.h>
#include <log/log_properties.h>

/**
 * Maximum size of a message that can be logged to the trace buffer.
 * Note this message includes a tag, the pid, and the string given as the name.
 * Names should be kept short to get the most use of the trace buffer.
 */
#define ATRACE_MESSAGE_LENGTH 1024

atomic_bool             atrace_is_ready      = ATOMIC_VAR_INIT(false);
int                     atrace_marker_fd     = -1;
uint64_t                atrace_enabled_tags  = ATRACE_TAG_NOT_READY;
static bool             atrace_is_debuggable = false;
static atomic_bool      atrace_is_enabled    = ATOMIC_VAR_INIT(true);
static pthread_mutex_t  atrace_tags_mutex    = PTHREAD_MUTEX_INITIALIZER;

// Set whether this process is debuggable, which determines whether
// application-level tracing is allowed when the ro.debuggable system property
// is not set to '1'.
void atrace_set_debuggable(bool debuggable)
{
    atrace_is_debuggable = debuggable;
    atrace_update_tags();
}

// Check whether the given command line matches one of the comma-separated
// values listed in the app_cmdlines property.
static bool atrace_is_cmdline_match(const char* cmdline)
{
    int count = property_get_int32("debug.atrace.app_number", 0);

    char buf[PROPERTY_KEY_MAX];
    char value[PROPERTY_VALUE_MAX];

    for (int i = 0; i < count; i++) {
        snprintf(buf, sizeof(buf), "debug.atrace.app_%d", i);
        property_get(buf, value, "");
        if (strcmp(value, "*") == 0 || strcmp(value, cmdline) == 0) {
            return true;
        }
    }

    return false;
}

// Determine whether application-level tracing is enabled for this process.
static bool atrace_is_app_tracing_enabled()
{
    bool sys_debuggable = __android_log_is_debuggable();
    bool result = false;

    if (sys_debuggable || atrace_is_debuggable) {
        // Check whether tracing is enabled for this process.
        FILE * file = fopen("/proc/self/cmdline", "re");
        if (file) {
            char cmdline[4096];
            if (fgets(cmdline, sizeof(cmdline), file)) {
                result = atrace_is_cmdline_match(cmdline);
            } else {
                ALOGE("Error reading cmdline: %s (%d)", strerror(errno), errno);
            }
            fclose(file);
        } else {
            ALOGE("Error opening /proc/self/cmdline: %s (%d)", strerror(errno),
                    errno);
        }
    }

    return result;
}

// Read the sysprop and return the value tags should be set to
static uint64_t atrace_get_property()
{
    char value[PROPERTY_VALUE_MAX];
    char *endptr;
    uint64_t tags;

    property_get("debug.atrace.tags.enableflags", value, "0");
    errno = 0;
    tags = strtoull(value, &endptr, 0);
    if (value[0] == '\0' || *endptr != '\0') {
        ALOGE("Error parsing trace property: Not a number: %s", value);
        return 0;
    } else if (errno == ERANGE || tags == ULLONG_MAX) {
        ALOGE("Error parsing trace property: Number too large: %s", value);
        return 0;
    }

    // Only set the "app" tag if this process was selected for app-level debug
    // tracing.
    if (atrace_is_app_tracing_enabled()) {
        tags |= ATRACE_TAG_APP;
    } else {
        tags &= ~ATRACE_TAG_APP;
    }

    return (tags | ATRACE_TAG_ALWAYS) & ATRACE_TAG_VALID_MASK;
}

// Update tags if tracing is ready. Useful as a sysprop change callback.
void atrace_update_tags()
{
    uint64_t tags;
    if (CC_UNLIKELY(atomic_load_explicit(&atrace_is_ready, memory_order_acquire))) {
        if (atomic_load_explicit(&atrace_is_enabled, memory_order_acquire)) {
            tags = atrace_get_property();
            pthread_mutex_lock(&atrace_tags_mutex);
            atrace_enabled_tags = tags;
            pthread_mutex_unlock(&atrace_tags_mutex);
        } else {
            // Tracing is disabled for this process, so we simply don't
            // initialize the tags.
            pthread_mutex_lock(&atrace_tags_mutex);
            atrace_enabled_tags = ATRACE_TAG_NOT_READY;
            pthread_mutex_unlock(&atrace_tags_mutex);
        }
    }
}

#define WRITE_MSG(format_begin, format_end, name, value) { \
    char buf[ATRACE_MESSAGE_LENGTH]; \
    int pid = getpid(); \
    int len = snprintf(buf, sizeof(buf), format_begin "%s" format_end, pid, \
        name, value); \
    if (len >= (int) sizeof(buf)) { \
        /* Given the sizeof(buf), and all of the current format buffers, \
         * it is impossible for name_len to be < 0 if len >= sizeof(buf). */ \
        int name_len = strlen(name) - (len - sizeof(buf)) - 1; \
        /* Truncate the name to make the message fit. */ \
        ALOGW("Truncated name in %s: %s\n", __FUNCTION__, name); \
        len = snprintf(buf, sizeof(buf), format_begin "%.*s" format_end, pid, \
            name_len, name, value); \
    } \
    write(atrace_marker_fd, buf, len); \
}

#endif  // __TRACE_DEV_INC