summaryrefslogtreecommitdiffstats
blob: aac3e699bdb84ea51f05b4743f159fe6af7bcb3f (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
/* libs/diskconfig/diskconfig.c
 *
 * Copyright 2008, The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *     http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#define LOG_TAG "diskconfig"

#include <errno.h>
#include <fcntl.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <unistd.h>
#include <sys/ioctl.h>
#include <sys/stat.h>

#include <linux/fs.h>

#include <cutils/config_utils.h>
#include <cutils/log.h>

#include <diskconfig/diskconfig.h>


static int
parse_len(const char *str, uint64_t *plen)
{
    char tmp[64];
    int len_str;
    uint32_t multiple = 1;

    strncpy(tmp, str, sizeof(tmp));
    tmp[sizeof(tmp)-1] = '\0';
    len_str = strlen(tmp);
    if (!len_str) {
        LOGE("Invalid disk length specified.");
        return 1;
    }

    switch(tmp[len_str - 1]) {
        case 'M': case 'm':
            /* megabyte */
            multiple <<= 10;
        case 'K': case 'k':
            /* kilobytes */
            multiple <<= 10;
            tmp[len_str - 1] = '\0';
            break;
        default:
            break;
    }

    *plen = strtoull(tmp, NULL, 0);
    if (!*plen) {
        LOGE("Invalid length specified: %s", str);
        return 1;
    }

    if (*plen == (uint64_t)-1) {
        if (multiple > 1) {
            LOGE("Size modifier illegal when len is -1");
            return 1;
        }
    } else {
        /* convert len to kilobytes */
        if (multiple > 1024)
            multiple >>= 10;
        *plen *= multiple;

        if (*plen > 0xffffffffULL) {
            LOGE("Length specified is too large!: %llu KB", *plen);
            return 1;
        }
    }

    return 0;
}


static int
load_partitions(cnode *root, struct disk_info *dinfo)
{
    cnode *partnode;

    dinfo->num_parts = 0;
    for (partnode = root->first_child; partnode; partnode = partnode->next) {
        struct part_info *pinfo = &dinfo->part_lst[dinfo->num_parts];
        const char *tmp;

        /* bleh, i will leak memory here, but i DONT CARE since
         * the only right thing to do when this function fails
         * is to quit */
        pinfo->name = strdup(partnode->name);

        if(config_bool(partnode, "active", 0))
            pinfo->flags |= PART_ACTIVE_FLAG;

        if (!(tmp = config_str(partnode, "type", NULL))) {
            LOGE("Partition type required: %s", pinfo->name);
            return 1;
        }

        /* possible values are: linux, fat32 */
        if (!strcmp(tmp, "linux")) {
            pinfo->type = PC_PART_TYPE_LINUX;
        } else if (!strcmp(tmp, "fat32")) {
            pinfo->type = PC_PART_TYPE_FAT32;
        } else {
            LOGE("Unsupported partition type found: %s", tmp);
            return 1;
        }

        if ((tmp = config_str(partnode, "len", NULL)) != NULL) {
            uint64_t len;
            if (parse_len(tmp, &len))
                return 1;
            pinfo->len_kb = (uint32_t) len;
        } else 
            pinfo->len_kb = 0;

        ++dinfo->num_parts;
    }

    return 0;
}

struct disk_info *
load_diskconfig(const char *fn, char *path_override)
{
    struct disk_info *dinfo;
    cnode *devroot;
    cnode *partnode;
    cnode *root = config_node("", "");
    const char *tmp;

    if (!(dinfo = malloc(sizeof(struct disk_info)))) {
        LOGE("Could not malloc disk_info");
        return NULL;
    }
    memset(dinfo, 0, sizeof(struct disk_info));

    if (!(dinfo->part_lst = malloc(MAX_NUM_PARTS * sizeof(struct part_info)))) {
        LOGE("Could not malloc part_lst");
        goto fail;
    }
    memset(dinfo->part_lst, 0,
           (MAX_NUM_PARTS * sizeof(struct part_info)));

    config_load_file(root, fn);
    if (root->first_child == NULL) {
        LOGE("Could not read config file %s", fn);
        goto fail;
    }

    if (!(devroot = config_find(root, "device"))) {
        LOGE("Could not find device section in config file '%s'", fn);
        goto fail;
    }


    if (!(tmp = config_str(devroot, "path", path_override))) {
        LOGE("device path is requried");
        goto fail;
    }
    dinfo->device = strdup(tmp);

    /* find the partition scheme */
    if (!(tmp = config_str(devroot, "scheme", NULL))) {
        LOGE("partition scheme is required");
        goto fail;
    } else if (!strcmp(tmp, "mbr")) {
        dinfo->scheme = PART_SCHEME_MBR;
    } else if (!strcmp(tmp, "gpt")) {
        LOGE("'gpt' partition scheme not supported yet.");
        goto fail;
    } else {
        LOGE("Unknown partition scheme specified: %s", tmp);
        goto fail;
    }

    /* grab the sector size (in bytes) */
    tmp = config_str(devroot, "sector_size", "512");
    dinfo->sect_size = strtol(tmp, NULL, 0);
    if (!dinfo->sect_size) {
        LOGE("Invalid sector size: %s", tmp);
        goto fail;
    }

    /* first lba where the partitions will start on disk */
    if (!(tmp = config_str(devroot, "start_lba", NULL))) {
        LOGE("start_lba must be provided");
        goto fail;
    }

    if (!(dinfo->skip_lba = strtol(tmp, NULL, 0))) {
        LOGE("Invalid starting LBA (or zero): %s", tmp);
        goto fail;
    }

    /* Number of LBAs on disk */
    if (!(tmp = config_str(devroot, "num_lba", NULL))) {
        LOGE("num_lba is required");
        goto fail;
    }
    dinfo->num_lba = strtoul(tmp, NULL, 0);

    if (!(partnode = config_find(devroot, "partitions"))) {
        LOGE("Device must specify partition list");
        goto fail;
    }

    if (load_partitions(partnode, dinfo))
        goto fail;

    return dinfo;

fail:
    if (dinfo->part_lst)
        free(dinfo->part_lst);
    if (dinfo->device)
        free(dinfo->device);
    free(dinfo);
    return NULL;
}

static int
sync_ptable(int fd)
{
    struct stat stat;
    int rv;

    sync();

    if (fstat(fd, &stat)) {
       LOGE("Cannot stat, errno=%d.", errno);
       return -1;
    }

    if (S_ISBLK(stat.st_mode) && ((rv = ioctl(fd, BLKRRPART, NULL)) < 0)) {
        LOGE("Could not re-read partition table. REBOOT!. (errno=%d)", errno);
        return -1;
    }

    return 0;
}

/* This function verifies that the disk info provided is valid, and if so,
 * returns an open file descriptor.
 *
 * This does not necessarily mean that it will later be successfully written
 * though. If we use the pc-bios partitioning scheme, we must use extended
 * partitions, which eat up some hd space. If the user manually provisioned
 * every single partition, but did not account for the extra needed space,
 * then we will later fail.
 *
 * TODO: Make validation more complete.
 */
static int
validate(struct disk_info *dinfo)
{
    int fd;
    int sect_sz;
    uint64_t disk_size;
    uint64_t total_size;
    int cnt;
    struct stat stat;

    if (!dinfo)
        return -1;

    if ((fd = open(dinfo->device, O_RDWR)) < 0) {
        LOGE("Cannot open device '%s' (errno=%d)", dinfo->device, errno);
        return -1;
    }

    if (fstat(fd, &stat)) {
        LOGE("Cannot stat file '%s', errno=%d.", dinfo->device, errno);
        goto fail;
    }


    /* XXX: Some of the code below is kind of redundant and should probably
     * be refactored a little, but it will do for now. */

    /* Verify that we can operate on the device that was requested.
     * We presently only support block devices and regular file images. */
    if (S_ISBLK(stat.st_mode)) {
        /* get the sector size and make sure we agree */
        if (ioctl(fd, BLKSSZGET, &sect_sz) < 0) {
            LOGE("Cannot get sector size (errno=%d)", errno);
            goto fail;
        }

        if (!sect_sz || sect_sz != dinfo->sect_size) {
            LOGE("Device sector size is zero or sector sizes do not match!");
            goto fail;
        }

        /* allow the user override the "disk size" if they provided num_lba */
        if (!dinfo->num_lba) {
            if (ioctl(fd, BLKGETSIZE64, &disk_size) < 0) {
                LOGE("Could not get block device size (errno=%d)", errno);
                goto fail;
            }
            /* XXX: we assume that the disk has < 2^32 sectors :-) */
            dinfo->num_lba = (uint32_t)(disk_size / (uint64_t)dinfo->sect_size);
        } else
            disk_size = (uint64_t)dinfo->num_lba * (uint64_t)dinfo->sect_size;
    } else if (S_ISREG(stat.st_mode)) {
        LOGI("Requesting operation on a regular file, not block device.");
        if (!dinfo->sect_size) {
            LOGE("Sector size for regular file images cannot be zero");
            goto fail;
        }
        if (dinfo->num_lba)
            disk_size = (uint64_t)dinfo->num_lba * (uint64_t)dinfo->sect_size;
        else {
            dinfo->num_lba = (uint32_t)(stat.st_size / dinfo->sect_size);
            disk_size = (uint64_t)stat.st_size;
        }
    } else {
        LOGE("Device does not refer to a regular file or a block device!");
        goto fail;
    }

#if 1
    ALOGV("Device/file %s: size=%llu bytes, num_lba=%u, sect_size=%d",
         dinfo->device, disk_size, dinfo->num_lba, dinfo->sect_size);
#endif

    /* since this is our offset into the disk, we start off with that as
     * our size of needed partitions */
    total_size = dinfo->skip_lba * dinfo->sect_size;

    /* add up all the partition sizes and make sure it fits */
    for (cnt = 0; cnt < dinfo->num_parts; ++cnt) {
        struct part_info *part = &dinfo->part_lst[cnt];
        if (part->len_kb != (uint32_t)-1) {
            total_size += part->len_kb * 1024;
        } else if (part->len_kb == 0) {
            LOGE("Zero-size partition '%s' is invalid.", part->name);
            goto fail;
        } else {
            /* the partition requests the rest of the disk. */
            if (cnt + 1 != dinfo->num_parts) {
                LOGE("Only the last partition in the list can request to fill "
                     "the rest of disk.");
                goto fail;
            }
        }

        if ((part->type != PC_PART_TYPE_LINUX) &&
            (part->type != PC_PART_TYPE_FAT32)) {
            LOGE("Unknown partition type (0x%x) encountered for partition "
                 "'%s'\n", part->type, part->name);
            goto fail;
        }
    }

    /* only matters for disks, not files */
    if (S_ISBLK(stat.st_mode) && total_size > disk_size) {
        LOGE("Total requested size of partitions (%llu) is greater than disk "
             "size (%llu).", total_size, disk_size);
        goto fail;
    }

    return fd;

fail:
    close(fd);
    return -1;
}

static int
validate_and_config(struct disk_info *dinfo, int *fd, struct write_list **lst)
{
    *lst = NULL;
    *fd = -1;

    if ((*fd = validate(dinfo)) < 0)
        return 1;

    switch (dinfo->scheme) {
        case PART_SCHEME_MBR:
            *lst = config_mbr(dinfo);
            return *lst == NULL;
        case PART_SCHEME_GPT:
            /* not supported yet */
        default:
            LOGE("Uknown partition scheme.");
            break;
    }

    close(*fd);
    *lst = NULL;
    return 1;
}

/* validate and process the disk layout configuration.
 * This will cause an update to the partitions' start lba.
 *
 * Basically, this does the same thing as apply_disk_config in test mode,
 * except that wlist_commit is not called to print out the data to be
 * written.
 */
int
process_disk_config(struct disk_info *dinfo)
{
    struct write_list *lst;
    int fd;

    if (validate_and_config(dinfo, &fd, &lst) != 0)
        return 1;

    close(fd);
    wlist_free(lst);
    return 0;
}


int
apply_disk_config(struct disk_info *dinfo, int test)
{
    int fd;
    struct write_list *wr_lst = NULL;
    int rv;

    if (validate_and_config(dinfo, &fd, &wr_lst) != 0) {
        LOGE("Configuration is invalid.");
        goto fail;
    }

    if ((rv = wlist_commit(fd, wr_lst, test)) >= 0)
        rv = test ? 0 : sync_ptable(fd);

    close(fd);
    wlist_free(wr_lst);
    return rv;

fail:
    close(fd);
    if (wr_lst)
        wlist_free(wr_lst);
    return 1;
}

int
dump_disk_config(struct disk_info *dinfo)
{
    int cnt;
    struct part_info *part;

    printf("Device: %s\n", dinfo->device);
    printf("Scheme: ");
    switch (dinfo->scheme) {
        case PART_SCHEME_MBR:
            printf("MBR");
            break;
        case PART_SCHEME_GPT:
            printf("GPT (unsupported)");
            break;
        default:
            printf("Unknown");
            break;
    }
    printf ("\n");

    printf("Sector size: %d\n", dinfo->sect_size);
    printf("Skip leading LBAs: %u\n", dinfo->skip_lba);
    printf("Number of LBAs: %u\n", dinfo->num_lba);
    printf("Partitions:\n");

    for (cnt = 0; cnt < dinfo->num_parts; ++cnt) {
        part = &dinfo->part_lst[cnt];
        printf("\tname = %s\n", part->name);
        printf("\t\tflags = %s\n",
               part->flags & PART_ACTIVE_FLAG ? "Active" : "None");
        printf("\t\ttype = %s\n",
               part->type == PC_PART_TYPE_LINUX ? "Linux" : "Unknown");
        if (part->len_kb == (uint32_t)-1)
            printf("\t\tlen = rest of disk\n");
        else
            printf("\t\tlen = %uKB\n", part->len_kb);
    }
    printf("Total number of partitions: %d\n", cnt);
    printf("\n");

    return 0;
}

struct part_info *
find_part(struct disk_info *dinfo, const char *name)
{
    struct part_info *pinfo;
    int cnt;

    for (cnt = 0; cnt < dinfo->num_parts; ++cnt) {
        pinfo = &dinfo->part_lst[cnt];
        if (!strcmp(pinfo->name, name))
            return pinfo;
    }

    return NULL;
}

/* NOTE: If the returned ptr is non-NULL, it must be freed by the caller. */
char *
find_part_device(struct disk_info *dinfo, const char *name)
{
    switch (dinfo->scheme) {
        case PART_SCHEME_MBR:
            return find_mbr_part(dinfo, name);
        case PART_SCHEME_GPT:
            LOGE("GPT is presently not supported");
            break;
        default:
            LOGE("Unknown partition table scheme");
            break;
    }

    return NULL;
}