summaryrefslogtreecommitdiffstats
blob: d01708d8b67a110e1a1ba170e322d560a5c0448f (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
/*
 * Copyright (C) 2005-2014 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef _LIBS_LOG_LOG_H
#define _LIBS_LOG_LOG_H

/* Too many in the ecosystem assume these are included */
#if !defined(_WIN32)
#include <pthread.h>
#endif
#include <stdint.h> /* uint16_t, int32_t */
#include <stdio.h>
#include <sys/types.h>
#include <time.h>
#include <unistd.h>

#include <android/log.h>
#include <log/log_id.h>
#include <log/log_main.h>
#include <log/log_radio.h>
#include <log/log_read.h>
#include <log/log_safetynet.h>
#include <log/log_system.h>
#include <log/log_time.h>
#include <log/uio.h> /* helper to define iovec for portability */

#ifdef __cplusplus
extern "C" {
#endif

/*
 * LOG_TAG is the local tag used for the following simplified
 * logging macros.  You can change this preprocessor definition
 * before using the other macros to change the tag.
 */

#ifndef LOG_TAG
#define LOG_TAG NULL
#endif

/*
 * Normally we strip the effects of ALOGV (VERBOSE messages),
 * LOG_FATAL and LOG_FATAL_IF (FATAL assert messages) from the
 * release builds be defining NDEBUG.  You can modify this (for
 * example with "#define LOG_NDEBUG 0" at the top of your source
 * file) to change that behavior.
 */

#ifndef LOG_NDEBUG
#ifdef NDEBUG
#define LOG_NDEBUG 1
#else
#define LOG_NDEBUG 0
#endif
#endif

/* --------------------------------------------------------------------- */

/*
 * This file uses ", ## __VA_ARGS__" zero-argument token pasting to
 * work around issues with debug-only syntax errors in assertions
 * that are missing format strings.  See commit
 * 19299904343daf191267564fe32e6cd5c165cd42
 */
#if defined(__clang__)
#pragma clang diagnostic push
#pragma clang diagnostic ignored "-Wgnu-zero-variadic-macro-arguments"
#endif

/* --------------------------------------------------------------------- */

/*
 * Event logging.
 */

/*
 * The following should not be used directly.
 */

int __android_log_bwrite(int32_t tag, const void* payload, size_t len);
int __android_log_btwrite(int32_t tag, char type, const void* payload,
                          size_t len);
int __android_log_bswrite(int32_t tag, const char* payload);

#define android_bWriteLog(tag, payload, len) \
  __android_log_bwrite(tag, payload, len)
#define android_btWriteLog(tag, type, payload, len) \
  __android_log_btwrite(tag, type, payload, len)

/*
 * Event log entry types.
 */
#ifndef __AndroidEventLogType_defined
#define __AndroidEventLogType_defined
typedef enum {
  /* Special markers for android_log_list_element type */
  EVENT_TYPE_LIST_STOP = '\n', /* declare end of list  */
  EVENT_TYPE_UNKNOWN = '?',    /* protocol error       */

  /* must match with declaration in java/android/android/util/EventLog.java */
  EVENT_TYPE_INT = 0,  /* int32_t */
  EVENT_TYPE_LONG = 1, /* int64_t */
  EVENT_TYPE_STRING = 2,
  EVENT_TYPE_LIST = 3,
  EVENT_TYPE_FLOAT = 4,
} AndroidEventLogType;
#endif
#define sizeof_AndroidEventLogType sizeof(typeof_AndroidEventLogType)
#define typeof_AndroidEventLogType unsigned char

#ifndef LOG_EVENT_INT
#define LOG_EVENT_INT(_tag, _value)                                          \
  {                                                                          \
    int intBuf = _value;                                                     \
    (void)android_btWriteLog(_tag, EVENT_TYPE_INT, &intBuf, sizeof(intBuf)); \
  }
#endif
#ifndef LOG_EVENT_LONG
#define LOG_EVENT_LONG(_tag, _value)                                            \
  {                                                                             \
    long long longBuf = _value;                                                 \
    (void)android_btWriteLog(_tag, EVENT_TYPE_LONG, &longBuf, sizeof(longBuf)); \
  }
#endif
#ifndef LOG_EVENT_FLOAT
#define LOG_EVENT_FLOAT(_tag, _value)                           \
  {                                                             \
    float floatBuf = _value;                                    \
    (void)android_btWriteLog(_tag, EVENT_TYPE_FLOAT, &floatBuf, \
                             sizeof(floatBuf));                 \
  }
#endif
#ifndef LOG_EVENT_STRING
#define LOG_EVENT_STRING(_tag, _value) \
  (void)__android_log_bswrite(_tag, _value);
#endif

#ifdef __linux__

#ifndef __ANDROID_USE_LIBLOG_CLOCK_INTERFACE
#ifndef __ANDROID_API__
#define __ANDROID_USE_LIBLOG_CLOCK_INTERFACE 1
#elif __ANDROID_API__ > 22 /* > Lollipop */
#define __ANDROID_USE_LIBLOG_CLOCK_INTERFACE 1
#else
#define __ANDROID_USE_LIBLOG_CLOCK_INTERFACE 0
#endif
#endif

#if __ANDROID_USE_LIBLOG_CLOCK_INTERFACE
clockid_t android_log_clockid(void);
#endif

#endif /* __linux__ */

/* --------------------------------------------------------------------- */

#ifndef __ANDROID_USE_LIBLOG_CLOSE_INTERFACE
#ifndef __ANDROID_API__
#define __ANDROID_USE_LIBLOG_CLOSE_INTERFACE 1
#elif __ANDROID_API__ > 18 /* > JellyBean */
#define __ANDROID_USE_LIBLOG_CLOSE_INTERFACE 1
#else
#define __ANDROID_USE_LIBLOG_CLOSE_INTERFACE 0
#endif
#endif

#if __ANDROID_USE_LIBLOG_CLOSE_INTERFACE
/*
 * Release any logger resources (a new log write will immediately re-acquire)
 *
 * May be used to clean up File descriptors after a Fork, the resources are
 * all O_CLOEXEC so wil self clean on exec().
 */
void __android_log_close(void);
#endif

#ifndef __ANDROID_USE_LIBLOG_RATELIMIT_INTERFACE
#ifndef __ANDROID_API__
#define __ANDROID_USE_LIBLOG_RATELIMIT_INTERFACE 1
#elif __ANDROID_API__ > 25 /* > OC */
#define __ANDROID_USE_LIBLOG_RATELIMIT_INTERFACE 1
#else
#define __ANDROID_USE_LIBLOG_RATELIMIT_INTERFACE 0
#endif
#endif

#if __ANDROID_USE_LIBLOG_RATELIMIT_INTERFACE

/*
 * if last is NULL, caller _must_ provide a consistent value for seconds.
 *
 * Return -1 if we can not acquire a lock, which below will permit the logging,
 * error on allowing a log message through.
 */
int __android_log_ratelimit(time_t seconds, time_t* last);

/*
 * Usage:
 *
 *   // Global default and state
 *   IF_ALOG_RATELIMIT() {
 *      ALOG*(...);
 *   }
 *
 *   // local state, 10 seconds ratelimit
 *   static time_t local_state;
 *   IF_ALOG_RATELIMIT_LOCAL(10, &local_state) {
 *     ALOG*(...);
 *   }
 */

#define IF_ALOG_RATELIMIT() if (__android_log_ratelimit(0, NULL) > 0)
#define IF_ALOG_RATELIMIT_LOCAL(seconds, state) \
  if (__android_log_ratelimit(seconds, state) > 0)

#else

/* No ratelimiting as API unsupported */
#define IF_ALOG_RATELIMIT() if (1)
#define IF_ALOG_RATELIMIT_LOCAL(...) if (1)

#endif

#if defined(__clang__)
#pragma clang diagnostic pop
#endif

#ifdef __cplusplus
}
#endif

#endif /* _LIBS_LOG_LOG_H */