summaryrefslogtreecommitdiffstats
blob: bb1ce348520721bd4a6a6907956b0c37c833e649 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
/*
 * Copyright (C) 2005-2016 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef _LIBS_LOG_EVENT_LIST_H
#define _LIBS_LOG_EVENT_LIST_H

#include <errno.h>
#include <stdint.h>

#if (defined(__cplusplus) && defined(_USING_LIBCXX))
extern "C++" {
#include <string>
}
#endif

#include <log/log.h>

#ifdef __cplusplus
extern "C" {
#endif

#ifndef __ANDROID_USE_LIBLOG_EVENT_INTERFACE
#ifndef __ANDROID_API__
#define __ANDROID_USE_LIBLOG_EVENT_INTERFACE 1
#elif __ANDROID_API__ > 23 /* > Marshmallow */
#define __ANDROID_USE_LIBLOG_EVENT_INTERFACE 1
#else
#define __ANDROID_USE_LIBLOG_EVENT_INTERFACE 0
#endif
#endif

#if __ANDROID_USE_LIBLOG_EVENT_INTERFACE

/* For manipulating lists of events. */

#define ANDROID_MAX_LIST_NEST_DEPTH 8

/*
 * The opaque context used to manipulate lists of events.
 */
#ifndef __android_log_context_defined
#define __android_log_context_defined
typedef struct android_log_context_internal* android_log_context;
#endif

/*
 * Elements returned when reading a list of events.
 */
#ifndef __android_log_list_element_defined
#define __android_log_list_element_defined
typedef struct {
  AndroidEventLogType type;
  uint16_t complete;
  uint16_t len;
  union {
    int32_t int32;
    int64_t int64;
    char* string;
    float float32;
  } data;
} android_log_list_element;
#endif

/*
 * Creates a context associated with an event tag to write elements to
 * the list of events.
 */
android_log_context create_android_logger(uint32_t tag);

/* All lists must be braced by a begin and end call */
/*
 * NB: If the first level braces are missing when specifying multiple
 *     elements, we will manufacturer a list to embrace it for your API
 *     convenience. For a single element, it will remain solitary.
 */
int android_log_write_list_begin(android_log_context ctx);
int android_log_write_list_end(android_log_context ctx);

int android_log_write_int32(android_log_context ctx, int32_t value);
int android_log_write_int64(android_log_context ctx, int64_t value);
int android_log_write_string8(android_log_context ctx, const char* value);
int android_log_write_string8_len(android_log_context ctx, const char* value,
                                  size_t maxlen);
int android_log_write_float32(android_log_context ctx, float value);

/* Submit the composed list context to the specified logger id */
/* NB: LOG_ID_EVENTS and LOG_ID_SECURITY only valid binary buffers */
int android_log_write_list(android_log_context ctx, log_id_t id);

/*
 * Creates a context from a raw buffer representing a list of events to be read.
 */
android_log_context create_android_log_parser(const char* msg, size_t len);

android_log_list_element android_log_read_next(android_log_context ctx);
android_log_list_element android_log_peek_next(android_log_context ctx);

/* Finished with reader or writer context */
int android_log_destroy(android_log_context* ctx);

#ifdef __cplusplus
#ifndef __class_android_log_event_list_defined
#define __class_android_log_event_list_defined
/* android_log_list C++ helpers */
extern "C++" {
class android_log_event_list {
  friend class __android_log_event_list;

 private:
  android_log_context ctx;
  int ret;

  android_log_event_list(const android_log_event_list&) = delete;
  void operator=(const android_log_event_list&) = delete;

 public:
  explicit android_log_event_list(int tag) : ret(0) {
    ctx = create_android_logger(static_cast<uint32_t>(tag));
  }
  explicit android_log_event_list(log_msg& log_msg) : ret(0) {
    ctx = create_android_log_parser(log_msg.msg() + sizeof(uint32_t),
                                    log_msg.entry.len - sizeof(uint32_t));
  }
  ~android_log_event_list() {
    android_log_destroy(&ctx);
  }

  int close() {
    int retval = android_log_destroy(&ctx);
    if (retval < 0) ret = retval;
    return retval;
  }

  /* To allow above C calls to use this class as parameter */
  operator android_log_context() const {
    return ctx;
  }

  /* return errors or transmit status */
  int status() const {
    return ret;
  }

  int begin() {
    int retval = android_log_write_list_begin(ctx);
    if (retval < 0) ret = retval;
    return ret;
  }
  int end() {
    int retval = android_log_write_list_end(ctx);
    if (retval < 0) ret = retval;
    return ret;
  }

  android_log_event_list& operator<<(int32_t value) {
    int retval = android_log_write_int32(ctx, value);
    if (retval < 0) ret = retval;
    return *this;
  }

  android_log_event_list& operator<<(uint32_t value) {
    int retval = android_log_write_int32(ctx, static_cast<int32_t>(value));
    if (retval < 0) ret = retval;
    return *this;
  }

  android_log_event_list& operator<<(bool value) {
    int retval = android_log_write_int32(ctx, value ? 1 : 0);
    if (retval < 0) ret = retval;
    return *this;
  }

  android_log_event_list& operator<<(int64_t value) {
    int retval = android_log_write_int64(ctx, value);
    if (retval < 0) ret = retval;
    return *this;
  }

  android_log_event_list& operator<<(uint64_t value) {
    int retval = android_log_write_int64(ctx, static_cast<int64_t>(value));
    if (retval < 0) ret = retval;
    return *this;
  }

  android_log_event_list& operator<<(const char* value) {
    int retval = android_log_write_string8(ctx, value);
    if (retval < 0) ret = retval;
    return *this;
  }

#if defined(_USING_LIBCXX)
  android_log_event_list& operator<<(const std::string& value) {
    int retval =
        android_log_write_string8_len(ctx, value.data(), value.length());
    if (retval < 0) ret = retval;
    return *this;
  }
#endif

  android_log_event_list& operator<<(float value) {
    int retval = android_log_write_float32(ctx, value);
    if (retval < 0) ret = retval;
    return *this;
  }

  int write(log_id_t id = LOG_ID_EVENTS) {
    /* facilitate -EBUSY retry */
    if ((ret == -EBUSY) || (ret > 0)) ret = 0;
    int retval = android_log_write_list(ctx, id);
    /* existing errors trump transmission errors */
    if (!ret) ret = retval;
    return ret;
  }

  int operator<<(log_id_t id) {
    write(id);
    android_log_destroy(&ctx);
    return ret;
  }

  /*
   * Append<Type> methods removes any integer promotion
   * confusion, and adds access to string with length.
   * Append methods are also added for all types for
   * convenience.
   */

  bool AppendInt(int32_t value) {
    int retval = android_log_write_int32(ctx, value);
    if (retval < 0) ret = retval;
    return ret >= 0;
  }

  bool AppendLong(int64_t value) {
    int retval = android_log_write_int64(ctx, value);
    if (retval < 0) ret = retval;
    return ret >= 0;
  }

  bool AppendString(const char* value) {
    int retval = android_log_write_string8(ctx, value);
    if (retval < 0) ret = retval;
    return ret >= 0;
  }

  bool AppendString(const char* value, size_t len) {
    int retval = android_log_write_string8_len(ctx, value, len);
    if (retval < 0) ret = retval;
    return ret >= 0;
  }

#if defined(_USING_LIBCXX)
  bool AppendString(const std::string& value) {
    int retval =
        android_log_write_string8_len(ctx, value.data(), value.length());
    if (retval < 0) ret = retval;
    return ret;
  }

  bool Append(const std::string& value) {
    int retval =
        android_log_write_string8_len(ctx, value.data(), value.length());
    if (retval < 0) ret = retval;
    return ret;
  }
#endif

  bool AppendFloat(float value) {
    int retval = android_log_write_float32(ctx, value);
    if (retval < 0) ret = retval;
    return ret >= 0;
  }

  template <typename Tvalue>
  bool Append(Tvalue value) {
    *this << value;
    return ret >= 0;
  }

  bool Append(const char* value, size_t len) {
    int retval = android_log_write_string8_len(ctx, value, len);
    if (retval < 0) ret = retval;
    return ret >= 0;
  }

  android_log_list_element read() {
    return android_log_read_next(ctx);
  }
  android_log_list_element peek() {
    return android_log_peek_next(ctx);
  }
};
}
#endif
#endif

#endif /* __ANDROID_USE_LIBLOG_EVENT_INTERFACE */

#ifdef __cplusplus
}
#endif

#endif /* _LIBS_LOG_EVENT_LIST_H */