summaryrefslogtreecommitdiffstats
blob: 93b9d4e9332495d46059ae7e66dfd8838d912d20 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
/*
 * Copyright (C) 2005-2017 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef _LIBS_LOG_LOG_READ_H
#define _LIBS_LOG_LOG_READ_H

/* deal with possible sys/cdefs.h conflict with fcntl.h */
#ifdef __unused
#define __unused_defined __unused
#undef __unused
#endif

#include <fcntl.h> /* Pick up O_* macros */

/* restore definitions from above */
#ifdef __unused_defined
#define __unused __attribute__((__unused__))
#endif

#include <stdint.h>

#include <log/log_id.h>
#include <log/log_time.h>

#ifdef __cplusplus
extern "C" {
#endif

/*
 * Native log reading interface section. See logcat for sample code.
 *
 * The preferred API is an exec of logcat. Likely uses of this interface
 * are if native code suffers from exec or filtration being too costly,
 * access to raw information, or parsing is an issue.
 */

/*
 * The userspace structure for version 1 of the logger_entry ABI.
 */
#ifndef __struct_logger_entry_defined
#define __struct_logger_entry_defined
struct logger_entry {
  uint16_t len;   /* length of the payload */
  uint16_t __pad; /* no matter what, we get 2 bytes of padding */
  int32_t pid;    /* generating process's pid */
  int32_t tid;    /* generating process's tid */
  int32_t sec;    /* seconds since Epoch */
  int32_t nsec;   /* nanoseconds */
#ifndef __cplusplus
  char msg[0]; /* the entry's payload */
#endif
};
#endif

/*
 * The userspace structure for version 2 of the logger_entry ABI.
 */
#ifndef __struct_logger_entry_v2_defined
#define __struct_logger_entry_v2_defined
struct logger_entry_v2 {
  uint16_t len;      /* length of the payload */
  uint16_t hdr_size; /* sizeof(struct logger_entry_v2) */
  int32_t pid;       /* generating process's pid */
  int32_t tid;       /* generating process's tid */
  int32_t sec;       /* seconds since Epoch */
  int32_t nsec;      /* nanoseconds */
  uint32_t euid;     /* effective UID of logger */
#ifndef __cplusplus
  char msg[0]; /* the entry's payload */
#endif
} __attribute__((__packed__));
#endif

/*
 * The userspace structure for version 3 of the logger_entry ABI.
 */
#ifndef __struct_logger_entry_v3_defined
#define __struct_logger_entry_v3_defined
struct logger_entry_v3 {
  uint16_t len;      /* length of the payload */
  uint16_t hdr_size; /* sizeof(struct logger_entry_v3) */
  int32_t pid;       /* generating process's pid */
  int32_t tid;       /* generating process's tid */
  int32_t sec;       /* seconds since Epoch */
  int32_t nsec;      /* nanoseconds */
  uint32_t lid;      /* log id of the payload */
#ifndef __cplusplus
  char msg[0]; /* the entry's payload */
#endif
} __attribute__((__packed__));
#endif

/*
 * The userspace structure for version 4 of the logger_entry ABI.
 */
#ifndef __struct_logger_entry_v4_defined
#define __struct_logger_entry_v4_defined
struct logger_entry_v4 {
  uint16_t len;      /* length of the payload */
  uint16_t hdr_size; /* sizeof(struct logger_entry_v4) */
  int32_t pid;       /* generating process's pid */
  uint32_t tid;      /* generating process's tid */
  uint32_t sec;      /* seconds since Epoch */
  uint32_t nsec;     /* nanoseconds */
  uint32_t lid;      /* log id of the payload, bottom 4 bits currently */
  uint32_t uid;      /* generating process's uid */
#ifndef __cplusplus
  char msg[0]; /* the entry's payload */
#endif
};
#endif

/*
 * The maximum size of the log entry payload that can be
 * written to the logger. An attempt to write more than
 * this amount will result in a truncated log entry.
 */
#define LOGGER_ENTRY_MAX_PAYLOAD 4068

/*
 * The maximum size of a log entry which can be read.
 * An attempt to read less than this amount may result
 * in read() returning EINVAL.
 */
#define LOGGER_ENTRY_MAX_LEN (5 * 1024)

#ifndef __struct_log_msg_defined
#define __struct_log_msg_defined
struct log_msg {
  union {
    unsigned char buf[LOGGER_ENTRY_MAX_LEN + 1];
    struct logger_entry_v4 entry;
    struct logger_entry_v4 entry_v4;
    struct logger_entry_v3 entry_v3;
    struct logger_entry_v2 entry_v2;
    struct logger_entry entry_v1;
  } __attribute__((aligned(4)));
#ifdef __cplusplus
  /* Matching log_time operators */
  bool operator==(const log_msg& T) const {
    return (entry.sec == T.entry.sec) && (entry.nsec == T.entry.nsec);
  }
  bool operator!=(const log_msg& T) const {
    return !(*this == T);
  }
  bool operator<(const log_msg& T) const {
    return (entry.sec < T.entry.sec) ||
           ((entry.sec == T.entry.sec) && (entry.nsec < T.entry.nsec));
  }
  bool operator>=(const log_msg& T) const {
    return !(*this < T);
  }
  bool operator>(const log_msg& T) const {
    return (entry.sec > T.entry.sec) ||
           ((entry.sec == T.entry.sec) && (entry.nsec > T.entry.nsec));
  }
  bool operator<=(const log_msg& T) const {
    return !(*this > T);
  }
  uint64_t nsec() const {
    return static_cast<uint64_t>(entry.sec) * NS_PER_SEC + entry.nsec;
  }

  /* packet methods */
  log_id_t id() {
    return static_cast<log_id_t>(entry.lid);
  }
  char* msg() {
    unsigned short hdr_size = entry.hdr_size;
    if (!hdr_size) {
      hdr_size = sizeof(entry_v1);
    }
    if ((hdr_size < sizeof(entry_v1)) || (hdr_size > sizeof(entry))) {
      return nullptr;
    }
    return reinterpret_cast<char*>(buf) + hdr_size;
  }
  unsigned int len() {
    return (entry.hdr_size ? entry.hdr_size
                           : static_cast<uint16_t>(sizeof(entry_v1))) +
           entry.len;
  }
#endif
};
#endif

#ifndef __ANDROID_USE_LIBLOG_READER_INTERFACE
#ifndef __ANDROID_API__
#define __ANDROID_USE_LIBLOG_READER_INTERFACE 3
#elif __ANDROID_API__ > 23 /* > Marshmallow */
#define __ANDROID_USE_LIBLOG_READER_INTERFACE 3
#elif __ANDROID_API__ > 22 /* > Lollipop */
#define __ANDROID_USE_LIBLOG_READER_INTERFACE 2
#elif __ANDROID_API__ > 19 /* > KitKat */
#define __ANDROID_USE_LIBLOG_READER_INTERFACE 1
#else
#define __ANDROID_USE_LIBLOG_READER_INTERFACE 0
#endif
#endif

#if __ANDROID_USE_LIBLOG_READER_INTERFACE

struct logger;

log_id_t android_logger_get_id(struct logger* logger);

int android_logger_clear(struct logger* logger);
long android_logger_get_log_size(struct logger* logger);
int android_logger_set_log_size(struct logger* logger, unsigned long size);
long android_logger_get_log_readable_size(struct logger* logger);
int android_logger_get_log_version(struct logger* logger);

struct logger_list;

#if __ANDROID_USE_LIBLOG_READER_INTERFACE > 1
ssize_t android_logger_get_statistics(struct logger_list* logger_list,
                                      char* buf, size_t len);
ssize_t android_logger_get_prune_list(struct logger_list* logger_list,
                                      char* buf, size_t len);
int android_logger_set_prune_list(struct logger_list* logger_list, char* buf,
                                  size_t len);
#endif

#define ANDROID_LOG_RDONLY O_RDONLY
#define ANDROID_LOG_WRONLY O_WRONLY
#define ANDROID_LOG_RDWR O_RDWR
#define ANDROID_LOG_ACCMODE O_ACCMODE
#ifndef O_NONBLOCK
#define ANDROID_LOG_NONBLOCK 0x00000800
#else
#define ANDROID_LOG_NONBLOCK O_NONBLOCK
#endif
#if __ANDROID_USE_LIBLOG_READER_INTERFACE > 2
#define ANDROID_LOG_WRAP 0x40000000 /* Block until buffer about to wrap */
#define ANDROID_LOG_WRAP_DEFAULT_TIMEOUT 7200 /* 2 hour default */
#endif
#if __ANDROID_USE_LIBLOG_READER_INTERFACE > 1
#define ANDROID_LOG_PSTORE 0x80000000
#endif

struct logger_list* android_logger_list_alloc(int mode, unsigned int tail,
                                              pid_t pid);
struct logger_list* android_logger_list_alloc_time(int mode, log_time start,
                                                   pid_t pid);
void android_logger_list_free(struct logger_list* logger_list);
/* In the purest sense, the following two are orthogonal interfaces */
int android_logger_list_read(struct logger_list* logger_list,
                             struct log_msg* log_msg);

/* Multiple log_id_t opens */
struct logger* android_logger_open(struct logger_list* logger_list, log_id_t id);
#define android_logger_close android_logger_free
/* Single log_id_t open */
struct logger_list* android_logger_list_open(log_id_t id, int mode,
                                             unsigned int tail, pid_t pid);
#define android_logger_list_close android_logger_list_free

#endif /* __ANDROID_USE_LIBLOG_READER_INTERFACE */

#ifdef __cplusplus
}
#endif

#endif /* _LIBS_LOG_LOG_H */