1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
|
/*
* Copyright (C) 2015 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#include "nativeloader/native_loader.h"
#include "ScopedUtfChars.h"
#include <dlfcn.h>
#ifdef __ANDROID__
#define LOG_TAG "libnativeloader"
#include "nativeloader/dlext_namespaces.h"
#include "cutils/properties.h"
#include "log/log.h"
#endif
#include "nativebridge/native_bridge.h"
#include <algorithm>
#include <vector>
#include <string>
#include <mutex>
#include <android-base/file.h>
#include <android-base/macros.h>
#include <android-base/strings.h>
#define CHECK(predicate) LOG_ALWAYS_FATAL_IF(!(predicate),\
"%s:%d: %s CHECK '" #predicate "' failed.",\
__FILE__, __LINE__, __FUNCTION__)
namespace android {
#if defined(__ANDROID__)
class NativeLoaderNamespace {
public:
NativeLoaderNamespace()
: android_ns_(nullptr), native_bridge_ns_(nullptr) { }
explicit NativeLoaderNamespace(android_namespace_t* ns)
: android_ns_(ns), native_bridge_ns_(nullptr) { }
explicit NativeLoaderNamespace(native_bridge_namespace_t* ns)
: android_ns_(nullptr), native_bridge_ns_(ns) { }
NativeLoaderNamespace(NativeLoaderNamespace&& that) = default;
NativeLoaderNamespace(const NativeLoaderNamespace& that) = default;
NativeLoaderNamespace& operator=(const NativeLoaderNamespace& that) = default;
android_namespace_t* get_android_ns() const {
CHECK(native_bridge_ns_ == nullptr);
return android_ns_;
}
native_bridge_namespace_t* get_native_bridge_ns() const {
CHECK(android_ns_ == nullptr);
return native_bridge_ns_;
}
bool is_android_namespace() const {
return native_bridge_ns_ == nullptr;
}
private:
// Only one of them can be not null
android_namespace_t* android_ns_;
native_bridge_namespace_t* native_bridge_ns_;
};
static constexpr const char* kPublicNativeLibrariesSystemConfigPathFromRoot =
"/etc/public.libraries.txt";
static constexpr const char* kPublicNativeLibrariesVendorConfig =
"/vendor/etc/public.libraries.txt";
// (http://b/27588281) This is a workaround for apps using custom classloaders and calling
// System.load() with an absolute path which is outside of the classloader library search path.
// This list includes all directories app is allowed to access this way.
static constexpr const char* kWhitelistedDirectories = "/data:/mnt/expand";
static bool is_debuggable() {
char debuggable[PROP_VALUE_MAX];
property_get("ro.debuggable", debuggable, "0");
return std::string(debuggable) == "1";
}
class LibraryNamespaces {
public:
LibraryNamespaces() : initialized_(false) { }
bool Create(JNIEnv* env,
jobject class_loader,
bool is_shared,
jstring java_library_path,
jstring java_permitted_path,
NativeLoaderNamespace* ns,
std::string* error_msg) {
std::string library_path; // empty string by default.
if (java_library_path != nullptr) {
ScopedUtfChars library_path_utf_chars(env, java_library_path);
library_path = library_path_utf_chars.c_str();
}
// (http://b/27588281) This is a workaround for apps using custom
// classloaders and calling System.load() with an absolute path which
// is outside of the classloader library search path.
//
// This part effectively allows such a classloader to access anything
// under /data and /mnt/expand
std::string permitted_path = kWhitelistedDirectories;
if (java_permitted_path != nullptr) {
ScopedUtfChars path(env, java_permitted_path);
if (path.c_str() != nullptr && path.size() > 0) {
permitted_path = permitted_path + ":" + path.c_str();
}
}
if (!initialized_ && !InitPublicNamespace(library_path.c_str(), error_msg)) {
return false;
}
bool found = FindNamespaceByClassLoader(env, class_loader, nullptr);
LOG_ALWAYS_FATAL_IF(found,
"There is already a namespace associated with this classloader");
uint64_t namespace_type = ANDROID_NAMESPACE_TYPE_ISOLATED;
if (is_shared) {
namespace_type |= ANDROID_NAMESPACE_TYPE_SHARED;
}
NativeLoaderNamespace parent_ns;
bool found_parent_namespace = FindParentNamespaceByClassLoader(env, class_loader, &parent_ns);
bool is_native_bridge = false;
if (found_parent_namespace) {
is_native_bridge = !parent_ns.is_android_namespace();
} else if (!library_path.empty()) {
is_native_bridge = NativeBridgeIsPathSupported(library_path.c_str());
}
NativeLoaderNamespace native_loader_ns;
if (!is_native_bridge) {
android_namespace_t* ns = android_create_namespace("classloader-namespace",
nullptr,
library_path.c_str(),
namespace_type,
permitted_path.c_str(),
parent_ns.get_android_ns());
if (ns == nullptr) {
*error_msg = dlerror();
return false;
}
native_loader_ns = NativeLoaderNamespace(ns);
} else {
native_bridge_namespace_t* ns = NativeBridgeCreateNamespace("classloader-namespace",
nullptr,
library_path.c_str(),
namespace_type,
permitted_path.c_str(),
parent_ns.get_native_bridge_ns());
if (ns == nullptr) {
*error_msg = NativeBridgeGetError();
return false;
}
native_loader_ns = NativeLoaderNamespace(ns);
}
namespaces_.push_back(std::make_pair(env->NewWeakGlobalRef(class_loader), native_loader_ns));
*ns = native_loader_ns;
return true;
}
bool FindNamespaceByClassLoader(JNIEnv* env, jobject class_loader, NativeLoaderNamespace* ns) {
auto it = std::find_if(namespaces_.begin(), namespaces_.end(),
[&](const std::pair<jweak, NativeLoaderNamespace>& value) {
return env->IsSameObject(value.first, class_loader);
});
if (it != namespaces_.end()) {
if (ns != nullptr) {
*ns = it->second;
}
return true;
}
return false;
}
void Initialize() {
// Once public namespace is initialized there is no
// point in running this code - it will have no effect
// on the current list of public libraries.
if (initialized_) {
return;
}
std::vector<std::string> sonames;
const char* android_root_env = getenv("ANDROID_ROOT");
std::string root_dir = android_root_env != nullptr ? android_root_env : "/system";
std::string public_native_libraries_system_config =
root_dir + kPublicNativeLibrariesSystemConfigPathFromRoot;
std::string error_msg;
LOG_ALWAYS_FATAL_IF(!ReadConfig(public_native_libraries_system_config, &sonames, &error_msg),
"Error reading public native library list from \"%s\": %s",
public_native_libraries_system_config.c_str(), error_msg.c_str());
// For debuggable platform builds use ANDROID_ADDITIONAL_PUBLIC_LIBRARIES environment
// variable to add libraries to the list. This is intended for platform tests only.
if (is_debuggable()) {
const char* additional_libs = getenv("ANDROID_ADDITIONAL_PUBLIC_LIBRARIES");
if (additional_libs != nullptr && additional_libs[0] != '\0') {
std::vector<std::string> additional_libs_vector = base::Split(additional_libs, ":");
std::copy(additional_libs_vector.begin(),
additional_libs_vector.end(),
std::back_inserter(sonames));
}
}
// This file is optional, quietly ignore if the file does not exist.
ReadConfig(kPublicNativeLibrariesVendorConfig, &sonames);
// android_init_namespaces() expects all the public libraries
// to be loaded so that they can be found by soname alone.
//
// TODO(dimitry): this is a bit misleading since we do not know
// if the vendor public library is going to be opened from /vendor/lib
// we might as well end up loading them from /system/lib
// For now we rely on CTS test to catch things like this but
// it should probably be addressed in the future.
for (const auto& soname : sonames) {
dlopen(soname.c_str(), RTLD_NOW | RTLD_NODELETE);
}
public_libraries_ = base::Join(sonames, ':');
}
void Reset() {
namespaces_.clear();
}
private:
bool ReadConfig(const std::string& configFile, std::vector<std::string>* sonames,
std::string* error_msg = nullptr) {
// Read list of public native libraries from the config file.
std::string file_content;
if(!base::ReadFileToString(configFile, &file_content)) {
if (error_msg) *error_msg = strerror(errno);
return false;
}
std::vector<std::string> lines = base::Split(file_content, "\n");
for (auto& line : lines) {
auto trimmed_line = base::Trim(line);
if (trimmed_line[0] == '#' || trimmed_line.empty()) {
continue;
}
size_t space_pos = trimmed_line.rfind(' ');
if (space_pos != std::string::npos) {
std::string type = trimmed_line.substr(space_pos + 1);
if (type != "32" && type != "64") {
if (error_msg) *error_msg = "Malformed line: " + line;
return false;
}
#if defined(__LP64__)
// Skip 32 bit public library.
if (type == "32") {
continue;
}
#else
// Skip 64 bit public library.
if (type == "64") {
continue;
}
#endif
trimmed_line.resize(space_pos);
}
sonames->push_back(trimmed_line);
}
return true;
}
bool InitPublicNamespace(const char* library_path, std::string* error_msg) {
// Ask native bride if this apps library path should be handled by it
bool is_native_bridge = NativeBridgeIsPathSupported(library_path);
// (http://b/25844435) - Some apps call dlopen from generated code (mono jited
// code is one example) unknown to linker in which case linker uses anonymous
// namespace. The second argument specifies the search path for the anonymous
// namespace which is the library_path of the classloader.
initialized_ = android_init_namespaces(public_libraries_.c_str(),
is_native_bridge ? nullptr : library_path);
if (!initialized_) {
*error_msg = dlerror();
return false;
}
// and now initialize native bridge namespaces if necessary.
if (NativeBridgeInitialized()) {
initialized_ = NativeBridgeInitNamespace(public_libraries_.c_str(),
is_native_bridge ? library_path : nullptr);
if (!initialized_) {
*error_msg = NativeBridgeGetError();
}
}
return initialized_;
}
jobject GetParentClassLoader(JNIEnv* env, jobject class_loader) {
jclass class_loader_class = env->FindClass("java/lang/ClassLoader");
jmethodID get_parent = env->GetMethodID(class_loader_class,
"getParent",
"()Ljava/lang/ClassLoader;");
return env->CallObjectMethod(class_loader, get_parent);
}
bool FindParentNamespaceByClassLoader(JNIEnv* env,
jobject class_loader,
NativeLoaderNamespace* ns) {
jobject parent_class_loader = GetParentClassLoader(env, class_loader);
while (parent_class_loader != nullptr) {
if (FindNamespaceByClassLoader(env, parent_class_loader, ns)) {
return true;
}
parent_class_loader = GetParentClassLoader(env, parent_class_loader);
}
return false;
}
bool initialized_;
std::vector<std::pair<jweak, NativeLoaderNamespace>> namespaces_;
std::string public_libraries_;
DISALLOW_COPY_AND_ASSIGN(LibraryNamespaces);
};
static std::mutex g_namespaces_mutex;
static LibraryNamespaces* g_namespaces = new LibraryNamespaces;
#endif
void InitializeNativeLoader() {
#if defined(__ANDROID__)
std::lock_guard<std::mutex> guard(g_namespaces_mutex);
g_namespaces->Initialize();
#endif
}
void ResetNativeLoader() {
#if defined(__ANDROID__)
std::lock_guard<std::mutex> guard(g_namespaces_mutex);
g_namespaces->Reset();
#endif
}
jstring CreateClassLoaderNamespace(JNIEnv* env,
int32_t target_sdk_version,
jobject class_loader,
bool is_shared,
jstring library_path,
jstring permitted_path) {
#if defined(__ANDROID__)
UNUSED(target_sdk_version);
std::lock_guard<std::mutex> guard(g_namespaces_mutex);
std::string error_msg;
NativeLoaderNamespace ns;
bool success = g_namespaces->Create(env,
class_loader,
is_shared,
library_path,
permitted_path,
&ns,
&error_msg);
if (!success) {
return env->NewStringUTF(error_msg.c_str());
}
#else
UNUSED(env, target_sdk_version, class_loader, is_shared,
library_path, permitted_path);
#endif
return nullptr;
}
void* OpenNativeLibrary(JNIEnv* env,
int32_t target_sdk_version,
const char* path,
jobject class_loader,
jstring library_path,
bool* needs_native_bridge,
std::string* error_msg) {
#if defined(__ANDROID__)
UNUSED(target_sdk_version);
if (class_loader == nullptr) {
*needs_native_bridge = false;
return dlopen(path, RTLD_NOW);
}
std::lock_guard<std::mutex> guard(g_namespaces_mutex);
NativeLoaderNamespace ns;
if (!g_namespaces->FindNamespaceByClassLoader(env, class_loader, &ns)) {
// This is the case where the classloader was not created by ApplicationLoaders
// In this case we create an isolated not-shared namespace for it.
if (!g_namespaces->Create(env, class_loader, false, library_path, nullptr, &ns, error_msg)) {
return nullptr;
}
}
if (ns.is_android_namespace()) {
android_dlextinfo extinfo;
extinfo.flags = ANDROID_DLEXT_USE_NAMESPACE;
extinfo.library_namespace = ns.get_android_ns();
void* handle = android_dlopen_ext(path, RTLD_NOW, &extinfo);
if (handle == nullptr) {
*error_msg = dlerror();
}
*needs_native_bridge = false;
return handle;
} else {
void* handle = NativeBridgeLoadLibraryExt(path, RTLD_NOW, ns.get_native_bridge_ns());
if (handle == nullptr) {
*error_msg = NativeBridgeGetError();
}
*needs_native_bridge = true;
return handle;
}
#else
UNUSED(env, target_sdk_version, class_loader, library_path);
*needs_native_bridge = false;
void* handle = dlopen(path, RTLD_NOW);
if (handle == nullptr) {
if (NativeBridgeIsSupported(path)) {
*needs_native_bridge = true;
handle = NativeBridgeLoadLibrary(path, RTLD_NOW);
if (handle == nullptr) {
*error_msg = NativeBridgeGetError();
}
} else {
*needs_native_bridge = false;
*error_msg = dlerror();
}
}
return handle;
#endif
}
bool CloseNativeLibrary(void* handle, const bool needs_native_bridge) {
return needs_native_bridge ? NativeBridgeUnloadLibrary(handle) :
dlclose(handle);
}
#if defined(__ANDROID__)
// native_bridge_namespaces are not supported for callers of this function.
// This function will return nullptr in the case when application is running
// on native bridge.
android_namespace_t* FindNamespaceByClassLoader(JNIEnv* env, jobject class_loader) {
std::lock_guard<std::mutex> guard(g_namespaces_mutex);
NativeLoaderNamespace ns;
if (g_namespaces->FindNamespaceByClassLoader(env, class_loader, &ns)) {
return ns.is_android_namespace() ? ns.get_android_ns() : nullptr;
}
return nullptr;
}
#endif
}; // android namespace
|