1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
|
/*
* Copyright 2014 Google, Inc
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
//#define LOG_NDEBUG 0
#define LOG_TAG "libprocessgroup"
#include <assert.h>
#include <dirent.h>
#include <errno.h>
#include <fcntl.h>
#include <inttypes.h>
#include <signal.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <sys/stat.h>
#include <sys/types.h>
#include <unistd.h>
#include <chrono>
#include <memory>
#include <mutex>
#include <set>
#include <string>
#include <thread>
#include <android-base/file.h>
#include <android-base/logging.h>
#ifdef __ANDROID__
#include <android-base/properties.h>
#endif
#include <android-base/stringprintf.h>
#include <android-base/strings.h>
#include <private/android_filesystem_config.h>
#include <processgroup/processgroup.h>
#ifdef __ANDROID__
using android::base::GetBoolProperty;
#endif
using android::base::StartsWith;
using android::base::StringPrintf;
using android::base::WriteStringToFile;
using namespace std::chrono_literals;
#define MEM_CGROUP_PATH "/dev/memcg/apps"
#define MEM_CGROUP_TASKS "/dev/memcg/apps/tasks"
#define ACCT_CGROUP_PATH "/acct"
#define PROCESSGROUP_CGROUP_PROCS_FILE "/cgroup.procs"
std::once_flag init_path_flag;
static const std::string& GetCgroupRootPath() {
static std::string cgroup_root_path;
std::call_once(init_path_flag, [&]() {
#ifdef __ANDROID__
// low-ram devices use per-app memcg by default, unlike high-end ones
bool low_ram_device = GetBoolProperty("ro.config.low_ram", false);
bool per_app_memcg =
GetBoolProperty("ro.config.per_app_memcg", low_ram_device);
#else
// host does not support Android properties
bool per_app_memcg = false;
#endif
if (per_app_memcg) {
// Check if mem cgroup is mounted, only then check for
// write-access to avoid SELinux denials
cgroup_root_path =
(access(MEM_CGROUP_TASKS, F_OK) || access(MEM_CGROUP_PATH, W_OK) ?
ACCT_CGROUP_PATH : MEM_CGROUP_PATH);
} else {
cgroup_root_path = ACCT_CGROUP_PATH;
}
});
return cgroup_root_path;
}
static std::string ConvertUidToPath(uid_t uid) {
return StringPrintf("%s/uid_%d", GetCgroupRootPath().c_str(), uid);
}
static std::string ConvertUidPidToPath(uid_t uid, int pid) {
return StringPrintf("%s/uid_%d/pid_%d", GetCgroupRootPath().c_str(), uid, pid);
}
static int RemoveProcessGroup(uid_t uid, int pid) {
int ret;
auto uid_pid_path = ConvertUidPidToPath(uid, pid);
ret = rmdir(uid_pid_path.c_str());
auto uid_path = ConvertUidToPath(uid);
rmdir(uid_path.c_str());
return ret;
}
static void RemoveUidProcessGroups(const std::string& uid_path) {
std::unique_ptr<DIR, decltype(&closedir)> uid(opendir(uid_path.c_str()), closedir);
if (uid != NULL) {
dirent* dir;
while ((dir = readdir(uid.get())) != nullptr) {
if (dir->d_type != DT_DIR) {
continue;
}
if (!StartsWith(dir->d_name, "pid_")) {
continue;
}
auto path = StringPrintf("%s/%s", uid_path.c_str(), dir->d_name);
LOG(VERBOSE) << "Removing " << path;
if (rmdir(path.c_str()) == -1) PLOG(WARNING) << "Failed to remove " << path;
}
}
}
void removeAllProcessGroups()
{
LOG(VERBOSE) << "removeAllProcessGroups()";
const auto& cgroup_root_path = GetCgroupRootPath();
std::unique_ptr<DIR, decltype(&closedir)> root(opendir(cgroup_root_path.c_str()), closedir);
if (root == NULL) {
PLOG(ERROR) << "Failed to open " << cgroup_root_path;
} else {
dirent* dir;
while ((dir = readdir(root.get())) != nullptr) {
if (dir->d_type != DT_DIR) {
continue;
}
if (!StartsWith(dir->d_name, "uid_")) {
continue;
}
auto path = StringPrintf("%s/%s", cgroup_root_path.c_str(), dir->d_name);
RemoveUidProcessGroups(path);
LOG(VERBOSE) << "Removing " << path;
if (rmdir(path.c_str()) == -1) PLOG(WARNING) << "Failed to remove " << path;
}
}
}
// Returns number of processes killed on success
// Returns 0 if there are no processes in the process cgroup left to kill
// Returns -1 on error
static int DoKillProcessGroupOnce(uid_t uid, int initialPid, int signal) {
auto path = ConvertUidPidToPath(uid, initialPid) + PROCESSGROUP_CGROUP_PROCS_FILE;
std::unique_ptr<FILE, decltype(&fclose)> fd(fopen(path.c_str(), "re"), fclose);
if (!fd) {
PLOG(WARNING) << "Failed to open process cgroup uid " << uid << " pid " << initialPid;
return -1;
}
// We separate all of the pids in the cgroup into those pids that are also the leaders of
// process groups (stored in the pgids set) and those that are not (stored in the pids set).
std::set<pid_t> pgids;
pgids.emplace(initialPid);
std::set<pid_t> pids;
pid_t pid;
int processes = 0;
while (fscanf(fd.get(), "%d\n", &pid) == 1 && pid >= 0) {
processes++;
if (pid == 0) {
// Should never happen... but if it does, trying to kill this
// will boomerang right back and kill us! Let's not let that happen.
LOG(WARNING) << "Yikes, we've been told to kill pid 0! How about we don't do that?";
continue;
}
pid_t pgid = getpgid(pid);
if (pgid == -1) PLOG(ERROR) << "getpgid(" << pid << ") failed";
if (pgid == pid) {
pgids.emplace(pid);
} else {
pids.emplace(pid);
}
}
// Erase all pids that will be killed when we kill the process groups.
for (auto it = pids.begin(); it != pids.end();) {
pid_t pgid = getpgid(pid);
if (pgids.count(pgid) == 1) {
it = pids.erase(it);
} else {
++it;
}
}
// Kill all process groups.
for (const auto pgid : pgids) {
LOG(VERBOSE) << "Killing process group " << -pgid << " in uid " << uid
<< " as part of process cgroup " << initialPid;
if (kill(-pgid, signal) == -1) {
PLOG(WARNING) << "kill(" << -pgid << ", " << signal << ") failed";
}
}
// Kill remaining pids.
for (const auto pid : pids) {
LOG(VERBOSE) << "Killing pid " << pid << " in uid " << uid << " as part of process cgroup "
<< initialPid;
if (kill(pid, signal) == -1) {
PLOG(WARNING) << "kill(" << pid << ", " << signal << ") failed";
}
}
return feof(fd.get()) ? processes : -1;
}
static int KillProcessGroup(uid_t uid, int initialPid, int signal, int retries) {
std::chrono::steady_clock::time_point start = std::chrono::steady_clock::now();
int retry = retries;
int processes;
while ((processes = DoKillProcessGroupOnce(uid, initialPid, signal)) > 0) {
LOG(VERBOSE) << "Killed " << processes << " processes for processgroup " << initialPid;
if (retry > 0) {
std::this_thread::sleep_for(5ms);
--retry;
} else {
break;
}
}
if (processes < 0) {
PLOG(ERROR) << "Error encountered killing process cgroup uid " << uid << " pid "
<< initialPid;
return -1;
}
std::chrono::steady_clock::time_point end = std::chrono::steady_clock::now();
auto ms = std::chrono::duration_cast<std::chrono::milliseconds>(end - start).count();
// We only calculate the number of 'processes' when killing the processes.
// In the retries == 0 case, we only kill the processes once and therefore
// will not have waited then recalculated how many processes are remaining
// after the first signals have been sent.
// Logging anything regarding the number of 'processes' here does not make sense.
if (processes == 0) {
if (retries > 0) {
LOG(INFO) << "Successfully killed process cgroup uid " << uid << " pid " << initialPid
<< " in " << static_cast<int>(ms) << "ms";
}
return RemoveProcessGroup(uid, initialPid);
} else {
if (retries > 0) {
LOG(ERROR) << "Failed to kill process cgroup uid " << uid << " pid " << initialPid
<< " in " << static_cast<int>(ms) << "ms, " << processes
<< " processes remain";
}
return -1;
}
}
int killProcessGroup(uid_t uid, int initialPid, int signal) {
return KillProcessGroup(uid, initialPid, signal, 40 /*retries*/);
}
int killProcessGroupOnce(uid_t uid, int initialPid, int signal) {
return KillProcessGroup(uid, initialPid, signal, 0 /*retries*/);
}
static bool MkdirAndChown(const std::string& path, mode_t mode, uid_t uid, gid_t gid) {
if (mkdir(path.c_str(), mode) == -1 && errno != EEXIST) {
return false;
}
if (chown(path.c_str(), uid, gid) == -1) {
int saved_errno = errno;
rmdir(path.c_str());
errno = saved_errno;
return false;
}
return true;
}
int createProcessGroup(uid_t uid, int initialPid)
{
auto uid_path = ConvertUidToPath(uid);
if (!MkdirAndChown(uid_path, 0750, AID_SYSTEM, AID_SYSTEM)) {
PLOG(ERROR) << "Failed to make and chown " << uid_path;
return -errno;
}
auto uid_pid_path = ConvertUidPidToPath(uid, initialPid);
if (!MkdirAndChown(uid_pid_path, 0750, AID_SYSTEM, AID_SYSTEM)) {
PLOG(ERROR) << "Failed to make and chown " << uid_pid_path;
return -errno;
}
auto uid_pid_procs_file = uid_pid_path + PROCESSGROUP_CGROUP_PROCS_FILE;
int ret = 0;
if (!WriteStringToFile(std::to_string(initialPid), uid_pid_procs_file)) {
ret = -errno;
PLOG(ERROR) << "Failed to write '" << initialPid << "' to " << uid_pid_procs_file;
}
return ret;
}
static bool SetProcessGroupValue(uid_t uid, int pid, const std::string& file_name, int64_t value) {
if (GetCgroupRootPath() != MEM_CGROUP_PATH) {
PLOG(ERROR) << "Memcg is not mounted.";
return false;
}
auto path = ConvertUidPidToPath(uid, pid) + file_name;
if (!WriteStringToFile(std::to_string(value), path)) {
PLOG(ERROR) << "Failed to write '" << value << "' to " << path;
return false;
}
return true;
}
bool setProcessGroupSwappiness(uid_t uid, int pid, int swappiness) {
return SetProcessGroupValue(uid, pid, "/memory.swappiness", swappiness);
}
bool setProcessGroupSoftLimit(uid_t uid, int pid, int64_t soft_limit_in_bytes) {
return SetProcessGroupValue(uid, pid, "/memory.soft_limit_in_bytes", soft_limit_in_bytes);
}
bool setProcessGroupLimit(uid_t uid, int pid, int64_t limit_in_bytes) {
return SetProcessGroupValue(uid, pid, "/memory.limit_in_bytes", limit_in_bytes);
}
|