summaryrefslogtreecommitdiffstats
blob: 42d4adb87f4ba76ef8245f965cd2fe35f9993f33 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
/*
 * Copyright (C) 2012 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef _LIBSPARSE_SPARSE_H_
#define _LIBSPARSE_SPARSE_H_

#include <stdbool.h>
#include <stdint.h>

#ifdef	__cplusplus
extern "C" {
#endif

struct sparse_file;

/**
 * sparse_file_new - create a new sparse file cookie
 *
 * @block_size - minimum size of a chunk
 * @len - size of the expanded sparse file.
 *
 * Creates a new sparse_file cookie that can be used to associate data
 * blocks.  Can later be written to a file with a variety of options.
 * block_size specifies the minimum size of a chunk in the file.  The maximum
 * size of the file is 2**32 * block_size (16TB for 4k block size).
 *
 * Returns the sparse file cookie, or NULL on error.
 */
struct sparse_file *sparse_file_new(unsigned int block_size, int64_t len);

/**
 * sparse_file_destroy - destroy a sparse file cookie
 *
 * @s - sparse file cookie
 *
 * Destroys a sparse file cookie.  After destroy, all memory passed in to
 * sparse_file_add_data can be freed by the caller
 */
void sparse_file_destroy(struct sparse_file *s);

/**
 * sparse_file_add_data - associate a data chunk with a sparse file
 *
 * @s - sparse file cookie
 * @data - pointer to data block
 * @len - length of the data block
 * @block - offset in blocks into the sparse file to place the data chunk
 *
 * Associates a data chunk with a sparse file cookie.  The region
 * [block * block_size : block * block_size + len) must not already be used in
 * the sparse file. If len is not a multiple of the block size the data
 * will be padded with zeros.
 *
 * The data pointer must remain valid until the sparse file is closed or the
 * data block is removed from the sparse file.
 *
 * Returns 0 on success, negative errno on error.
 */
int sparse_file_add_data(struct sparse_file *s,
		void *data, unsigned int len, unsigned int block);

/**
 * sparse_file_add_fill - associate a fill chunk with a sparse file
 *
 * @s - sparse file cookie
 * @fill_val - 32 bit fill data
 * @len - length of the fill block
 * @block - offset in blocks into the sparse file to place the fill chunk
 *
 * Associates a chunk filled with fill_val with a sparse file cookie.
 * The region [block * block_size : block * block_size + len) must not already
 * be used in the sparse file. If len is not a multiple of the block size the
 * data will be padded with zeros.
 *
 * Returns 0 on success, negative errno on error.
 */
int sparse_file_add_fill(struct sparse_file *s,
		uint32_t fill_val, unsigned int len, unsigned int block);

/**
 * sparse_file_add_file - associate a chunk of a file with a sparse file
 *
 * @s - sparse file cookie
 * @filename - filename of the file to be copied
 * @file_offset - offset into the copied file
 * @len - length of the copied block
 * @block - offset in blocks into the sparse file to place the file chunk
 *
 * Associates a chunk of an existing file with a sparse file cookie.
 * The region [block * block_size : block * block_size + len) must not already
 * be used in the sparse file. If len is not a multiple of the block size the
 * data will be padded with zeros.
 *
 * Allows adding large amounts of data to a sparse file without needing to keep
 * it all mapped.  File size is limited by available virtual address space,
 * exceptionally large files may need to be added in multiple chunks.
 *
 * Returns 0 on success, negative errno on error.
 */
int sparse_file_add_file(struct sparse_file *s,
		const char *filename, int64_t file_offset, unsigned int len,
		unsigned int block);

/**
 * sparse_file_add_file - associate a chunk of a file with a sparse file
 *
 * @s - sparse file cookie
 * @filename - filename of the file to be copied
 * @file_offset - offset into the copied file
 * @len - length of the copied block
 * @block - offset in blocks into the sparse file to place the file chunk
 *
 * Associates a chunk of an existing fd with a sparse file cookie.
 * The region [block * block_size : block * block_size + len) must not already
 * be used in the sparse file. If len is not a multiple of the block size the
 * data will be padded with zeros.
 *
 * Allows adding large amounts of data to a sparse file without needing to keep
 * it all mapped.  File size is limited by available virtual address space,
 * exceptionally large files may need to be added in multiple chunks.
 *
 * The fd must remain open until the sparse file is closed or the fd block is
 * removed from the sparse file.
 *
 * Returns 0 on success, negative errno on error.
 */
int sparse_file_add_fd(struct sparse_file *s,
		int fd, int64_t file_offset, unsigned int len, unsigned int block);

/**
 * sparse_file_write - write a sparse file to a file
 *
 * @s - sparse file cookie
 * @fd - file descriptor to write to
 * @gz - write a gzipped file
 * @sparse - write in the Android sparse file format
 * @crc - append a crc chunk
 *
 * Writes a sparse file to a file.  If gz is true, the data will be passed
 * through zlib.  If sparse is true, the file will be written in the Android
 * sparse file format.  If sparse is false, the file will be written by seeking
 * over unused chunks, producing a smaller file if the filesystem supports
 * sparse files.  If crc is true, the crc of the expanded data will be
 * calculated and appended in a crc chunk.
 *
 * Returns 0 on success, negative errno on error.
 */
int sparse_file_write(struct sparse_file *s, int fd, bool gz, bool sparse,
		bool crc);

/**
 * sparse_file_len - return the length of a sparse file if written to disk
 *
 * @s - sparse file cookie
 * @sparse - write in the Android sparse file format
 * @crc - append a crc chunk
 *
 * Returns the size a sparse file would be on disk if it were written in the
 * specified format.  If sparse is true, this is the size of the data in the
 * sparse format.  If sparse is false, this is the size of the normal
 * non-sparse file.
 */
int64_t sparse_file_len(struct sparse_file *s, bool sparse, bool crc);

/**
 * sparse_file_callback - call a callback for blocks in sparse file
 *
 * @s - sparse file cookie
 * @sparse - write in the Android sparse file format
 * @crc - append a crc chunk
 * @write - function to call for each block
 * @priv - value that will be passed as the first argument to write
 *
 * Writes a sparse file by calling a callback function.  If sparse is true, the
 * file will be written in the Android sparse file format.  If crc is true, the
 * crc of the expanded data will be calculated and appended in a crc chunk.
 * The callback 'write' will be called with data and length for each data,
 * and with data==NULL to skip over a region (only used for non-sparse format).
 * The callback should return negative on error, 0 on success.
 *
 * Returns 0 on success, negative errno on error.
 */
int sparse_file_callback(struct sparse_file *s, bool sparse, bool crc,
		int (*write)(void *priv, const void *data, int len), void *priv);

/**
 * sparse_file_read - read a file into a sparse file cookie
 *
 * @s - sparse file cookie
 * @fd - file descriptor to read from
 * @sparse - read a file in the Android sparse file format
 * @crc - verify the crc of a file in the Android sparse file format
 *
 * Reads a file into a sparse file cookie.  If sparse is true, the file is
 * assumed to be in the Android sparse file format.  If sparse is false, the
 * file will be sparsed by looking for block aligned chunks of all zeros or
 * another 32 bit value.  If crc is true, the crc of the sparse file will be
 * verified.
 *
 * Returns 0 on success, negative errno on error.
 */
int sparse_file_read(struct sparse_file *s, int fd, bool sparse, bool crc);

/**
 * sparse_file_import - import an existing sparse file
 *
 * @s - sparse file cookie
 * @verbose - print verbose errors while reading the sparse file
 * @crc - verify the crc of a file in the Android sparse file format
 *
 * Reads an existing sparse file into a sparse file cookie, recreating the same
 * sparse cookie that was used to write it.  If verbose is true, prints verbose
 * errors when the sparse file is formatted incorrectly.
 *
 * Returns a new sparse file cookie on success, NULL on error.
 */
struct sparse_file *sparse_file_import(int fd, bool verbose, bool crc);

/**
 * sparse_file_import_auto - import an existing sparse or normal file
 *
 * @fd - file descriptor to read from
 * @crc - verify the crc of a file in the Android sparse file format
 * @verbose - whether to use verbose logging
 *
 * Reads an existing sparse or normal file into a sparse file cookie.
 * Attempts to determine if the file is sparse or not by looking for the sparse
 * file magic number in the first 4 bytes.  If the file is not sparse, the file
 * will be sparsed by looking for block aligned chunks of all zeros or another
 * 32 bit value.  If crc is true, the crc of the sparse file will be verified.
 *
 * Returns a new sparse file cookie on success, NULL on error.
 */
struct sparse_file *sparse_file_import_auto(int fd, bool crc, bool verbose);

/** sparse_file_resparse - rechunk an existing sparse file into smaller files
 *
 * @in_s - sparse file cookie of the existing sparse file
 * @max_len - maximum file size
 * @out_s - array of sparse file cookies
 * @out_s_count - size of out_s array
 *
 * Splits chunks of an existing sparse file into smaller sparse files such that
 * each sparse file is less than max_len.  Returns the number of sparse_files
 * that would have been written to out_s if out_s were big enough.
 */
int sparse_file_resparse(struct sparse_file *in_s, unsigned int max_len,
		struct sparse_file **out_s, int out_s_count);

/**
 * sparse_file_verbose - set a sparse file cookie to print verbose errors
 *
 * @s - sparse file cookie
 *
 * Print verbose sparse file errors whenever using the sparse file cookie.
 */
void sparse_file_verbose(struct sparse_file *s);

/**
 * sparse_print_verbose - function called to print verbose errors
 *
 * By default, verbose errors will print to standard error.
 * sparse_print_verbose may be overridden to log verbose errors somewhere else.
 *
 */
extern void (*sparse_print_verbose)(const char *fmt, ...);

#ifdef	__cplusplus
}
#endif

#endif