1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
|
/*
* Copyright (C) 2006 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
//
// Encapsulate a shared file mapping.
//
#ifndef __LIBS_FILE_MAP_H
#define __LIBS_FILE_MAP_H
#include <sys/types.h>
#include <utils/Compat.h>
#if defined(__MINGW32__)
// Ensure that we always pull in winsock2.h before windows.h
#if defined(_WIN32)
#include <winsock2.h>
#endif
#include <windows.h>
#endif
namespace android {
/*
* This represents a memory-mapped file. It might be the entire file or
* only part of it. This requires a little bookkeeping because the mapping
* needs to be aligned on page boundaries, and in some cases we'd like to
* have multiple references to the mapped area without creating additional
* maps.
*
* This always uses MAP_SHARED.
*
* TODO: we should be able to create a new FileMap that is a subset of
* an existing FileMap and shares the underlying mapped pages. Requires
* completing the refcounting stuff and possibly introducing the notion
* of a FileMap hierarchy.
*/
class FileMap {
public:
FileMap(void);
FileMap(FileMap&& f);
FileMap& operator=(FileMap&& f);
/*
* Create a new mapping on an open file.
*
* Closing the file descriptor does not unmap the pages, so we don't
* claim ownership of the fd.
*
* Returns "false" on failure.
*/
bool create(const char* origFileName, int fd,
off64_t offset, size_t length, bool readOnly);
~FileMap(void);
/*
* Return the name of the file this map came from, if known.
*/
const char* getFileName(void) const { return mFileName; }
/*
* Get a pointer to the piece of the file we requested.
*/
void* getDataPtr(void) const { return mDataPtr; }
/*
* Get the length we requested.
*/
size_t getDataLength(void) const { return mDataLength; }
/*
* Get the data offset used to create this map.
*/
off64_t getDataOffset(void) const { return mDataOffset; }
/*
* This maps directly to madvise() values, but allows us to avoid
* including <sys/mman.h> everywhere.
*/
enum MapAdvice {
NORMAL, RANDOM, SEQUENTIAL, WILLNEED, DONTNEED
};
/*
* Apply an madvise() call to the entire file.
*
* Returns 0 on success, -1 on failure.
*/
int advise(MapAdvice advice);
protected:
private:
// these are not implemented
FileMap(const FileMap& src);
const FileMap& operator=(const FileMap& src);
char* mFileName; // original file name, if known
void* mBasePtr; // base of mmap area; page aligned
size_t mBaseLength; // length, measured from "mBasePtr"
off64_t mDataOffset; // offset used when map was created
void* mDataPtr; // start of requested data, offset from base
size_t mDataLength; // length, measured from "mDataPtr"
#if defined(__MINGW32__)
HANDLE mFileHandle; // Win32 file handle
HANDLE mFileMapping; // Win32 file mapping handle
#endif
static long mPageSize;
};
} // namespace android
#endif // __LIBS_FILE_MAP_H
|