1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
|
/*
* Copyright (C) 2010 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef UTILS_LOOPER_H
#define UTILS_LOOPER_H
#include <utils/threads.h>
#include <utils/RefBase.h>
#include <utils/KeyedVector.h>
#include <utils/Timers.h>
#include <sys/epoll.h>
#include <android-base/unique_fd.h>
namespace android {
/*
* NOTE: Since Looper is used to implement the NDK ALooper, the Looper
* enums and the signature of Looper_callbackFunc need to align with
* that implementation.
*/
/**
* For callback-based event loops, this is the prototype of the function
* that is called when a file descriptor event occurs.
* It is given the file descriptor it is associated with,
* a bitmask of the poll events that were triggered (typically EVENT_INPUT),
* and the data pointer that was originally supplied.
*
* Implementations should return 1 to continue receiving callbacks, or 0
* to have this file descriptor and callback unregistered from the looper.
*/
typedef int (*Looper_callbackFunc)(int fd, int events, void* data);
/**
* A message that can be posted to a Looper.
*/
struct Message {
Message() : what(0) { }
Message(int w) : what(w) { }
/* The message type. (interpretation is left up to the handler) */
int what;
};
/**
* Interface for a Looper message handler.
*
* The Looper holds a strong reference to the message handler whenever it has
* a message to deliver to it. Make sure to call Looper::removeMessages
* to remove any pending messages destined for the handler so that the handler
* can be destroyed.
*/
class MessageHandler : public virtual RefBase {
protected:
virtual ~MessageHandler();
public:
/**
* Handles a message.
*/
virtual void handleMessage(const Message& message) = 0;
};
/**
* A simple proxy that holds a weak reference to a message handler.
*/
class WeakMessageHandler : public MessageHandler {
protected:
virtual ~WeakMessageHandler();
public:
WeakMessageHandler(const wp<MessageHandler>& handler);
virtual void handleMessage(const Message& message);
private:
wp<MessageHandler> mHandler;
};
/**
* A looper callback.
*/
class LooperCallback : public virtual RefBase {
protected:
virtual ~LooperCallback();
public:
/**
* Handles a poll event for the given file descriptor.
* It is given the file descriptor it is associated with,
* a bitmask of the poll events that were triggered (typically EVENT_INPUT),
* and the data pointer that was originally supplied.
*
* Implementations should return 1 to continue receiving callbacks, or 0
* to have this file descriptor and callback unregistered from the looper.
*/
virtual int handleEvent(int fd, int events, void* data) = 0;
};
/**
* Wraps a Looper_callbackFunc function pointer.
*/
class SimpleLooperCallback : public LooperCallback {
protected:
virtual ~SimpleLooperCallback();
public:
SimpleLooperCallback(Looper_callbackFunc callback);
virtual int handleEvent(int fd, int events, void* data);
private:
Looper_callbackFunc mCallback;
};
/**
* A polling loop that supports monitoring file descriptor events, optionally
* using callbacks. The implementation uses epoll() internally.
*
* A looper can be associated with a thread although there is no requirement that it must be.
*/
class Looper : public RefBase {
protected:
virtual ~Looper();
public:
enum {
/**
* Result from Looper_pollOnce() and Looper_pollAll():
* The poll was awoken using wake() before the timeout expired
* and no callbacks were executed and no other file descriptors were ready.
*/
POLL_WAKE = -1,
/**
* Result from Looper_pollOnce() and Looper_pollAll():
* One or more callbacks were executed.
*/
POLL_CALLBACK = -2,
/**
* Result from Looper_pollOnce() and Looper_pollAll():
* The timeout expired.
*/
POLL_TIMEOUT = -3,
/**
* Result from Looper_pollOnce() and Looper_pollAll():
* An error occurred.
*/
POLL_ERROR = -4,
};
/**
* Flags for file descriptor events that a looper can monitor.
*
* These flag bits can be combined to monitor multiple events at once.
*/
enum {
/**
* The file descriptor is available for read operations.
*/
EVENT_INPUT = 1 << 0,
/**
* The file descriptor is available for write operations.
*/
EVENT_OUTPUT = 1 << 1,
/**
* The file descriptor has encountered an error condition.
*
* The looper always sends notifications about errors; it is not necessary
* to specify this event flag in the requested event set.
*/
EVENT_ERROR = 1 << 2,
/**
* The file descriptor was hung up.
* For example, indicates that the remote end of a pipe or socket was closed.
*
* The looper always sends notifications about hangups; it is not necessary
* to specify this event flag in the requested event set.
*/
EVENT_HANGUP = 1 << 3,
/**
* The file descriptor is invalid.
* For example, the file descriptor was closed prematurely.
*
* The looper always sends notifications about invalid file descriptors; it is not necessary
* to specify this event flag in the requested event set.
*/
EVENT_INVALID = 1 << 4,
};
enum {
/**
* Option for Looper_prepare: this looper will accept calls to
* Looper_addFd() that do not have a callback (that is provide NULL
* for the callback). In this case the caller of Looper_pollOnce()
* or Looper_pollAll() MUST check the return from these functions to
* discover when data is available on such fds and process it.
*/
PREPARE_ALLOW_NON_CALLBACKS = 1<<0
};
/**
* Creates a looper.
*
* If allowNonCallbaks is true, the looper will allow file descriptors to be
* registered without associated callbacks. This assumes that the caller of
* pollOnce() is prepared to handle callback-less events itself.
*/
Looper(bool allowNonCallbacks);
/**
* Returns whether this looper instance allows the registration of file descriptors
* using identifiers instead of callbacks.
*/
bool getAllowNonCallbacks() const;
/**
* Waits for events to be available, with optional timeout in milliseconds.
* Invokes callbacks for all file descriptors on which an event occurred.
*
* If the timeout is zero, returns immediately without blocking.
* If the timeout is negative, waits indefinitely until an event appears.
*
* Returns POLL_WAKE if the poll was awoken using wake() before
* the timeout expired and no callbacks were invoked and no other file
* descriptors were ready.
*
* Returns POLL_CALLBACK if one or more callbacks were invoked.
*
* Returns POLL_TIMEOUT if there was no data before the given
* timeout expired.
*
* Returns POLL_ERROR if an error occurred.
*
* Returns a value >= 0 containing an identifier if its file descriptor has data
* and it has no callback function (requiring the caller here to handle it).
* In this (and only this) case outFd, outEvents and outData will contain the poll
* events and data associated with the fd, otherwise they will be set to NULL.
*
* This method does not return until it has finished invoking the appropriate callbacks
* for all file descriptors that were signalled.
*/
int pollOnce(int timeoutMillis, int* outFd, int* outEvents, void** outData);
inline int pollOnce(int timeoutMillis) {
return pollOnce(timeoutMillis, nullptr, nullptr, nullptr);
}
/**
* Like pollOnce(), but performs all pending callbacks until all
* data has been consumed or a file descriptor is available with no callback.
* This function will never return POLL_CALLBACK.
*/
int pollAll(int timeoutMillis, int* outFd, int* outEvents, void** outData);
inline int pollAll(int timeoutMillis) {
return pollAll(timeoutMillis, nullptr, nullptr, nullptr);
}
/**
* Wakes the poll asynchronously.
*
* This method can be called on any thread.
* This method returns immediately.
*/
void wake();
/**
* Adds a new file descriptor to be polled by the looper.
* If the same file descriptor was previously added, it is replaced.
*
* "fd" is the file descriptor to be added.
* "ident" is an identifier for this event, which is returned from pollOnce().
* The identifier must be >= 0, or POLL_CALLBACK if providing a non-NULL callback.
* "events" are the poll events to wake up on. Typically this is EVENT_INPUT.
* "callback" is the function to call when there is an event on the file descriptor.
* "data" is a private data pointer to supply to the callback.
*
* There are two main uses of this function:
*
* (1) If "callback" is non-NULL, then this function will be called when there is
* data on the file descriptor. It should execute any events it has pending,
* appropriately reading from the file descriptor. The 'ident' is ignored in this case.
*
* (2) If "callback" is NULL, the 'ident' will be returned by Looper_pollOnce
* when its file descriptor has data available, requiring the caller to take
* care of processing it.
*
* Returns 1 if the file descriptor was added, 0 if the arguments were invalid.
*
* This method can be called on any thread.
* This method may block briefly if it needs to wake the poll.
*
* The callback may either be specified as a bare function pointer or as a smart
* pointer callback object. The smart pointer should be preferred because it is
* easier to avoid races when the callback is removed from a different thread.
* See removeFd() for details.
*/
int addFd(int fd, int ident, int events, Looper_callbackFunc callback, void* data);
int addFd(int fd, int ident, int events, const sp<LooperCallback>& callback, void* data);
/**
* Removes a previously added file descriptor from the looper.
*
* When this method returns, it is safe to close the file descriptor since the looper
* will no longer have a reference to it. However, it is possible for the callback to
* already be running or for it to run one last time if the file descriptor was already
* signalled. Calling code is responsible for ensuring that this case is safely handled.
* For example, if the callback takes care of removing itself during its own execution either
* by returning 0 or by calling this method, then it can be guaranteed to not be invoked
* again at any later time unless registered anew.
*
* A simple way to avoid this problem is to use the version of addFd() that takes
* a sp<LooperCallback> instead of a bare function pointer. The LooperCallback will
* be released at the appropriate time by the Looper.
*
* Returns 1 if the file descriptor was removed, 0 if none was previously registered.
*
* This method can be called on any thread.
* This method may block briefly if it needs to wake the poll.
*/
int removeFd(int fd);
/**
* Enqueues a message to be processed by the specified handler.
*
* The handler must not be null.
* This method can be called on any thread.
*/
void sendMessage(const sp<MessageHandler>& handler, const Message& message);
/**
* Enqueues a message to be processed by the specified handler after all pending messages
* after the specified delay.
*
* The time delay is specified in uptime nanoseconds.
* The handler must not be null.
* This method can be called on any thread.
*/
void sendMessageDelayed(nsecs_t uptimeDelay, const sp<MessageHandler>& handler,
const Message& message);
/**
* Enqueues a message to be processed by the specified handler after all pending messages
* at the specified time.
*
* The time is specified in uptime nanoseconds.
* The handler must not be null.
* This method can be called on any thread.
*/
void sendMessageAtTime(nsecs_t uptime, const sp<MessageHandler>& handler,
const Message& message);
/**
* Removes all messages for the specified handler from the queue.
*
* The handler must not be null.
* This method can be called on any thread.
*/
void removeMessages(const sp<MessageHandler>& handler);
/**
* Removes all messages of a particular type for the specified handler from the queue.
*
* The handler must not be null.
* This method can be called on any thread.
*/
void removeMessages(const sp<MessageHandler>& handler, int what);
/**
* Returns whether this looper's thread is currently polling for more work to do.
* This is a good signal that the loop is still alive rather than being stuck
* handling a callback. Note that this method is intrinsically racy, since the
* state of the loop can change before you get the result back.
*/
bool isPolling() const;
/**
* Prepares a looper associated with the calling thread, and returns it.
* If the thread already has a looper, it is returned. Otherwise, a new
* one is created, associated with the thread, and returned.
*
* The opts may be PREPARE_ALLOW_NON_CALLBACKS or 0.
*/
static sp<Looper> prepare(int opts);
/**
* Sets the given looper to be associated with the calling thread.
* If another looper is already associated with the thread, it is replaced.
*
* If "looper" is NULL, removes the currently associated looper.
*/
static void setForThread(const sp<Looper>& looper);
/**
* Returns the looper associated with the calling thread, or NULL if
* there is not one.
*/
static sp<Looper> getForThread();
private:
struct Request {
int fd;
int ident;
int events;
int seq;
sp<LooperCallback> callback;
void* data;
void initEventItem(struct epoll_event* eventItem) const;
};
struct Response {
int events;
Request request;
};
struct MessageEnvelope {
MessageEnvelope() : uptime(0) { }
MessageEnvelope(nsecs_t u, const sp<MessageHandler> h,
const Message& m) : uptime(u), handler(h), message(m) {
}
nsecs_t uptime;
sp<MessageHandler> handler;
Message message;
};
const bool mAllowNonCallbacks; // immutable
android::base::unique_fd mWakeEventFd; // immutable
Mutex mLock;
Vector<MessageEnvelope> mMessageEnvelopes; // guarded by mLock
bool mSendingMessage; // guarded by mLock
// Whether we are currently waiting for work. Not protected by a lock,
// any use of it is racy anyway.
volatile bool mPolling;
android::base::unique_fd mEpollFd; // guarded by mLock but only modified on the looper thread
bool mEpollRebuildRequired; // guarded by mLock
// Locked list of file descriptor monitoring requests.
KeyedVector<int, Request> mRequests; // guarded by mLock
int mNextRequestSeq;
// This state is only used privately by pollOnce and does not require a lock since
// it runs on a single thread.
Vector<Response> mResponses;
size_t mResponseIndex;
nsecs_t mNextMessageUptime; // set to LLONG_MAX when none
int pollInner(int timeoutMillis);
int removeFd(int fd, int seq);
void awoken();
void pushResponse(int events, const Request& request);
void rebuildEpollLocked();
void scheduleEpollRebuildLocked();
static void initTLSKey();
static void threadDestructor(void *st);
static void initEpollEvent(struct epoll_event* eventItem);
};
} // namespace android
#endif // UTILS_LOOPER_H
|