1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
591
592
593
594
595
596
597
598
599
600
601
602
603
604
605
606
607
608
609
610
611
612
613
614
615
616
617
618
619
620
621
622
623
624
625
626
627
628
629
630
631
632
633
634
635
636
637
638
639
640
641
642
643
644
645
646
647
648
649
650
651
652
653
654
655
656
657
658
659
660
661
662
663
664
665
666
667
668
669
670
671
672
673
674
675
676
677
678
679
680
681
682
683
684
685
686
687
688
689
690
|
/*
* Copyright (C) 2016 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
// SOME COMMENTS ABOUT USAGE:
// This provides primarily wp<> weak pointer types and RefBase, which work
// together with sp<> from <StrongPointer.h>.
// sp<> (and wp<>) are a type of smart pointer that use a well defined protocol
// to operate. As long as the object they are templated with implements that
// protocol, these smart pointers work. In several places the platform
// instantiates sp<> with non-RefBase objects; the two are not tied to each
// other.
// RefBase is such an implementation and it supports strong pointers, weak
// pointers and some magic features for the binder.
// So, when using RefBase objects, you have the ability to use strong and weak
// pointers through sp<> and wp<>.
// Normally, when the last strong pointer goes away, the object is destroyed,
// i.e. it's destructor is called. HOWEVER, parts of its associated memory is not
// freed until the last weak pointer is released.
// Weak pointers are essentially "safe" pointers. They are always safe to
// access through promote(). They may return nullptr if the object was
// destroyed because it ran out of strong pointers. This makes them good candidates
// for keys in a cache for instance.
// Weak pointers remain valid for comparison purposes even after the underlying
// object has been destroyed. Even if object A is destroyed and its memory reused
// for B, A remaining weak pointer to A will not compare equal to one to B.
// This again makes them attractive for use as keys.
// How is this supposed / intended to be used?
// Our recommendation is to use strong references (sp<>) when there is an
// ownership relation. e.g. when an object "owns" another one, use a strong
// ref. And of course use strong refs as arguments of functions (it's extremely
// rare that a function will take a wp<>).
// Typically a newly allocated object will immediately be used to initialize
// a strong pointer, which may then be used to construct or assign to other
// strong and weak pointers.
// Use weak references when there are no ownership relation. e.g. the keys in a
// cache (you cannot use plain pointers because there is no safe way to acquire
// a strong reference from a vanilla pointer).
// This implies that two objects should never (or very rarely) have sp<> on
// each other, because they can't both own each other.
// Caveats with reference counting
// Obviously, circular strong references are a big problem; this creates leaks
// and it's hard to debug -- except it's in fact really easy because RefBase has
// tons of debugging code for that. It can basically tell you exactly where the
// leak is.
// Another problem has to do with destructors with side effects. You must
// assume that the destructor of reference counted objects can be called AT ANY
// TIME. For instance code as simple as this:
// void setStuff(const sp<Stuff>& stuff) {
// std::lock_guard<std::mutex> lock(mMutex);
// mStuff = stuff;
// }
// is very dangerous. This code WILL deadlock one day or another.
// What isn't obvious is that ~Stuff() can be called as a result of the
// assignment. And it gets called with the lock held. First of all, the lock is
// protecting mStuff, not ~Stuff(). Secondly, if ~Stuff() uses its own internal
// mutex, now you have mutex ordering issues. Even worse, if ~Stuff() is
// virtual, now you're calling into "user" code (potentially), by that, I mean,
// code you didn't even write.
// A correct way to write this code is something like:
// void setStuff(const sp<Stuff>& stuff) {
// std::unique_lock<std::mutex> lock(mMutex);
// sp<Stuff> hold = mStuff;
// mStuff = stuff;
// lock.unlock();
// }
// More importantly, reference counted objects should do as little work as
// possible in their destructor, or at least be mindful that their destructor
// could be called from very weird and unintended places.
// Other more specific restrictions for wp<> and sp<>:
// Do not construct a strong pointer to "this" in an object's constructor.
// The onFirstRef() callback would be made on an incompletely constructed
// object.
// Construction of a weak pointer to "this" in an object's constructor is also
// discouraged. But the implementation was recently changed so that, in the
// absence of extendObjectLifetime() calls, weak pointers no longer impact
// object lifetime, and hence this no longer risks premature deallocation,
// and hence usually works correctly.
// Such strong or weak pointers can be safely created in the RefBase onFirstRef()
// callback.
// Use of wp::unsafe_get() for any purpose other than debugging is almost
// always wrong. Unless you somehow know that there is a longer-lived sp<> to
// the same object, it may well return a pointer to a deallocated object that
// has since been reallocated for a different purpose. (And if you know there
// is a longer-lived sp<>, why not use an sp<> directly?) A wp<> should only be
// dereferenced by using promote().
// Any object inheriting from RefBase should always be destroyed as the result
// of a reference count decrement, not via any other means. Such objects
// should never be stack allocated, or appear directly as data members in other
// objects. Objects inheriting from RefBase should have their strong reference
// count incremented as soon as possible after construction. Usually this
// will be done via construction of an sp<> to the object, but may instead
// involve other means of calling RefBase::incStrong().
// Explicitly deleting or otherwise destroying a RefBase object with outstanding
// wp<> or sp<> pointers to it will result in an abort or heap corruption.
// It is particularly important not to mix sp<> and direct storage management
// since the sp from raw pointer constructor is implicit. Thus if a RefBase-
// -derived object of type T is managed without ever incrementing its strong
// count, and accidentally passed to f(sp<T>), a strong pointer to the object
// will be temporarily constructed and destroyed, prematurely deallocating the
// object, and resulting in heap corruption. None of this would be easily
// visible in the source.
// Extra Features:
// RefBase::extendObjectLifetime() can be used to prevent destruction of the
// object while there are still weak references. This is really special purpose
// functionality to support Binder.
// Wp::promote(), implemented via the attemptIncStrong() member function, is
// used to try to convert a weak pointer back to a strong pointer. It's the
// normal way to try to access the fields of an object referenced only through
// a wp<>. Binder code also sometimes uses attemptIncStrong() directly.
// RefBase provides a number of additional callbacks for certain reference count
// events, as well as some debugging facilities.
// Debugging support can be enabled by turning on DEBUG_REFS in RefBase.cpp.
// Otherwise little checking is provided.
// Thread safety:
// Like std::shared_ptr, sp<> and wp<> allow concurrent accesses to DIFFERENT
// sp<> and wp<> instances that happen to refer to the same underlying object.
// They do NOT support concurrent access (where at least one access is a write)
// to THE SAME sp<> or wp<>. In effect, their thread-safety properties are
// exactly like those of T*, NOT atomic<T*>.
#ifndef ANDROID_REF_BASE_H
#define ANDROID_REF_BASE_H
#include <atomic>
#include <stdint.h>
#include <sys/types.h>
#include <stdlib.h>
#include <string.h>
// LightRefBase used to be declared in this header, so we have to include it
#include <utils/LightRefBase.h>
#include <utils/StrongPointer.h>
#include <utils/TypeHelpers.h>
// ---------------------------------------------------------------------------
namespace android {
class TextOutput;
TextOutput& printWeakPointer(TextOutput& to, const void* val);
// ---------------------------------------------------------------------------
#define COMPARE_WEAK(_op_) \
inline bool operator _op_ (const sp<T>& o) const { \
return m_ptr _op_ o.m_ptr; \
} \
inline bool operator _op_ (const T* o) const { \
return m_ptr _op_ o; \
} \
template<typename U> \
inline bool operator _op_ (const sp<U>& o) const { \
return m_ptr _op_ o.m_ptr; \
} \
template<typename U> \
inline bool operator _op_ (const U* o) const { \
return m_ptr _op_ o; \
}
// ---------------------------------------------------------------------------
// RefererenceRenamer is pure abstract, there is no virtual method
// implementation to put in a translation unit in order to silence the
// weak vtables warning.
#if defined(__clang__)
#pragma clang diagnostic push
#pragma clang diagnostic ignored "-Wweak-vtables"
#endif
class ReferenceRenamer {
protected:
// destructor is purposely not virtual so we avoid code overhead from
// subclasses; we have to make it protected to guarantee that it
// cannot be called from this base class (and to make strict compilers
// happy).
~ReferenceRenamer() { }
public:
virtual void operator()(size_t i) const = 0;
};
#if defined(__clang__)
#pragma clang diagnostic pop
#endif
// ---------------------------------------------------------------------------
class RefBase
{
public:
void incStrong(const void* id) const;
void decStrong(const void* id) const;
void forceIncStrong(const void* id) const;
//! DEBUGGING ONLY: Get current strong ref count.
int32_t getStrongCount() const;
class weakref_type
{
public:
RefBase* refBase() const;
void incWeak(const void* id);
void decWeak(const void* id);
// acquires a strong reference if there is already one.
bool attemptIncStrong(const void* id);
// acquires a weak reference if there is already one.
// This is not always safe. see ProcessState.cpp and BpBinder.cpp
// for proper use.
bool attemptIncWeak(const void* id);
//! DEBUGGING ONLY: Get current weak ref count.
int32_t getWeakCount() const;
//! DEBUGGING ONLY: Print references held on object.
void printRefs() const;
//! DEBUGGING ONLY: Enable tracking for this object.
// enable -- enable/disable tracking
// retain -- when tracking is enable, if true, then we save a stack trace
// for each reference and dereference; when retain == false, we
// match up references and dereferences and keep only the
// outstanding ones.
void trackMe(bool enable, bool retain);
};
weakref_type* createWeak(const void* id) const;
weakref_type* getWeakRefs() const;
//! DEBUGGING ONLY: Print references held on object.
inline void printRefs() const { getWeakRefs()->printRefs(); }
//! DEBUGGING ONLY: Enable tracking of object.
inline void trackMe(bool enable, bool retain)
{
getWeakRefs()->trackMe(enable, retain);
}
typedef RefBase basetype;
protected:
RefBase();
virtual ~RefBase();
//! Flags for extendObjectLifetime()
enum {
OBJECT_LIFETIME_STRONG = 0x0000,
OBJECT_LIFETIME_WEAK = 0x0001,
OBJECT_LIFETIME_MASK = 0x0001
};
void extendObjectLifetime(int32_t mode);
//! Flags for onIncStrongAttempted()
enum {
FIRST_INC_STRONG = 0x0001
};
// Invoked after creation of initial strong pointer/reference.
virtual void onFirstRef();
// Invoked when either the last strong reference goes away, or we need to undo
// the effect of an unnecessary onIncStrongAttempted.
virtual void onLastStrongRef(const void* id);
// Only called in OBJECT_LIFETIME_WEAK case. Returns true if OK to promote to
// strong reference. May have side effects if it returns true.
// The first flags argument is always FIRST_INC_STRONG.
// TODO: Remove initial flag argument.
virtual bool onIncStrongAttempted(uint32_t flags, const void* id);
// Invoked in the OBJECT_LIFETIME_WEAK case when the last reference of either
// kind goes away. Unused.
// TODO: Remove.
virtual void onLastWeakRef(const void* id);
private:
friend class weakref_type;
class weakref_impl;
RefBase(const RefBase& o);
RefBase& operator=(const RefBase& o);
private:
friend class ReferenceMover;
static void renameRefs(size_t n, const ReferenceRenamer& renamer);
static void renameRefId(weakref_type* ref,
const void* old_id, const void* new_id);
static void renameRefId(RefBase* ref,
const void* old_id, const void* new_id);
weakref_impl* const mRefs;
};
// ---------------------------------------------------------------------------
template <typename T>
class wp
{
public:
typedef typename RefBase::weakref_type weakref_type;
inline wp() : m_ptr(0) { }
wp(T* other); // NOLINT(implicit)
wp(const wp<T>& other);
explicit wp(const sp<T>& other);
template<typename U> wp(U* other); // NOLINT(implicit)
template<typename U> wp(const sp<U>& other); // NOLINT(implicit)
template<typename U> wp(const wp<U>& other); // NOLINT(implicit)
~wp();
// Assignment
wp& operator = (T* other);
wp& operator = (const wp<T>& other);
wp& operator = (const sp<T>& other);
template<typename U> wp& operator = (U* other);
template<typename U> wp& operator = (const wp<U>& other);
template<typename U> wp& operator = (const sp<U>& other);
void set_object_and_refs(T* other, weakref_type* refs);
// promotion to sp
sp<T> promote() const;
// Reset
void clear();
// Accessors
inline weakref_type* get_refs() const { return m_refs; }
inline T* unsafe_get() const { return m_ptr; }
// Operators
COMPARE_WEAK(==)
COMPARE_WEAK(!=)
COMPARE_WEAK(>)
COMPARE_WEAK(<)
COMPARE_WEAK(<=)
COMPARE_WEAK(>=)
inline bool operator == (const wp<T>& o) const {
return (m_ptr == o.m_ptr) && (m_refs == o.m_refs);
}
template<typename U>
inline bool operator == (const wp<U>& o) const {
return m_ptr == o.m_ptr;
}
inline bool operator > (const wp<T>& o) const {
return (m_ptr == o.m_ptr) ? (m_refs > o.m_refs) : (m_ptr > o.m_ptr);
}
template<typename U>
inline bool operator > (const wp<U>& o) const {
return (m_ptr == o.m_ptr) ? (m_refs > o.m_refs) : (m_ptr > o.m_ptr);
}
inline bool operator < (const wp<T>& o) const {
return (m_ptr == o.m_ptr) ? (m_refs < o.m_refs) : (m_ptr < o.m_ptr);
}
template<typename U>
inline bool operator < (const wp<U>& o) const {
return (m_ptr == o.m_ptr) ? (m_refs < o.m_refs) : (m_ptr < o.m_ptr);
}
inline bool operator != (const wp<T>& o) const { return m_refs != o.m_refs; }
template<typename U> inline bool operator != (const wp<U>& o) const { return !operator == (o); }
inline bool operator <= (const wp<T>& o) const { return !operator > (o); }
template<typename U> inline bool operator <= (const wp<U>& o) const { return !operator > (o); }
inline bool operator >= (const wp<T>& o) const { return !operator < (o); }
template<typename U> inline bool operator >= (const wp<U>& o) const { return !operator < (o); }
private:
template<typename Y> friend class sp;
template<typename Y> friend class wp;
T* m_ptr;
weakref_type* m_refs;
};
template <typename T>
TextOutput& operator<<(TextOutput& to, const wp<T>& val);
#undef COMPARE_WEAK
// ---------------------------------------------------------------------------
// No user serviceable parts below here.
template<typename T>
wp<T>::wp(T* other)
: m_ptr(other)
{
if (other) m_refs = other->createWeak(this);
}
template<typename T>
wp<T>::wp(const wp<T>& other)
: m_ptr(other.m_ptr), m_refs(other.m_refs)
{
if (m_ptr) m_refs->incWeak(this);
}
template<typename T>
wp<T>::wp(const sp<T>& other)
: m_ptr(other.m_ptr)
{
if (m_ptr) {
m_refs = m_ptr->createWeak(this);
}
}
template<typename T> template<typename U>
wp<T>::wp(U* other)
: m_ptr(other)
{
if (other) m_refs = other->createWeak(this);
}
template<typename T> template<typename U>
wp<T>::wp(const wp<U>& other)
: m_ptr(other.m_ptr)
{
if (m_ptr) {
m_refs = other.m_refs;
m_refs->incWeak(this);
}
}
template<typename T> template<typename U>
wp<T>::wp(const sp<U>& other)
: m_ptr(other.m_ptr)
{
if (m_ptr) {
m_refs = m_ptr->createWeak(this);
}
}
template<typename T>
wp<T>::~wp()
{
if (m_ptr) m_refs->decWeak(this);
}
template<typename T>
wp<T>& wp<T>::operator = (T* other)
{
weakref_type* newRefs =
other ? other->createWeak(this) : 0;
if (m_ptr) m_refs->decWeak(this);
m_ptr = other;
m_refs = newRefs;
return *this;
}
template<typename T>
wp<T>& wp<T>::operator = (const wp<T>& other)
{
weakref_type* otherRefs(other.m_refs);
T* otherPtr(other.m_ptr);
if (otherPtr) otherRefs->incWeak(this);
if (m_ptr) m_refs->decWeak(this);
m_ptr = otherPtr;
m_refs = otherRefs;
return *this;
}
template<typename T>
wp<T>& wp<T>::operator = (const sp<T>& other)
{
weakref_type* newRefs =
other != NULL ? other->createWeak(this) : 0;
T* otherPtr(other.m_ptr);
if (m_ptr) m_refs->decWeak(this);
m_ptr = otherPtr;
m_refs = newRefs;
return *this;
}
template<typename T> template<typename U>
wp<T>& wp<T>::operator = (U* other)
{
weakref_type* newRefs =
other ? other->createWeak(this) : 0;
if (m_ptr) m_refs->decWeak(this);
m_ptr = other;
m_refs = newRefs;
return *this;
}
template<typename T> template<typename U>
wp<T>& wp<T>::operator = (const wp<U>& other)
{
weakref_type* otherRefs(other.m_refs);
U* otherPtr(other.m_ptr);
if (otherPtr) otherRefs->incWeak(this);
if (m_ptr) m_refs->decWeak(this);
m_ptr = otherPtr;
m_refs = otherRefs;
return *this;
}
template<typename T> template<typename U>
wp<T>& wp<T>::operator = (const sp<U>& other)
{
weakref_type* newRefs =
other != NULL ? other->createWeak(this) : 0;
U* otherPtr(other.m_ptr);
if (m_ptr) m_refs->decWeak(this);
m_ptr = otherPtr;
m_refs = newRefs;
return *this;
}
template<typename T>
void wp<T>::set_object_and_refs(T* other, weakref_type* refs)
{
if (other) refs->incWeak(this);
if (m_ptr) m_refs->decWeak(this);
m_ptr = other;
m_refs = refs;
}
template<typename T>
sp<T> wp<T>::promote() const
{
sp<T> result;
if (m_ptr && m_refs->attemptIncStrong(&result)) {
result.set_pointer(m_ptr);
}
return result;
}
template<typename T>
void wp<T>::clear()
{
if (m_ptr) {
m_refs->decWeak(this);
m_ptr = 0;
}
}
template <typename T>
inline TextOutput& operator<<(TextOutput& to, const wp<T>& val)
{
return printWeakPointer(to, val.unsafe_get());
}
// ---------------------------------------------------------------------------
// this class just serves as a namespace so TYPE::moveReferences can stay
// private.
class ReferenceMover {
public:
// it would be nice if we could make sure no extra code is generated
// for sp<TYPE> or wp<TYPE> when TYPE is a descendant of RefBase:
// Using a sp<RefBase> override doesn't work; it's a bit like we wanted
// a template<typename TYPE inherits RefBase> template...
template<typename TYPE> static inline
void move_references(sp<TYPE>* dest, sp<TYPE> const* src, size_t n) {
class Renamer : public ReferenceRenamer {
sp<TYPE>* d_;
sp<TYPE> const* s_;
virtual void operator()(size_t i) const {
// The id are known to be the sp<>'s this pointer
TYPE::renameRefId(d_[i].get(), &s_[i], &d_[i]);
}
public:
Renamer(sp<TYPE>* d, sp<TYPE> const* s) : d_(d), s_(s) { }
virtual ~Renamer() { }
};
memmove(dest, src, n*sizeof(sp<TYPE>));
TYPE::renameRefs(n, Renamer(dest, src));
}
template<typename TYPE> static inline
void move_references(wp<TYPE>* dest, wp<TYPE> const* src, size_t n) {
class Renamer : public ReferenceRenamer {
wp<TYPE>* d_;
wp<TYPE> const* s_;
virtual void operator()(size_t i) const {
// The id are known to be the wp<>'s this pointer
TYPE::renameRefId(d_[i].get_refs(), &s_[i], &d_[i]);
}
public:
Renamer(wp<TYPE>* rd, wp<TYPE> const* rs) : d_(rd), s_(rs) { }
virtual ~Renamer() { }
};
memmove(dest, src, n*sizeof(wp<TYPE>));
TYPE::renameRefs(n, Renamer(dest, src));
}
};
// specialization for moving sp<> and wp<> types.
// these are used by the [Sorted|Keyed]Vector<> implementations
// sp<> and wp<> need to be handled specially, because they do not
// have trivial copy operation in the general case (see RefBase.cpp
// when DEBUG ops are enabled), but can be implemented very
// efficiently in most cases.
template<typename TYPE> inline
void move_forward_type(sp<TYPE>* d, sp<TYPE> const* s, size_t n) {
ReferenceMover::move_references(d, s, n);
}
template<typename TYPE> inline
void move_backward_type(sp<TYPE>* d, sp<TYPE> const* s, size_t n) {
ReferenceMover::move_references(d, s, n);
}
template<typename TYPE> inline
void move_forward_type(wp<TYPE>* d, wp<TYPE> const* s, size_t n) {
ReferenceMover::move_references(d, s, n);
}
template<typename TYPE> inline
void move_backward_type(wp<TYPE>* d, wp<TYPE> const* s, size_t n) {
ReferenceMover::move_references(d, s, n);
}
} // namespace android
// ---------------------------------------------------------------------------
#endif // ANDROID_REF_BASE_H
|