1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
|
/*
* Copyright (C) 2008 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef LIBZIPARCHIVE_ZIPARCHIVE_PRIVATE_H_
#define LIBZIPARCHIVE_ZIPARCHIVE_PRIVATE_H_
#include <stdint.h>
#include <stdlib.h>
#include <unistd.h>
#include <memory>
#include <vector>
#include <utils/FileMap.h>
#include <ziparchive/zip_archive.h>
#include "android-base/macros.h"
static const char* kErrorMessages[] = {
"Success",
"Iteration ended",
"Zlib error",
"Invalid file",
"Invalid handle",
"Duplicate entries in archive",
"Empty archive",
"Entry not found",
"Invalid offset",
"Inconsistent information",
"Invalid entry name",
"I/O error",
"File mapping failed",
};
enum ErrorCodes : int32_t {
kIterationEnd = -1,
// We encountered a Zlib error when inflating a stream from this file.
// Usually indicates file corruption.
kZlibError = -2,
// The input file cannot be processed as a zip archive. Usually because
// it's too small, too large or does not have a valid signature.
kInvalidFile = -3,
// An invalid iteration / ziparchive handle was passed in as an input
// argument.
kInvalidHandle = -4,
// The zip archive contained two (or possibly more) entries with the same
// name.
kDuplicateEntry = -5,
// The zip archive contains no entries.
kEmptyArchive = -6,
// The specified entry was not found in the archive.
kEntryNotFound = -7,
// The zip archive contained an invalid local file header pointer.
kInvalidOffset = -8,
// The zip archive contained inconsistent entry information. This could
// be because the central directory & local file header did not agree, or
// if the actual uncompressed length or crc32 do not match their declared
// values.
kInconsistentInformation = -9,
// An invalid entry name was encountered.
kInvalidEntryName = -10,
// An I/O related system call (read, lseek, ftruncate, map) failed.
kIoError = -11,
// We were not able to mmap the central directory or entry contents.
kMmapFailed = -12,
kLastErrorCode = kMmapFailed,
};
class MappedZipFile {
public:
explicit MappedZipFile(const int fd)
: has_fd_(true), fd_(fd), base_ptr_(nullptr), data_length_(0) {}
explicit MappedZipFile(void* address, size_t length)
: has_fd_(false), fd_(-1), base_ptr_(address), data_length_(static_cast<off64_t>(length)) {}
bool HasFd() const { return has_fd_; }
int GetFileDescriptor() const;
void* GetBasePtr() const;
off64_t GetFileLength() const;
bool ReadAtOffset(uint8_t* buf, size_t len, off64_t off) const;
private:
// If has_fd_ is true, fd is valid and we'll read contents of a zip archive
// from the file. Otherwise, we're opening the archive from a memory mapped
// file. In that case, base_ptr_ points to the start of the memory region and
// data_length_ defines the file length.
const bool has_fd_;
const int fd_;
void* const base_ptr_;
const off64_t data_length_;
};
class CentralDirectory {
public:
CentralDirectory(void) : base_ptr_(nullptr), length_(0) {}
const uint8_t* GetBasePtr() const { return base_ptr_; }
size_t GetMapLength() const { return length_; }
void Initialize(void* map_base_ptr, off64_t cd_start_offset, size_t cd_size);
private:
const uint8_t* base_ptr_;
size_t length_;
};
struct ZipArchive {
// open Zip archive
mutable MappedZipFile mapped_zip;
const bool close_file;
// mapped central directory area
off64_t directory_offset;
CentralDirectory central_directory;
std::unique_ptr<android::FileMap> directory_map;
// number of entries in the Zip archive
uint16_t num_entries;
// We know how many entries are in the Zip archive, so we can have a
// fixed-size hash table. We define a load factor of 0.75 and over
// allocate so the maximum number entries can never be higher than
// ((4 * UINT16_MAX) / 3 + 1) which can safely fit into a uint32_t.
uint32_t hash_table_size;
ZipString* hash_table;
ZipArchive(const int fd, bool assume_ownership);
ZipArchive(void* address, size_t length);
~ZipArchive();
bool InitializeCentralDirectory(const char* debug_file_name, off64_t cd_start_offset,
size_t cd_size);
};
#endif // LIBZIPARCHIVE_ZIPARCHIVE_PRIVATE_H_
|