summaryrefslogtreecommitdiffstats
blob: 6ad3366e4622a85b7b18eb705d1ef1a4ae682f6c (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
/*
 * Copyright (C) 2015 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include "ziparchive/zip_writer.h"

#include <sys/param.h>
#include <sys/stat.h>
#include <zlib.h>
#include <cstdio>
#define DEF_MEM_LEVEL 8  // normally in zutil.h?

#include <memory>
#include <vector>

#include "android-base/logging.h"
#include "utils/Compat.h"
#include "utils/Log.h"

#include "entry_name_utils-inl.h"
#include "zip_archive_common.h"

#if !defined(powerof2)
#define powerof2(x) ((((x)-1) & (x)) == 0)
#endif

/* Zip compression methods we support */
enum {
  kCompressStored = 0,    // no compression
  kCompressDeflated = 8,  // standard deflate
};

// Size of the output buffer used for compression.
static const size_t kBufSize = 32768u;

// No error, operation completed successfully.
static const int32_t kNoError = 0;

// The ZipWriter is in a bad state.
static const int32_t kInvalidState = -1;

// There was an IO error while writing to disk.
static const int32_t kIoError = -2;

// The zip entry name was invalid.
static const int32_t kInvalidEntryName = -3;

// An error occurred in zlib.
static const int32_t kZlibError = -4;

// The start aligned function was called with the aligned flag.
static const int32_t kInvalidAlign32Flag = -5;

// The alignment parameter is not a power of 2.
static const int32_t kInvalidAlignment = -6;

static const char* sErrorCodes[] = {
    "Invalid state", "IO error", "Invalid entry name", "Zlib error",
};

const char* ZipWriter::ErrorCodeString(int32_t error_code) {
  if (error_code < 0 && (-error_code) < static_cast<int32_t>(arraysize(sErrorCodes))) {
    return sErrorCodes[-error_code];
  }
  return nullptr;
}

static void DeleteZStream(z_stream* stream) {
  deflateEnd(stream);
  delete stream;
}

ZipWriter::ZipWriter(FILE* f)
    : file_(f),
      seekable_(false),
      current_offset_(0),
      state_(State::kWritingZip),
      z_stream_(nullptr, DeleteZStream),
      buffer_(kBufSize) {
  // Check if the file is seekable (regular file). If fstat fails, that's fine, subsequent calls
  // will fail as well.
  struct stat file_stats;
  if (fstat(fileno(f), &file_stats) == 0) {
    seekable_ = S_ISREG(file_stats.st_mode);
  }
}

ZipWriter::ZipWriter(ZipWriter&& writer)
    : file_(writer.file_),
      seekable_(writer.seekable_),
      current_offset_(writer.current_offset_),
      state_(writer.state_),
      files_(std::move(writer.files_)),
      z_stream_(std::move(writer.z_stream_)),
      buffer_(std::move(writer.buffer_)) {
  writer.file_ = nullptr;
  writer.state_ = State::kError;
}

ZipWriter& ZipWriter::operator=(ZipWriter&& writer) {
  file_ = writer.file_;
  seekable_ = writer.seekable_;
  current_offset_ = writer.current_offset_;
  state_ = writer.state_;
  files_ = std::move(writer.files_);
  z_stream_ = std::move(writer.z_stream_);
  buffer_ = std::move(writer.buffer_);
  writer.file_ = nullptr;
  writer.state_ = State::kError;
  return *this;
}

int32_t ZipWriter::HandleError(int32_t error_code) {
  state_ = State::kError;
  z_stream_.reset();
  return error_code;
}

int32_t ZipWriter::StartEntry(const char* path, size_t flags) {
  uint32_t alignment = 0;
  if (flags & kAlign32) {
    flags &= ~kAlign32;
    alignment = 4;
  }
  return StartAlignedEntryWithTime(path, flags, time_t(), alignment);
}

int32_t ZipWriter::StartAlignedEntry(const char* path, size_t flags, uint32_t alignment) {
  return StartAlignedEntryWithTime(path, flags, time_t(), alignment);
}

int32_t ZipWriter::StartEntryWithTime(const char* path, size_t flags, time_t time) {
  uint32_t alignment = 0;
  if (flags & kAlign32) {
    flags &= ~kAlign32;
    alignment = 4;
  }
  return StartAlignedEntryWithTime(path, flags, time, alignment);
}

static void ExtractTimeAndDate(time_t when, uint16_t* out_time, uint16_t* out_date) {
  /* round up to an even number of seconds */
  when = static_cast<time_t>((static_cast<unsigned long>(when) + 1) & (~1));

  struct tm* ptm;
#if !defined(_WIN32)
  struct tm tm_result;
  ptm = localtime_r(&when, &tm_result);
#else
  ptm = localtime(&when);
#endif

  int year = ptm->tm_year;
  if (year < 80) {
    year = 80;
  }

  *out_date = (year - 80) << 9 | (ptm->tm_mon + 1) << 5 | ptm->tm_mday;
  *out_time = ptm->tm_hour << 11 | ptm->tm_min << 5 | ptm->tm_sec >> 1;
}

static void CopyFromFileEntry(const ZipWriter::FileEntry& src, bool use_data_descriptor,
                              LocalFileHeader* dst) {
  dst->lfh_signature = LocalFileHeader::kSignature;
  if (use_data_descriptor) {
    // Set this flag to denote that a DataDescriptor struct will appear after the data,
    // containing the crc and size fields.
    dst->gpb_flags |= kGPBDDFlagMask;

    // The size and crc fields must be 0.
    dst->compressed_size = 0u;
    dst->uncompressed_size = 0u;
    dst->crc32 = 0u;
  } else {
    dst->compressed_size = src.compressed_size;
    dst->uncompressed_size = src.uncompressed_size;
    dst->crc32 = src.crc32;
  }
  dst->compression_method = src.compression_method;
  dst->last_mod_time = src.last_mod_time;
  dst->last_mod_date = src.last_mod_date;
  dst->file_name_length = src.path.size();
  dst->extra_field_length = src.padding_length;
}

int32_t ZipWriter::StartAlignedEntryWithTime(const char* path, size_t flags, time_t time,
                                             uint32_t alignment) {
  if (state_ != State::kWritingZip) {
    return kInvalidState;
  }

  if (flags & kAlign32) {
    return kInvalidAlign32Flag;
  }

  if (powerof2(alignment) == 0) {
    return kInvalidAlignment;
  }

  FileEntry file_entry = {};
  file_entry.local_file_header_offset = current_offset_;
  file_entry.path = path;

  if (!IsValidEntryName(reinterpret_cast<const uint8_t*>(file_entry.path.data()),
                        file_entry.path.size())) {
    return kInvalidEntryName;
  }

  if (flags & ZipWriter::kCompress) {
    file_entry.compression_method = kCompressDeflated;

    int32_t result = PrepareDeflate();
    if (result != kNoError) {
      return result;
    }
  } else {
    file_entry.compression_method = kCompressStored;
  }

  ExtractTimeAndDate(time, &file_entry.last_mod_time, &file_entry.last_mod_date);

  off_t offset = current_offset_ + sizeof(LocalFileHeader) + file_entry.path.size();
  std::vector<char> zero_padding;
  if (alignment != 0 && (offset & (alignment - 1))) {
    // Pad the extra field so the data will be aligned.
    uint16_t padding = alignment - (offset % alignment);
    file_entry.padding_length = padding;
    offset += padding;
    zero_padding.resize(padding, 0);
  }

  LocalFileHeader header = {};
  // Always start expecting a data descriptor. When the data has finished being written,
  // if it is possible to seek back, the GPB flag will reset and the sizes written.
  CopyFromFileEntry(file_entry, true /*use_data_descriptor*/, &header);

  if (fwrite(&header, sizeof(header), 1, file_) != 1) {
    return HandleError(kIoError);
  }

  if (fwrite(path, sizeof(*path), file_entry.path.size(), file_) != file_entry.path.size()) {
    return HandleError(kIoError);
  }

  if (file_entry.padding_length != 0 && fwrite(zero_padding.data(), 1, file_entry.padding_length,
                                               file_) != file_entry.padding_length) {
    return HandleError(kIoError);
  }

  current_file_entry_ = std::move(file_entry);
  current_offset_ = offset;
  state_ = State::kWritingEntry;
  return kNoError;
}

int32_t ZipWriter::DiscardLastEntry() {
  if (state_ != State::kWritingZip || files_.empty()) {
    return kInvalidState;
  }

  FileEntry& last_entry = files_.back();
  current_offset_ = last_entry.local_file_header_offset;
  if (fseeko(file_, current_offset_, SEEK_SET) != 0) {
    return HandleError(kIoError);
  }
  files_.pop_back();
  return kNoError;
}

int32_t ZipWriter::GetLastEntry(FileEntry* out_entry) {
  CHECK(out_entry != nullptr);

  if (files_.empty()) {
    return kInvalidState;
  }
  *out_entry = files_.back();
  return kNoError;
}

int32_t ZipWriter::PrepareDeflate() {
  CHECK(state_ == State::kWritingZip);

  // Initialize the z_stream for compression.
  z_stream_ = std::unique_ptr<z_stream, void (*)(z_stream*)>(new z_stream(), DeleteZStream);

#pragma GCC diagnostic push
#pragma GCC diagnostic ignored "-Wold-style-cast"
  int zerr = deflateInit2(z_stream_.get(), Z_BEST_COMPRESSION, Z_DEFLATED, -MAX_WBITS,
                          DEF_MEM_LEVEL, Z_DEFAULT_STRATEGY);
#pragma GCC diagnostic pop

  if (zerr != Z_OK) {
    if (zerr == Z_VERSION_ERROR) {
      ALOGE("Installed zlib is not compatible with linked version (%s)", ZLIB_VERSION);
      return HandleError(kZlibError);
    } else {
      ALOGE("deflateInit2 failed (zerr=%d)", zerr);
      return HandleError(kZlibError);
    }
  }

  z_stream_->next_out = buffer_.data();
  z_stream_->avail_out = buffer_.size();
  return kNoError;
}

int32_t ZipWriter::WriteBytes(const void* data, size_t len) {
  if (state_ != State::kWritingEntry) {
    return HandleError(kInvalidState);
  }

  int32_t result = kNoError;
  if (current_file_entry_.compression_method & kCompressDeflated) {
    result = CompressBytes(&current_file_entry_, data, len);
  } else {
    result = StoreBytes(&current_file_entry_, data, len);
  }

  if (result != kNoError) {
    return result;
  }

  current_file_entry_.crc32 =
      crc32(current_file_entry_.crc32, reinterpret_cast<const Bytef*>(data), len);
  current_file_entry_.uncompressed_size += len;
  return kNoError;
}

int32_t ZipWriter::StoreBytes(FileEntry* file, const void* data, size_t len) {
  CHECK(state_ == State::kWritingEntry);

  if (fwrite(data, 1, len, file_) != len) {
    return HandleError(kIoError);
  }
  file->compressed_size += len;
  current_offset_ += len;
  return kNoError;
}

int32_t ZipWriter::CompressBytes(FileEntry* file, const void* data, size_t len) {
  CHECK(state_ == State::kWritingEntry);
  CHECK(z_stream_);
  CHECK(z_stream_->next_out != nullptr);
  CHECK(z_stream_->avail_out != 0);

  // Prepare the input.
  z_stream_->next_in = reinterpret_cast<const uint8_t*>(data);
  z_stream_->avail_in = len;

  while (z_stream_->avail_in > 0) {
    // We have more data to compress.
    int zerr = deflate(z_stream_.get(), Z_NO_FLUSH);
    if (zerr != Z_OK) {
      return HandleError(kZlibError);
    }

    if (z_stream_->avail_out == 0) {
      // The output is full, let's write it to disk.
      size_t write_bytes = z_stream_->next_out - buffer_.data();
      if (fwrite(buffer_.data(), 1, write_bytes, file_) != write_bytes) {
        return HandleError(kIoError);
      }
      file->compressed_size += write_bytes;
      current_offset_ += write_bytes;

      // Reset the output buffer for the next input.
      z_stream_->next_out = buffer_.data();
      z_stream_->avail_out = buffer_.size();
    }
  }
  return kNoError;
}

int32_t ZipWriter::FlushCompressedBytes(FileEntry* file) {
  CHECK(state_ == State::kWritingEntry);
  CHECK(z_stream_);
  CHECK(z_stream_->next_out != nullptr);
  CHECK(z_stream_->avail_out != 0);

  // Keep deflating while there isn't enough space in the buffer to
  // to complete the compress.
  int zerr;
  while ((zerr = deflate(z_stream_.get(), Z_FINISH)) == Z_OK) {
    CHECK(z_stream_->avail_out == 0);
    size_t write_bytes = z_stream_->next_out - buffer_.data();
    if (fwrite(buffer_.data(), 1, write_bytes, file_) != write_bytes) {
      return HandleError(kIoError);
    }
    file->compressed_size += write_bytes;
    current_offset_ += write_bytes;

    z_stream_->next_out = buffer_.data();
    z_stream_->avail_out = buffer_.size();
  }
  if (zerr != Z_STREAM_END) {
    return HandleError(kZlibError);
  }

  size_t write_bytes = z_stream_->next_out - buffer_.data();
  if (write_bytes != 0) {
    if (fwrite(buffer_.data(), 1, write_bytes, file_) != write_bytes) {
      return HandleError(kIoError);
    }
    file->compressed_size += write_bytes;
    current_offset_ += write_bytes;
  }
  z_stream_.reset();
  return kNoError;
}

int32_t ZipWriter::FinishEntry() {
  if (state_ != State::kWritingEntry) {
    return kInvalidState;
  }

  if (current_file_entry_.compression_method & kCompressDeflated) {
    int32_t result = FlushCompressedBytes(&current_file_entry_);
    if (result != kNoError) {
      return result;
    }
  }

  if ((current_file_entry_.compression_method & kCompressDeflated) || !seekable_) {
    // Some versions of ZIP don't allow STORED data to have a trailing DataDescriptor.
    // If this file is not seekable, or if the data is compressed, write a DataDescriptor.
    const uint32_t sig = DataDescriptor::kOptSignature;
    if (fwrite(&sig, sizeof(sig), 1, file_) != 1) {
      return HandleError(kIoError);
    }

    DataDescriptor dd = {};
    dd.crc32 = current_file_entry_.crc32;
    dd.compressed_size = current_file_entry_.compressed_size;
    dd.uncompressed_size = current_file_entry_.uncompressed_size;
    if (fwrite(&dd, sizeof(dd), 1, file_) != 1) {
      return HandleError(kIoError);
    }
    current_offset_ += sizeof(DataDescriptor::kOptSignature) + sizeof(dd);
  } else {
    // Seek back to the header and rewrite to include the size.
    if (fseeko(file_, current_file_entry_.local_file_header_offset, SEEK_SET) != 0) {
      return HandleError(kIoError);
    }

    LocalFileHeader header = {};
    CopyFromFileEntry(current_file_entry_, false /*use_data_descriptor*/, &header);

    if (fwrite(&header, sizeof(header), 1, file_) != 1) {
      return HandleError(kIoError);
    }

    if (fseeko(file_, current_offset_, SEEK_SET) != 0) {
      return HandleError(kIoError);
    }
  }

  files_.emplace_back(std::move(current_file_entry_));
  state_ = State::kWritingZip;
  return kNoError;
}

int32_t ZipWriter::Finish() {
  if (state_ != State::kWritingZip) {
    return kInvalidState;
  }

  off_t startOfCdr = current_offset_;
  for (FileEntry& file : files_) {
    CentralDirectoryRecord cdr = {};
    cdr.record_signature = CentralDirectoryRecord::kSignature;
    if ((file.compression_method & kCompressDeflated) || !seekable_) {
      cdr.gpb_flags |= kGPBDDFlagMask;
    }
    cdr.compression_method = file.compression_method;
    cdr.last_mod_time = file.last_mod_time;
    cdr.last_mod_date = file.last_mod_date;
    cdr.crc32 = file.crc32;
    cdr.compressed_size = file.compressed_size;
    cdr.uncompressed_size = file.uncompressed_size;
    cdr.file_name_length = file.path.size();
    cdr.local_file_header_offset = static_cast<uint32_t>(file.local_file_header_offset);
    if (fwrite(&cdr, sizeof(cdr), 1, file_) != 1) {
      return HandleError(kIoError);
    }

    if (fwrite(file.path.data(), 1, file.path.size(), file_) != file.path.size()) {
      return HandleError(kIoError);
    }

    current_offset_ += sizeof(cdr) + file.path.size();
  }

  EocdRecord er = {};
  er.eocd_signature = EocdRecord::kSignature;
  er.disk_num = 0;
  er.cd_start_disk = 0;
  er.num_records_on_disk = files_.size();
  er.num_records = files_.size();
  er.cd_size = current_offset_ - startOfCdr;
  er.cd_start_offset = startOfCdr;

  if (fwrite(&er, sizeof(er), 1, file_) != 1) {
    return HandleError(kIoError);
  }

  current_offset_ += sizeof(er);

  // Since we can BackUp() and potentially finish writing at an offset less than one we had
  // already written at, we must truncate the file.

  if (ftruncate(fileno(file_), current_offset_) != 0) {
    return HandleError(kIoError);
  }

  if (fflush(file_) != 0) {
    return HandleError(kIoError);
  }

  state_ = State::kDone;
  return kNoError;
}