1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
|
# The entries in this file map a sparse set of log tag numbers to tag names.
# This is installed on the device, in /system/etc, and parsed by logcat.
#
# Tag numbers are decimal integers, from 0 to 2^31. (Let's leave the
# negative values alone for now.)
#
# Tag names are one or more ASCII letters and numbers or underscores, i.e.
# "[A-Z][a-z][0-9]_". Do not include spaces or punctuation (the former
# impacts log readability, the latter makes regex searches more annoying).
#
# Tag numbers and names are separated by whitespace. Blank lines and lines
# starting with '#' are ignored.
#
# Optionally, after the tag names can be put a description for the value(s)
# of the tag. Description are in the format
# (<name>|data type[|data unit])
# Multiple values are separated by commas.
#
# The data type is a number from the following values:
# 1: int
# 2: long
# 3: string
# 4: list
#
# The data unit is a number taken from the following list:
# 1: Number of objects
# 2: Number of bytes
# 3: Number of milliseconds
# 4: Number of allocations
# 5: Id
# 6: Percent
# Default value for data of type int/long is 2 (bytes).
#
# TODO: generate ".java" and ".h" files with integer constants from this file.
# These are used for testing, do not modify without updating
# tests/framework-tests/src/android/util/EventLogFunctionalTest.java.
42 answer (to life the universe etc|3)
314 pi
2718 e
2719 configuration_changed (config mask|1|5)
# "account" is the java hash of the account name
2720 sync (id|3),(event|1|5),(source|1|5),(account|1|5)
2721 cpu (total|1|6),(user|1|6),(system|1|6),(iowait|1|6),(irq|1|6),(softirq|1|6)
2722 battery_level (level|1|6),(voltage|1|1),(temperature|1|1)
2723 battery_status (status|1|5),(health|1|5),(present|1|5),(plugged|1|5),(technology|3)
# This is logged when the device is being forced to sleep (typically by
# the user pressing the power button).
2724 power_sleep_requested (wakeLocksCleared|1|1)
# This is logged when the screen on broadcast has completed
2725 power_screen_broadcast_send (wakelockCount|1|1)
# This is logged when the screen broadcast has completed
2726 power_screen_broadcast_done (on|1|5),(broadcastDuration|2|3),(wakelockCount|1|1)
# This is logged when the screen on broadcast has completed
2727 power_screen_broadcast_stop (which|1|5),(wakelockCount|1|1)
# This is logged when the screen is turned on or off.
2728 power_screen_state (offOrOn|1|5),(becauseOfUser|1|5),(totalTouchDownTime|2|3),(touchCycles|1|1)
# This is logged when the partial wake lock (keeping the device awake
# regardless of whether the screen is off) is acquired or released.
2729 power_partial_wake_state (releasedorAcquired|1|5),(tag|3)
# This is logged when battery goes from discharging to charging.
# It lets us count the total amount of time between charges and the discharge level
2730 battery_discharge (duration|2|3),(minLevel|1|6),(maxLevel|1|6)
#
# Leave IDs through 2739 for more power logs
#
# This event is logged when the location service uploads location data.
2740 location_controller
# This event is logged when someone is deciding to force a garbage collection
2741 force_gc (reason|3)
# This event is logged on each tickle
2742 tickle (authority|3)
# What happens in a sync operation (bytes sent and received, and
# operation details)
2743 sync_details (authority|3),(send|1|2),(recv|1|2),(details|3)
# The disk space free on the /data partition, in bytes
2744 free_storage_changed (data|2|2)
# Device low memory notification and disk space free on the /data partition, in bytes at that time
2745 low_storage (data|2|2)
# disk space free on the /data, /system, and /cache partitions in bytes
2746 free_storage_left (data|2|2),(system|2|2),(cache|2|2)
# contacts aggregation: time and number of contacts.
# count is negative for query phase, positive for merge phase
2747 contacts_aggregation (aggregation time|2|3), (count|1|1)
# when a NotificationManager.notify is called
2750 notification_enqueue (pkg|3),(id|1|5),(notification|3)
# when someone tries to cancel a notification, the notification manager sometimes
# calls this with flags too
2751 notification_cancel (pkg|3),(id|1|5),(required_flags|1)
# when someone tries to cancel all of the notifications for a particular package
2752 notification_cancel_all (pkg|3),(required_flags|1)
# This event is logged when GTalkService encounters important events
2800 gtalkservice (eventType|1)
# This event is logged for GTalk connection state changes. The status field is an int, but
# it really contains 4 separate values, each taking up a byte
# (eventType << 24) + (connection state << 16) + (connection error << 8) + network state
2801 gtalk_connection (status|1)
2802 watchdog (Service|3)
2803 watchdog_proc_pss (Process|3),(Pid|1|5),(Pss|1|2)
2804 watchdog_soft_reset (Process|3),(Pid|1|5),(MaxPss|1|2),(Pss|1|2),(Skip|3)
2805 watchdog_hard_reset (Process|3),(Pid|1|5),(MaxPss|1|2),(Pss|1|2)
2806 watchdog_pss_stats (EmptyPss|1|2),(EmptyCount|1|1),(BackgroundPss|1|2),(BackgroundCount|1|1),(ServicePss|1|2),(ServiceCount|1|1),(VisiblePss|1|2),(VisibleCount|1|1),(ForegroundPss|1|2),(ForegroundCount|1|1),(NoPssCount|1|1)
2807 watchdog_proc_stats (DeathsInOne|1|1),(DeathsInTwo|1|1),(DeathsInThree|1|1),(DeathsInFour|1|1),(DeathsInFive|1|1)
2808 watchdog_scheduled_reboot (Now|2|1),(Interval|1|3),(StartTime|1|3),(Window|1|3),(Skip|3)
2809 watchdog_meminfo (MemFree|1|2),(Buffers|1|2),(Cached|1|2),(Active|1|2),(Inactive|1|2),(AnonPages|1|2),(Mapped|1|2),(Slab|1|2),(SReclaimable|1|2),(SUnreclaim|1|2),(PageTables|1|2)
2810 watchdog_vmstat (runtime|2|3),(pgfree|1|1),(pgactivate|1|1),(pgdeactivate|1|1),(pgfault|1|1),(pgmajfault|1|1)
2811 watchdog_requested_reboot (NoWait|1|1),(ScheduleInterval|1|3),(RecheckInterval|1|3),(StartTime|1|3),(Window|1|3),(MinScreenOff|1|3),(MinNextAlarm|1|3)
2820 backup_data_changed (Package|3)
2821 backup_start (Transport|3)
2822 backup_transport_failure (Package|3)
2823 backup_agent_failure (Package|3),(Message|3)
2824 backup_package (Package|3),(Size|1|2)
2825 backup_success (Packages|1|1),(Time|1|3)
2826 backup_reset (Transport|3)
2827 backup_initialize
2830 restore_start (Transport|3),(Source|2|5)
2831 restore_transport_failure
2832 restore_agent_failure (Package|3),(Message|3)
2833 restore_package (Package|3),(Size|1|2)
2834 restore_success (Packages|1|1),(Time|1|3)
# Device boot timings. We include monotonic clock values because the
# intrinsic event log times are wall-clock.
#
# Runtime starts:
3000 boot_progress_start (time|2|3)
# SystemServer.run() starts:
3010 boot_progress_system_run (time|2|3)
# ZygoteInit class preloading starts:
3020 boot_progress_preload_start (time|2|3)
# ZygoteInit class preloading ends:
3030 boot_progress_preload_end (time|2|3)
# ActivityManagerService.systemReady() starts:
3040 boot_progress_ams_ready (time|2|3)
# ActivityManagerService calls enableScreenAfterBoot():
3050 boot_progress_enable_screen (time|2|3)
# Package Manager starts:
3060 boot_progress_pms_start (time|2|3)
# Package Manager .apk scan starts:
3070 boot_progress_pms_system_scan_start (time|2|3)
# Package Manager .apk scan starts:
3080 boot_progress_pms_data_scan_start (time|2|3)
# Package Manager .apk scan ends:
3090 boot_progress_pms_scan_end (time|2|3)
# Package Manager ready:
3100 boot_progress_pms_ready (time|2|3)
# + check activity_launch_time for Home app
# This event is logged when GTalk connection is closed.
# The status field is an int, but contains 2 different values, it's represented as
#
# (networkType << 8) + connection error
#
# the possible error values are
#
# no_error=0, no_network=1, connection_failed=2, unknown_host=3, auth_failed=4,
# auth_expired=5, heart_beat_timeout=6, server_error=7, server_reject_rate_limiting=8, unknown=10
#
# duration is the connection duration.
4000 gtalk_conn_close (status|1),(duration|1)
# This event is logged for GTalk heartbeat resets
# interval_and_nt contains both the heartbeat interval and the network type, It's represented as
# (networkType << 16) + interval
# interval is in seconds; network type can be 0 (mobile) or 1 (wifi); ip is the host ip addr.
4001 gtalk_heartbeat_reset (interval_and_nt|1),(ip|3)
# dvm_gc_info: LIST (LONG, LONG, LONG)
#
# First LONG:
#
# [63] 1
# [62-24] ASCII process identifier
# [23-12] GC time in ms
# [11- 0] Bytes freed
#
# Second LONG (aggregated heap info):
#
# [63-62] 10
# [61-60] Reserved; must be zero
# [59-48] Objects freed
# [47-36] Actual size (current footprint)
# [35-24] Allowed size (current hard max)
# [23-12] Objects allocated
# [11- 0] Bytes allocated
#
# Third LONG (zygote heap info):
#
# [63-62] 11
# [61-60] Reserved; must be zero
# [59-48] Soft limit
# [47-36] Actual size (current footprint)
# [35-24] Allowed size (current hard max)
# [23-12] Objects allocated
# [11- 0] Bytes allocated
#
# Fourth LONG:
#
# [63-48] Reserved; must be zero
# [47-36] dlmallocFootprint
# [35-24] mallinfo: total allocated space
# [23-12] External byte limit
# [11- 0] External bytes allocated
#
# See HeapDebug.c
#
20001 dvm_gc_info (custom|2),(custom|2),(custom|2),(custom|2)
20002 dvm_gc_madvise_info (total|1|2),(zygote|1|2)
# Do not change these names without updating the checkin_events setting in
# google3/googledata/wireless/android/provisioning/gservices.config !!
#
# An activity is being finished:
30001 am_finish_activity (Token|1|5),(Task ID|1|5),(Component Name|3),(Reason|3)
# A task is being brought to the front of the screen:
30002 am_task_to_front (Task|1|5)
# An existing activity is being given a new intent:
30003 am_new_intent (Token|1|5),(Task ID|1|5),(Component Name|3),(Action|3),(MIME Type|3),(URI|3),(Flags|1|5)
# A new task is being created:
30004 am_create_task (Task ID|1|5)
# A new activity is being created in an existing task:
30005 am_create_activity (Token|1|5),(Task ID|1|5),(Component Name|3),(Action|3),(MIME Type|3),(URI|3),(Flags|1|5)
# An activity has been resumed into the foreground but was not already running:
30006 am_restart_activity (Token|1|5),(Task ID|1|5),(Component Name|3)
# An activity has been resumed and is now in the foreground:
30007 am_resume_activity (Token|1|5),(Task ID|1|5),(Component Name|3)
# Application Not Responding
30008 anr (pid|1|5),(Package Name|3),(reason|3)
# Activity launch time
30009 activity_launch_time (Token|1|5),(Component Name|3),(time|2|3)
# Application process bound to work
30010 am_proc_bound (PID|1|5),(Process Name|3)
# Application process died
30011 am_proc_died (PID|1|5),(Process Name|3)
# The Activity Manager failed to pause the given activity.
30012 am_failed_to_pause (Token|1|5),(Wanting to pause|3),(Currently pausing|3)
# Attempting to pause the current activity
30013 am_pause_activity (Token|1|5),(Component Name|3)
# Application process has been started
30014 am_proc_start (PID|1|5),(UID|1|5),(Process Name|3),(Type|3),(Component|3)
# An application process has been marked as bad
30015 am_proc_bad (UID|1|5),(Process Name|3)
# An application process that was bad is now marked as good
30016 am_proc_good (UID|1|5),(Process Name|3)
# Reporting to applications that memory is low
30017 am_low_memory (Num Processes|1|1)
# An activity is being destroyed:
30018 am_destroy_activity (Token|1|5),(Task ID|1|5),(Component Name|3)
# An activity has been relaunched, resumed, and is now in the foreground:
30019 am_relaunch_resume_activity (Token|1|5),(Task ID|1|5),(Component Name|3)
# An activity has been relaunched:
30020 am_relaunch_activity (Token|1|5),(Task ID|1|5),(Component Name|3)
# The activity's onPause has been called.
30021 am_on_paused_called (Component Name|3)
# The activity's onResume has been called.
30022 am_on_resume_called (Component Name|3)
# Kill a process to reclaim memory.
30023 am_kill_for_memory (PID|1|5),(Process Name|3),(OomAdj|1|5)
# Discard an undelivered serialized broadcast (timeout/ANR/crash)
30024 am_broadcast_discard_filter (Broadcast|1|5),(Action|3),(Receiver Number|1|1),(BroadcastFilter|1|5)
30025 am_broadcast_discard_app (Broadcast|1|5),(Action|3),(Receiver Number|1|1),(App|3)
# A service is being created
30030 am_create_service (Service Record|1|5),(Name|3),(Intent|3),(PID|1|5)
# A service is being destroyed
30031 am_destroy_service (Service Record|1|5),(Name|3),(PID|1|5)
# A process has crashed too many times, it is being cleared
30032 am_process_crashed_too_much (Name|3),(PID|1|5)
# An unknown process is trying to attach to the activity manager
30033 am_drop_process (PID|1|5)
# A service has crashed too many times, it is being stopped
30034 am_service_crashed_too_much (Crash Count|1|1),(Component Name|3),(PID|1|5)
# A service is going to be restarted after its process went away
30035 am_schedule_service_restart (Component Name|3),(Time|2|3)
# A client was waiting for a content provider, but its process was lost
30036 am_provider_lost_process (Package Name|3),(UID|1|5),(Name|3)
# The activity manager gave up on a new process taking too long to start
30037 am_process_start_timeout (PID|1|5),(UID|1|5),(Process Name|3)
# Out of memory for surfaces.
31000 wm_no_surface_memory (Window|3),(PID|1|5),(Operation|3)
# Re-connecting to input method service because we haven't received its interface
32000 imf_force_reconnect_ime (IME|4),(Time Since Connect|2|3),(Showing|1|1)
75000 sqlite_mem_alarm_current (current|1|2)
75001 sqlite_mem_alarm_max (max|1|2)
75002 sqlite_mem_alarm_alloc_attempt (attempts|1|4)
75003 sqlite_mem_released (Memory released|1|2)
75004 sqlite_db_corrupt (Database file corrupt|3)
40000 checkin (Check in time|2|3)
50000 menu_item_selected (Menu type where 0 is options and 1 is context|1|5),(Menu item title|3)
50001 menu_opened (Menu type where 0 is options and 1 is context|1|5)
# Connectivity state changed:
# [31-13] Reserved for future use
# [12- 9] Network subtype (for mobile network, as defined by TelephonyManager)
# [ 8- 3] Detailed state ordinal (as defined by NetworkInfo.DetailedState)
# [ 2- 0] Network type (as defined by ConnectivityManager)
50020 connectivity_state_changed (custom|1|5)
# Wi-Fi network state changed:
# [31- 6] Reserved for future use
# [ 5- 0] Detailed state ordinal (as defined by NetworkInfo.DetailedState)
50021 wifi_network_state_changed (network_state|1|5)
# Wi-Fi supplicant state changed:
# [31- 6] Reserved for future use
# [ 5- 0] Supplicant state ordinal (as defined by SupplicantState)
50022 wifi_supplicant_state_changed (supplicant_state|1|5)
# Wi-Fi driver state changed:
# [31- 1] Reserved for future use
# [ 0- 0] Driver start (1) or stopped (0)
50023 wifi_driver_state_changed (driver_state|1|5)
# Wi-Fi interface configuration state changed:
# [31- 1] Reserved for future use
# [ 0- 0] Interface configuration succeeded (1) or failed (0)
50024 wifi_interface_configuration_state_changed (IP_configuration|1|5)
# Wi-Fi supplicant connection state changed:
# [31- 2] Reserved for future use
# [ 1- 0] Connected to supplicant (1) or disconnected from supplicant (0),
# or supplicant died (2)
50025 wifi_supplicant_connection_state_changed (connected|1|5)
# PDP Context has a bad DNS address
50100 pdp_bad_dns_address (dns_address|3)
# For data connection on PDP context, reached the data-out-without-data-in
# packet count that triggers a countdown to radio restart
50101 pdp_radio_reset_countdown_triggered (out_packet_count|1|1)
# Radio restart - timed out with no incoming packets.
50102 pdp_radio_reset (out_packet_count|1|1)
# PDP context reset - timed out with no incoming packets.
50103 pdp_context_reset (out_packet_count|1|1)
# Reregister to data network - timed out with no incoming packets.
50104 pdp_reregister_network (out_packet_count|1|1)
# PDP Setup failures
50105 pdp_setup_fail (cause|1|5), (cid|1|5), (network_type|1|5)
# Call drops
50106 call_drop (cause|1|5), (cid|1|5), (network_type|1|5)
# Data network registration failed after successful voice registration
50107 data_network_registration_fail (op_numeric|1|5), (cid|1|5)
# Suspicious status of data connection while radio poweroff
50108 data_network_status_on_radio_off (dc_state|3), (enable|1|5)
# PDP drop caused by network
50109 pdp_network_drop (cid|1|5), (network_type|1|5)
# CDMA data network setup failure
50110 cdma_data_setup_failed (cause|1|5), (cid|1|5), (network_type|1|5)
# CDMA data network drop
50111 cdma_data_drop (cid|1|5), (network_type|1|5)
# Do not change these names without updating tag in:
#//device/dalvik/libcore/luni/src/main/native/org_apache_harmony_luni_platform_OSNetworkSystem.c
51000 socket_stats (send|1|2),(recv|1|2),(ip|1|5),(port|1|5),(close|1|5)
# db stats. 0 is query, 1 is write (may become more fine grained in the
# future)
52000 db_operation (name|3),(op_type|1|5),(time|2|3)
# http request/response stats
52001 http_stats (useragent|3),(response|2|3),(processing|2|3),(tx|1|2),(rx|1|2)
60000 viewroot_draw (Draw time|1|3)
60001 viewroot_layout (Layout time|1|3)
60002 view_build_drawing_cache (View created drawing cache|1|5)
60003 view_use_drawing_cache (View drawn using bitmap cache|1|5)
# 0 for screen off, 1 for screen on, 2 for key-guard done
70000 screen_toggled (screen_state|1|5)
# browser stats for diary study
70101 browser_zoom_level_change (start level|1|5),(end level|1|5),(time|2|3)
70102 browser_double_tap_duration (duration|1|3),(time|2|3)
# aggregation service
70200 aggregation (aggregation time|2|3)
70201 aggregation_test (field1|1|2),(field2|1|2),(field3|1|2),(field4|1|2),(field5|1|2)
# NOTE - the range 1000000-2000000 is reserved for partners and others who
# want to define their own log tags without conflicting with the core platform.
|