summaryrefslogtreecommitdiffstats
blob: 9d9a857422ad45734c25d57956f153a3bdc64e6b (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
/*
 * Copyright 2012, Samsung Telecommunications of America
 * Copyright (C) 2014 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *     http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 *
 * Written by William Roberts <w.roberts@sta.samsung.com>
 *
 */

#include <errno.h>
#include <string.h>
#include <unistd.h>

#include "libaudit.h"

/**
 * Waits for an ack from the kernel
 * @param fd
 *  The netlink socket fd
 * @return
 *  This function returns 0 on success, else -errno.
 */
static int get_ack(int fd) {
    int rc;
    struct audit_message rep;

    /* Sanity check, this is an internal interface this shouldn't happen */
    if (fd < 0) {
        return -EINVAL;
    }

    rc = audit_get_reply(fd, &rep, GET_REPLY_BLOCKING, MSG_PEEK);
    if (rc < 0) {
        return rc;
    }

    if (rep.nlh.nlmsg_type == NLMSG_ERROR) {
        audit_get_reply(fd, &rep, GET_REPLY_BLOCKING, 0);
        rc = ((struct nlmsgerr*)rep.data)->error;
        if (rc) {
            return -rc;
        }
    }

    return 0;
}

/**
 *
 * @param fd
 *  The netlink socket fd
 * @param type
 *  The type of netlink message
 * @param data
 *  The data to send
 * @param size
 *  The length of the data in bytes
 * @return
 *  This function returns a positive sequence number on success, else -errno.
 */
static int audit_send(int fd, int type, const void* data, size_t size) {
    int rc;
    static int16_t sequence = 0;
    struct audit_message req;
    struct sockaddr_nl addr;

    memset(&req, 0, sizeof(req));
    memset(&addr, 0, sizeof(addr));

    /* We always send netlink messaged */
    addr.nl_family = AF_NETLINK;

    /* Set up the netlink headers */
    req.nlh.nlmsg_type = type;
    req.nlh.nlmsg_len = NLMSG_SPACE(size);
    req.nlh.nlmsg_flags = NLM_F_REQUEST | NLM_F_ACK;

    /*
     * Check for a valid fd, even though sendto would catch this, its easier
     * to always blindly increment the sequence number
     */
    if (fd < 0) {
        return -EBADF;
    }

    /* Ensure the message is not too big */
    if (NLMSG_SPACE(size) > MAX_AUDIT_MESSAGE_LENGTH) {
        return -EINVAL;
    }

    /* Only memcpy in the data if it was specified */
    if (size && data) {
        memcpy(NLMSG_DATA(&req.nlh), data, size);
    }

    /*
     * Only increment the sequence number on a guarantee
     * you will send it to the kernel.
     *
     * Also, the sequence is defined as a u32 in the kernel
     * struct. Using an int here might not work on 32/64 bit splits. A
     * signed 64 bit value can overflow a u32..but a u32
     * might not fit in the response, so we need to use s32.
     * Which is still kind of hackish since int could be 16 bits
     * in size. The only safe type to use here is a signed 16
     * bit value.
     */
    req.nlh.nlmsg_seq = ++sequence;

    /* While failing and its due to interrupts */

    rc = TEMP_FAILURE_RETRY(sendto(fd, &req, req.nlh.nlmsg_len, 0,
                                   (struct sockaddr*)&addr, sizeof(addr)));

    /* Not all the bytes were sent */
    if (rc < 0) {
        rc = -errno;
        goto out;
    } else if ((uint32_t)rc != req.nlh.nlmsg_len) {
        rc = -EPROTO;
        goto out;
    }

    /* We sent all the bytes, get the ack */
    rc = get_ack(fd);

    /* If the ack failed, return the error, else return the sequence number */
    rc = (rc == 0) ? (int)sequence : rc;

out:
    /* Don't let sequence roll to negative */
    if (sequence < 0) {
        sequence = 0;
    }

    return rc;
}

int audit_setup(int fd, pid_t pid) {
    int rc;
    struct audit_message rep;
    struct audit_status status;

    memset(&status, 0, sizeof(status));

    /*
     * In order to set the auditd PID we send an audit message over the netlink
     * socket with the pid field of the status struct set to our current pid,
     * and the the mask set to AUDIT_STATUS_PID
     */
    status.pid = pid;
    status.mask = AUDIT_STATUS_PID | AUDIT_STATUS_RATE_LIMIT;
    status.rate_limit = AUDIT_RATE_LIMIT; /* audit entries per second */

    /* Let the kernel know this pid will be registering for audit events */
    rc = audit_send(fd, AUDIT_SET, &status, sizeof(status));
    if (rc < 0) {
        return rc;
    }

    /*
     * In a request where we need to wait for a response, wait for the message
     * and discard it. This message confirms and sync's us with the kernel.
     * This daemon is now registered as the audit logger.
     *
     * TODO
     * If the daemon dies and restarts the message didn't come back,
     * so I went to non-blocking and it seemed to fix the bug.
     * Need to investigate further.
     */
    audit_get_reply(fd, &rep, GET_REPLY_NONBLOCKING, 0);

    return 0;
}

int audit_open() {
    return socket(PF_NETLINK, SOCK_RAW | SOCK_CLOEXEC, NETLINK_AUDIT);
}

int audit_get_reply(int fd, struct audit_message* rep, reply_t block, int peek) {
    ssize_t len;
    int flags;
    int rc = 0;

    struct sockaddr_nl nladdr;
    socklen_t nladdrlen = sizeof(nladdr);

    if (fd < 0) {
        return -EBADF;
    }

    /* Set up the flags for recv from */
    flags = (block == GET_REPLY_NONBLOCKING) ? MSG_DONTWAIT : 0;
    flags |= peek;

    /*
     * Get the data from the netlink socket but on error we need to be carefull,
     * the interface shows that EINTR can never be returned, other errors,
     * however, can be returned.
     */
    len = TEMP_FAILURE_RETRY(recvfrom(fd, rep, sizeof(*rep), flags,
                                      (struct sockaddr*)&nladdr, &nladdrlen));

    /*
     * EAGAIN should be re-tried until success or another error manifests.
     */
    if (len < 0) {
        rc = -errno;
        if (block == GET_REPLY_NONBLOCKING && rc == -EAGAIN) {
            /* If request is non blocking and errno is EAGAIN, just return 0 */
            return 0;
        }
        return rc;
    }

    if (nladdrlen != sizeof(nladdr)) {
        return -EPROTO;
    }

    /* Make sure the netlink message was not spoof'd */
    if (nladdr.nl_pid) {
        return -EINVAL;
    }

    /* Check if the reply from the kernel was ok */
    if (!NLMSG_OK(&rep->nlh, (size_t)len)) {
        rc = (len == sizeof(*rep)) ? -EFBIG : -EBADE;
    }

    return rc;
}

void audit_close(int fd) {
    close(fd);
}