summaryrefslogtreecommitdiffstats
blob: 15d830c3967170dbef518b4d5e1a9f68c444c709 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
/*
 * Copyright (C) 2016 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef _STORAGED_H_
#define _STORAGED_H_

#include <semaphore.h>
#include <stdint.h>
#include <time.h>

#include <queue>
#include <string>
#include <unordered_map>
#include <vector>

#include "storaged_uid_monitor.h"

#define FRIEND_TEST(test_case_name, test_name) \
friend class test_case_name##_##test_name##_Test

/* For debug */
#ifdef DEBUG
#define debuginfo(fmt, ...) \
 do {printf("%s():\t" fmt "\t[%s:%d]\n", __FUNCTION__, ##__VA_ARGS__, __FILE__, __LINE__);} \
 while(0)
#else
#define debuginfo(...)
#endif

#define SECTOR_SIZE ( 512 )
#define SEC_TO_MSEC ( 1000 )
#define MSEC_TO_USEC ( 1000 )
#define USEC_TO_NSEC ( 1000 )
#define SEC_TO_USEC ( 1000000 )

// number of attributes diskstats has
#define DISK_STATS_SIZE ( 11 )
// maximum size limit of a stats file
#define DISK_STATS_FILE_MAX_SIZE ( 256 )
#define DISK_STATS_IO_IN_FLIGHT_IDX ( 8 )
struct disk_stats {
    /* It will be extremely unlikely for any of the following entries to overflow.
     * For read_bytes(which will be greater than any of the following entries), it
     * will take 27 years to overflow uint64_t at the reading rate of 20GB/s, which
     * is the peak memory transfer rate for current memory.
     * The diskstats entries (first 11) need to be at top in this structure _after_
     * compiler's optimization.
     */
    uint64_t read_ios;       // number of read I/Os processed
    uint64_t read_merges;    // number of read I/Os merged with in-queue I/Os
    uint64_t read_sectors;   // number of sectors read
    uint64_t read_ticks;     // total wait time for read requests
    uint64_t write_ios;      // number of write I/Os processed
    uint64_t write_merges;   // number of write I/Os merged with in-queue I/Os
    uint64_t write_sectors;  // number of sectors written
    uint64_t write_ticks;    // total wait time for write requests
    uint64_t io_in_flight;   // number of I/Os currently in flight
    uint64_t io_ticks;       // total time this block device has been active
    uint64_t io_in_queue;    // total wait time for all requests

    uint64_t start_time;     // monotonic time accounting starts
    uint64_t end_time;       // monotonic time accounting ends
    uint32_t counter;        // private counter for accumulate calculations
    double   io_avg;         // average io_in_flight for accumulate calculations
};

#define MMC_VER_STR_LEN ( 9 )   // maximum length of the MMC version string, including NULL terminator
// minimum size of a ext_csd file
#define EXT_CSD_FILE_MIN_SIZE ( 1024 )
struct emmc_info {
    int eol;                        // pre-eol (end of life) information
    int lifetime_a;                 // device life time estimation (type A)
    int lifetime_b;                 // device life time estimation (type B)
    char mmc_ver[MMC_VER_STR_LEN];  // device version string
};

struct disk_perf {
    uint32_t read_perf;         // read speed (kbytes/s)
    uint32_t read_ios;          // read I/Os per second
    uint32_t write_perf;        // write speed (kbytes/s)
    uint32_t write_ios;         // write I/Os per second
    uint32_t queue;             // I/Os in queue
};

#define CMD_MAX_LEN ( 64 )
struct task_info {
    uint32_t pid;                   // task id
    uint64_t rchar;                 // characters read
    uint64_t wchar;                 // characters written
    uint64_t syscr;                 // read syscalls
    uint64_t syscw;                 // write syscalls
    uint64_t read_bytes;            // bytes read (from storage layer)
    uint64_t write_bytes;           // bytes written (to storage layer)
    uint64_t cancelled_write_bytes; // cancelled write byte by truncate

    uint64_t starttime;             // start time of task

    char cmd[CMD_MAX_LEN];          // filename of the executable
};

class lock_t {
    sem_t* mSem;
public:
    lock_t(sem_t* sem) {
        mSem = sem;
        sem_wait(mSem);
    }
    ~lock_t() {
        sem_post(mSem);
    }
};

class stream_stats {
private:
    double mSum;
    double mSquareSum;
    uint32_t mCnt;
public:
    stream_stats() : mSum(0), mSquareSum(0), mCnt(0) {};
    ~stream_stats() {};
    double get_mean() {
        return mSum / mCnt;
    }
    double get_std() {
        return sqrt(mSquareSum / mCnt - mSum * mSum / (mCnt * mCnt));
    }
    void add(uint32_t num) {
        mSum += (double)num;
        mSquareSum += (double)num * (double)num;
        mCnt++;
    }
    void evict(uint32_t num) {
        if (mSum < num || mSquareSum < (double)num * (double)num) return;
        mSum -= (double)num;
        mSquareSum -= (double)num * (double)num;
        mCnt--;
    }
};

#define MMC_DISK_STATS_PATH "/sys/block/mmcblk0/stat"
#define SDA_DISK_STATS_PATH "/sys/block/sda/stat"
#define EMMC_ECSD_PATH "/d/mmc0/mmc0:0001/ext_csd"
#define UID_IO_STATS_PATH "/proc/uid_io/stats"

class disk_stats_monitor {
private:
    FRIEND_TEST(storaged_test, disk_stats_monitor);
    const char* DISK_STATS_PATH;
    struct disk_stats mPrevious;
    struct disk_stats mAccumulate;
    bool mStall;
    std::queue<struct disk_perf> mBuffer;
    struct {
        stream_stats read_perf;           // read speed (bytes/s)
        stream_stats read_ios;            // read I/Os per second
        stream_stats write_perf;          // write speed (bytes/s)
        stream_stats write_ios;           // write I/O per second
        stream_stats queue;               // I/Os in queue
    } mStats;
    bool mValid;
    const uint32_t mWindow;
    const double mSigma;
    struct disk_perf mMean;
    struct disk_perf mStd;

    void update_mean();
    void update_std();
    void add(struct disk_perf* perf);
    void evict(struct disk_perf* perf);
    bool detect(struct disk_perf* perf);

    void update(struct disk_stats* stats);

public:
    disk_stats_monitor(uint32_t window_size = 5, double sigma = 1.0) :
            mStall(false),
            mValid(false),
            mWindow(window_size),
            mSigma(sigma) {
        memset(&mPrevious, 0, sizeof(mPrevious));
        memset(&mMean, 0, sizeof(mMean));
        memset(&mStd, 0, sizeof(mStd));

        if (access(MMC_DISK_STATS_PATH, R_OK) >= 0) {
            DISK_STATS_PATH = MMC_DISK_STATS_PATH;
        } else {
            DISK_STATS_PATH = SDA_DISK_STATS_PATH;
        }
    }
    void update(void);
};

class disk_stats_publisher {
private:
    FRIEND_TEST(storaged_test, disk_stats_publisher);
    const char* DISK_STATS_PATH;
    struct disk_stats mAccumulate;
    struct disk_stats mPrevious;
public:
    disk_stats_publisher(void) {
        memset(&mAccumulate, 0, sizeof(struct disk_stats));
        memset(&mPrevious, 0, sizeof(struct disk_stats));

        if (access(MMC_DISK_STATS_PATH, R_OK) >= 0) {
            DISK_STATS_PATH = MMC_DISK_STATS_PATH;
        } else {
            DISK_STATS_PATH = SDA_DISK_STATS_PATH;
        }
    }

    ~disk_stats_publisher(void) {}
    void publish(void);
    void update(void);
};

class emmc_info_t {
private:
    struct emmc_info mInfo;
    bool mValid;
    int mFdEmmc;
public:
    emmc_info_t(void) :
            mValid(false),
            mFdEmmc(-1) {
        memset(&mInfo, 0, sizeof(struct emmc_info));
    }
    ~emmc_info_t(void) {}

    void publish(void);
    void update(void);
    void set_emmc_fd(int fd) {
        mFdEmmc = fd;
    }
};

// Periodic chores intervals in seconds
#define DEFAULT_PERIODIC_CHORES_INTERVAL_UNIT ( 60 )
#define DEFAULT_PERIODIC_CHORES_INTERVAL_DISK_STATS_PUBLISH ( 3600 )
#define DEFAULT_PERIODIC_CHORES_INTERVAL_EMMC_INFO_PUBLISH ( 86400 )
#define DEFAULT_PERIODIC_CHORES_INTERVAL_UID_IO ( 3600 )

// UID IO threshold in bytes
#define DEFAULT_PERIODIC_CHORES_UID_IO_THRESHOLD ( 1024 * 1024 * 1024ULL )

struct storaged_config {
    int periodic_chores_interval_unit;
    int periodic_chores_interval_disk_stats_publish;
    int periodic_chores_interval_emmc_info_publish;
    int periodic_chores_interval_uid_io;
    bool proc_uid_io_available;      // whether uid_io is accessible
    bool emmc_available;        // whether eMMC est_csd file is readable
    bool diskstats_available;   // whether diskstats is accessible
    int event_time_check_usec;  // check how much cputime spent in event loop
};

class storaged_t {
private:
    time_t mTimer;
    storaged_config mConfig;
    disk_stats_publisher mDiskStats;
    disk_stats_monitor mDsm;
    emmc_info_t mEmmcInfo;
    uid_monitor mUidm;
    time_t mStarttime;
public:
    storaged_t(void);
    ~storaged_t() {}
    void event(void);
    void event_checked(void);
    void pause(void) {
        sleep(mConfig.periodic_chores_interval_unit);
    }

    void set_privileged_fds(int fd_emmc) {
        mEmmcInfo.set_emmc_fd(fd_emmc);
    }

    time_t get_starttime(void) {
        return mStarttime;
    }

    std::unordered_map<uint32_t, struct uid_info> get_uids(void) {
        return mUidm.get_uids();
    }
};

// Eventlog tag
// The content must match the definition in EventLogTags.logtags
#define EVENTLOGTAG_DISKSTATS ( 2732 )
#define EVENTLOGTAG_EMMCINFO ( 2733 )
#define EVENTLOGTAG_UID_IO_ALERT ( 2734 )

#endif /* _STORAGED_H_ */