/*
* Copyright (C) 2017 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#include <getopt.h>
#include <iostream>
#include <android-base/strings.h>
#include <vintf/AssembleVintf.h>
#include "utils.h"
void help() {
std::cerr << "assemble_vintf: Checks if a given manifest / matrix file is valid and \n"
" fill in build-time flags into the given file.\n"
"assemble_vintf -h\n"
" Display this help text.\n"
"assemble_vintf -i <input file>[:<input file>[...]] [-o <output file>] [-m]\n"
" [-c [<check file>]]\n"
" Fill in build-time flags into the given file.\n"
" -i <input file>[:<input file>[...]]\n"
" A list of input files. Format is automatically detected for the\n"
" first file, and the remaining files must have the same format.\n"
" Files other than the first file should only have <hal> defined;\n"
" other entries are ignored. Argument may also be specified\n"
" multiple times.\n"
" -o <output file>\n"
" Optional output file. If not specified, write to stdout.\n"
" -m\n"
" a compatible compatibility matrix is\n"
" generated instead; for example, given a device manifest,\n"
" a framework compatibility matrix is generated. This flag\n"
" is ignored when input is a compatibility matrix.\n"
" -c [<check file>]\n"
" The path of the \"check file\"; for example, this is the path\n"
" of the device manifest for framework compatibility matrix.\n"
" After writing the output file, the program checks against\n"
" the \"check file\", depending on environment variables.\n"
" - PRODUCT_ENFORCE_VINTF_MANIFEST=true: check compatibility\n"
" - VINTF_ENFORCE_NO_UNUSED_HALS =true: check unused HALs\n"
" If any check fails, an error message is written to stderr.\n"
" Return 1.\n"
" --kernel=<version>:<android-base.config>[:<android-base-arch.config>[...]]\n"
" Add a kernel entry to framework compatibility matrix.\n"
" Ignored for other input format.\n"
" <version> has format: 3.18.0\n"
" <android-base.config> is the location of android-base.config\n"
" <android-base-arch.config> is the location of an optional\n"
" arch-specific config fragment, more than one may be specified\n"
" -l, --hals-only\n"
" Output has only <hal> entries. Cannot be used with -n.\n"
" -n, --no-hals\n"
" Output has no <hal> entries (but all other entries).\n"
" Cannot be used with -l.\n"
" --no-kernel-requirements\n"
" Output has no <config> entries in <kernel>, and kernel minor\n"
" version is set to zero. (For example, 3.18.0).\n";
}
int main(int argc, char** argv) {
using namespace ::android::vintf;
const struct option longopts[] = {{"kernel", required_argument, NULL, 'k'},
{"hals-only", no_argument, NULL, 'l'},
{"no-hals", no_argument, NULL, 'n'},
{"no-kernel-requirements", no_argument, NULL, 'K'},
{0, 0, 0, 0}};
std::string outFilePath;
auto assembleVintf = AssembleVintf::newInstance();
int res;
int optind;
while ((res = getopt_long(argc, argv, "hi:o:mc:nl", longopts, &optind)) >= 0) {
switch (res) {
case 'i': {
for (const auto& inFilePath : ::android::base::Split(optarg, ":")) {
if (!assembleVintf->openInFile(inFilePath.c_str())) {
std::cerr << "Failed to open " << inFilePath << std::endl;
return 1;
}
}
} break;
case 'o': {
outFilePath = optarg;
if (!assembleVintf->openOutFile(optarg)) {
std::cerr << "Failed to open " << optarg << std::endl;
return 1;
}
} break;
case 'm': {
assembleVintf->setOutputMatrix();
} break;
case 'c': {
if (!assembleVintf->openCheckFile(optarg)) {
std::cerr << "Failed to open " << optarg << std::endl;
return 1;
}
} break;
case 'k': {
if (!assembleVintf->addKernel(optarg)) {
std::cerr << "ERROR: Unrecognized --kernel argument." << std::endl;
return 1;
}
} break;
case 'l': {
if (!assembleVintf->setHalsOnly()) {
return 1;
}
} break;
case 'n': {
if (!assembleVintf->setNoHals()) {
return 1;
}
} break;
case 'K': {
if (!assembleVintf->setNoKernelRequirements()) {
return 1;
}
} break;
case 'h':
default: {
help();
return 1;
} break;
}
}
bool success = assembleVintf->assemble();
return success ? 0 : 1;
}