summaryrefslogblamecommitdiffstats
blob: 8ccda3eaf4ac133c94c9c4bebd7ceb2e1165ed7a (plain) (tree)


















                                                                           
                 
                
 
                         
                             

                              




                   








                                                        
                     

                                                                                                  
                     
                                                            




                       
                                                     
                   
                    
                                                               
         




                         





                                                                                    
 












                                                          



                                                           








                                                                                      





                                                                                   







                                                                                           
 






                       
/*
 * Copyright (C) 2017 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef ANDROID_VINTF_UTILS_H
#define ANDROID_VINTF_UTILS_H

#include <memory>
#include <mutex>

#include <utils/Errors.h>
#include <vintf/FileSystem.h>
#include <vintf/RuntimeInfo.h>
#include <vintf/parse_xml.h>

namespace android {
namespace vintf {
namespace details {

class PartitionMounter {
   public:
    virtual ~PartitionMounter() {}
    virtual status_t mountSystem() const { return OK; }
    virtual status_t mountVendor() const { return OK; }
    virtual status_t umountSystem() const { return OK; }
    virtual status_t umountVendor() const { return OK; }
};

template <typename T>
status_t fetchAllInformation(const FileSystem* fileSystem, const std::string& path,
                             const XmlConverter<T>& converter, T* outObject, std::string* error) {
    std::string info;
    status_t result = fileSystem->fetch(path, &info, error);

    if (result != OK) {
        return result;
    }

    bool success = converter(outObject, info, error);
    if (!success) {
        if (error) {
            *error = "Illformed file: " + path + ": " + *error;
        }
        return BAD_VALUE;
    }
    return OK;
}

template <typename T>
class ObjectFactory {
   public:
    virtual ~ObjectFactory() = default;
    virtual std::shared_ptr<T> make_shared() const { return std::make_shared<T>(); }
};

// TODO(b/70628538): Do not infer from Shipping API level.
inline Level convertFromApiLevel(size_t apiLevel) {
    if (apiLevel < 26) {
        return Level::LEGACY;
    } else if (apiLevel == 26) {
        return Level::O;
    } else if (apiLevel == 27) {
        return Level::O_MR1;
    } else {
        return Level::UNSPECIFIED;
    }
}

class PropertyFetcher {
   public:
    virtual ~PropertyFetcher() = default;
    virtual std::string getProperty(const std::string& key,
                                    const std::string& defaultValue = "") const = 0;
    virtual uint64_t getUintProperty(const std::string& key, uint64_t defaultValue,
                                     uint64_t max = UINT64_MAX) const = 0;
    virtual bool getBoolProperty(const std::string& key, bool defaultValue) const = 0;
};

class PropertyFetcherImpl : public PropertyFetcher {
   public:
    virtual std::string getProperty(const std::string& key,
                                    const std::string& defaultValue = "") const;
    virtual uint64_t getUintProperty(const std::string& key, uint64_t defaultValue,
                                     uint64_t max = UINT64_MAX) const;
    virtual bool getBoolProperty(const std::string& key, bool defaultValue) const;
};

class PropertyFetcherNoOp : public PropertyFetcher {
   public:
    virtual std::string getProperty(const std::string& key,
                                    const std::string& defaultValue = "") const override;
    virtual uint64_t getUintProperty(const std::string& key, uint64_t defaultValue,
                                     uint64_t max = UINT64_MAX) const override;
    virtual bool getBoolProperty(const std::string& key, bool defaultValue) const override;
};

}  // namespace details
}  // namespace vintf
}  // namespace android



#endif