diff options
author | Steven Moreland | 2018-10-29 15:31:15 -0500 |
---|---|---|
committer | Steven Moreland | 2018-10-29 15:33:11 -0500 |
commit | 6e392846877911bc4036c85dbdf27211ddd15786 (patch) | |
tree | 98d1fca0cc32e69569c4ca34aa9fe66b6f309fd2 | |
parent | fab70a459138b23488f089fe76a0737f86388162 (diff) | |
download | platform-system-libvintf-master.tar.gz platform-system-libvintf-master.tar.xz platform-system-libvintf-master.zip |
VintfObject.h still references the original system/vendor locations for
manifests. These now correspond to many possible locations with legacy
compatibility rules and are themselves subject to change. Now, the
header just declares that they are built from component pieces.
Bug: 76108617
Test: N/A
Change-Id: Ie9d0353b0beb0aa1fb6b1ae23ff70bab98ae2667
-rw-r--r-- | include/vintf/VintfObject.h | 35 |
1 files changed, 19 insertions, 16 deletions
diff --git a/include/vintf/VintfObject.h b/include/vintf/VintfObject.h index 50c1fed..67c33b6 100644 --- a/include/vintf/VintfObject.h +++ b/include/vintf/VintfObject.h | |||
@@ -94,26 +94,29 @@ class VintfObject { | |||
94 | std::unique_ptr<details::PropertyFetcher>&& = nullptr); | 94 | std::unique_ptr<details::PropertyFetcher>&& = nullptr); |
95 | 95 | ||
96 | /* | 96 | /* |
97 | * Return the API that access the device-side HAL manifest stored | 97 | * Return the API that access the device-side HAL manifests built from component pieces on the |
98 | * in /vendor/manifest.xml. | 98 | * vendor partition. |
99 | */ | 99 | */ |
100 | std::shared_ptr<const HalManifest> getDeviceHalManifest(bool skipCache = false); | 100 | std::shared_ptr<const HalManifest> getDeviceHalManifest(bool skipCache = false); |
101 | 101 | ||
102 | /* | 102 | /* |
103 | * Return the API that access the framework-side HAL manifest stored | 103 | * Return the API that access the framework-side HAL manifest built from component pieces on the |
104 | * in /system/manfiest.xml. | 104 | * system partition. |
105 | */ | 105 | */ |
106 | std::shared_ptr<const HalManifest> getFrameworkHalManifest(bool skipCache = false); | 106 | std::shared_ptr<const HalManifest> getFrameworkHalManifest(bool skipCache = false); |
107 | 107 | ||
108 | /* | 108 | /* |
109 | * Return the API that access the device-side compatibility matrix stored | 109 | * Return the API that access the device-side compatibility matrix built from component pieces |
110 | * in /vendor/compatibility_matrix.xml. | 110 | * on the vendor partition. |
111 | */ | 111 | */ |
112 | std::shared_ptr<const CompatibilityMatrix> getDeviceCompatibilityMatrix(bool skipCache = false); | 112 | std::shared_ptr<const CompatibilityMatrix> getDeviceCompatibilityMatrix(bool skipCache = false); |
113 | 113 | ||
114 | /* | 114 | /* |
115 | * Return the API that access the framework-side compatibility matrix stored | 115 | * Return the API that access the framework-side compatibility matrix built from component |
116 | * in /system/compatibility_matrix.xml. | 116 | * pieces on the system partition. |
117 | * | ||
118 | * This automatically selects the right compatibility matrix according to the target-level | ||
119 | * specified by the device. | ||
117 | */ | 120 | */ |
118 | std::shared_ptr<const CompatibilityMatrix> getFrameworkCompatibilityMatrix( | 121 | std::shared_ptr<const CompatibilityMatrix> getFrameworkCompatibilityMatrix( |
119 | bool skipCache = false); | 122 | bool skipCache = false); |
@@ -228,27 +231,27 @@ class VintfObject { | |||
228 | // Static variants of member functions. | 231 | // Static variants of member functions. |
229 | 232 | ||
230 | /* | 233 | /* |
231 | * Return the API that access the device-side HAL manifest stored | 234 | * Return the API that access the device-side HAL manifest built from component pieces on the |
232 | * in /vendor/manifest.xml. | 235 | * vendor partition. |
233 | */ | 236 | */ |
234 | static std::shared_ptr<const HalManifest> GetDeviceHalManifest(bool skipCache = false); | 237 | static std::shared_ptr<const HalManifest> GetDeviceHalManifest(bool skipCache = false); |
235 | 238 | ||
236 | /* | 239 | /* |
237 | * Return the API that access the framework-side HAL manifest stored | 240 | * Return the API that access the framework-side HAL manifest built from component pieces on the |
238 | * in /system/manfiest.xml. | 241 | * system partition. |
239 | */ | 242 | */ |
240 | static std::shared_ptr<const HalManifest> GetFrameworkHalManifest(bool skipCache = false); | 243 | static std::shared_ptr<const HalManifest> GetFrameworkHalManifest(bool skipCache = false); |
241 | 244 | ||
242 | /* | 245 | /* |
243 | * Return the API that access the device-side compatibility matrix stored | 246 | * Return the API that access the device-side compatibility matrix built from component pieces |
244 | * in /vendor/compatibility_matrix.xml. | 247 | * on the vendor partition. |
245 | */ | 248 | */ |
246 | static std::shared_ptr<const CompatibilityMatrix> GetDeviceCompatibilityMatrix( | 249 | static std::shared_ptr<const CompatibilityMatrix> GetDeviceCompatibilityMatrix( |
247 | bool skipCache = false); | 250 | bool skipCache = false); |
248 | 251 | ||
249 | /* | 252 | /* |
250 | * Return the API that access the framework-side compatibility matrix stored | 253 | * Return the API that access the framework-side compatibility matrix built from component |
251 | * in /system/compatibility_matrix.xml. | 254 | * pieces on the system partition. |
252 | */ | 255 | */ |
253 | static std::shared_ptr<const CompatibilityMatrix> GetFrameworkCompatibilityMatrix( | 256 | static std::shared_ptr<const CompatibilityMatrix> GetFrameworkCompatibilityMatrix( |
254 | bool skipCache = false); | 257 | bool skipCache = false); |