summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
-rw-r--r--include/vintf/VintfObject.h35
1 files changed, 19 insertions, 16 deletions
diff --git a/include/vintf/VintfObject.h b/include/vintf/VintfObject.h
index 50c1fed..67c33b6 100644
--- a/include/vintf/VintfObject.h
+++ b/include/vintf/VintfObject.h
@@ -94,26 +94,29 @@ class VintfObject {
94 std::unique_ptr<details::PropertyFetcher>&& = nullptr); 94 std::unique_ptr<details::PropertyFetcher>&& = nullptr);
95 95
96 /* 96 /*
97 * Return the API that access the device-side HAL manifest stored 97 * Return the API that access the device-side HAL manifests built from component pieces on the
98 * in /vendor/manifest.xml. 98 * vendor partition.
99 */ 99 */
100 std::shared_ptr<const HalManifest> getDeviceHalManifest(bool skipCache = false); 100 std::shared_ptr<const HalManifest> getDeviceHalManifest(bool skipCache = false);
101 101
102 /* 102 /*
103 * Return the API that access the framework-side HAL manifest stored 103 * Return the API that access the framework-side HAL manifest built from component pieces on the
104 * in /system/manfiest.xml. 104 * system partition.
105 */ 105 */
106 std::shared_ptr<const HalManifest> getFrameworkHalManifest(bool skipCache = false); 106 std::shared_ptr<const HalManifest> getFrameworkHalManifest(bool skipCache = false);
107 107
108 /* 108 /*
109 * Return the API that access the device-side compatibility matrix stored 109 * Return the API that access the device-side compatibility matrix built from component pieces
110 * in /vendor/compatibility_matrix.xml. 110 * on the vendor partition.
111 */ 111 */
112 std::shared_ptr<const CompatibilityMatrix> getDeviceCompatibilityMatrix(bool skipCache = false); 112 std::shared_ptr<const CompatibilityMatrix> getDeviceCompatibilityMatrix(bool skipCache = false);
113 113
114 /* 114 /*
115 * Return the API that access the framework-side compatibility matrix stored 115 * Return the API that access the framework-side compatibility matrix built from component
116 * in /system/compatibility_matrix.xml. 116 * pieces on the system partition.
117 *
118 * This automatically selects the right compatibility matrix according to the target-level
119 * specified by the device.
117 */ 120 */
118 std::shared_ptr<const CompatibilityMatrix> getFrameworkCompatibilityMatrix( 121 std::shared_ptr<const CompatibilityMatrix> getFrameworkCompatibilityMatrix(
119 bool skipCache = false); 122 bool skipCache = false);
@@ -228,27 +231,27 @@ class VintfObject {
228 // Static variants of member functions. 231 // Static variants of member functions.
229 232
230 /* 233 /*
231 * Return the API that access the device-side HAL manifest stored 234 * Return the API that access the device-side HAL manifest built from component pieces on the
232 * in /vendor/manifest.xml. 235 * vendor partition.
233 */ 236 */
234 static std::shared_ptr<const HalManifest> GetDeviceHalManifest(bool skipCache = false); 237 static std::shared_ptr<const HalManifest> GetDeviceHalManifest(bool skipCache = false);
235 238
236 /* 239 /*
237 * Return the API that access the framework-side HAL manifest stored 240 * Return the API that access the framework-side HAL manifest built from component pieces on the
238 * in /system/manfiest.xml. 241 * system partition.
239 */ 242 */
240 static std::shared_ptr<const HalManifest> GetFrameworkHalManifest(bool skipCache = false); 243 static std::shared_ptr<const HalManifest> GetFrameworkHalManifest(bool skipCache = false);
241 244
242 /* 245 /*
243 * Return the API that access the device-side compatibility matrix stored 246 * Return the API that access the device-side compatibility matrix built from component pieces
244 * in /vendor/compatibility_matrix.xml. 247 * on the vendor partition.
245 */ 248 */
246 static std::shared_ptr<const CompatibilityMatrix> GetDeviceCompatibilityMatrix( 249 static std::shared_ptr<const CompatibilityMatrix> GetDeviceCompatibilityMatrix(
247 bool skipCache = false); 250 bool skipCache = false);
248 251
249 /* 252 /*
250 * Return the API that access the framework-side compatibility matrix stored 253 * Return the API that access the framework-side compatibility matrix built from component
251 * in /system/compatibility_matrix.xml. 254 * pieces on the system partition.
252 */ 255 */
253 static std::shared_ptr<const CompatibilityMatrix> GetFrameworkCompatibilityMatrix( 256 static std::shared_ptr<const CompatibilityMatrix> GetFrameworkCompatibilityMatrix(
254 bool skipCache = false); 257 bool skipCache = false);