/* * Copyright (C) 2017 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #include "CompatibilityMatrix.h" #include #include #include #include "parse_string.h" #include "parse_xml.h" #include "utils.h" namespace android { namespace vintf { bool CompatibilityMatrix::addKernel(MatrixKernel&& kernel, std::string* error) { if (mType != SchemaType::FRAMEWORK) { if (error) { *error = "Cannot add to a " + to_string(mType) + " compatibility matrix."; } return false; } auto it = framework.mKernels.begin(); for (; it != framework.mKernels.end(); ++it) { if (it->minLts() == kernel.minLts()) { break; } if (it->minLts().version == kernel.minLts().version && it->minLts().majorRev == kernel.minLts().majorRev) { if (error) { *error = "Kernel version mismatch; cannot add " + to_string(kernel.minLts()) + " because " + to_string(it->minLts()) + " was added."; } return false; } } bool seenVersion = it != framework.mKernels.end(); if (seenVersion) { // If no conditions, must be the first among the same minLts // because O libvintf only checks the first tag that version matches. if (kernel.conditions().empty()) { // Found first with the same minLts. // Append config if it does not have s, else error. if (it->conditions().empty()) { const auto& configs = kernel.configs(); it->mConfigs.insert(it->mConfigs.end(), configs.begin(), configs.end()); } else { if (error) { *error = "Base compatibility matrix has for the first " "with minlts " + to_string(kernel.minLts()) + " for unknown reason."; } return false; } return true; } } else { // First of a minLts must not have 's for backwards compatibility // with O libvintf. if (!kernel.conditions().empty()) { framework.mKernels.push_back(MatrixKernel(KernelVersion{kernel.minLts()}, {})); } } framework.mKernels.push_back(std::move(kernel)); return true; } SchemaType CompatibilityMatrix::type() const { return mType; } Level CompatibilityMatrix::level() const { return mLevel; } Version CompatibilityMatrix::getMinimumMetaVersion() const { // TODO(b/62801658): this needs to depend on whether there are 1.1 requirements // (e.g. required entry) return {1, 0}; } status_t CompatibilityMatrix::fetchAllInformation(const FileSystem* fileSystem, const std::string& path, std::string* error) { return details::fetchAllInformation(fileSystem, path, gCompatibilityMatrixConverter, this, error); } std::string CompatibilityMatrix::getXmlSchemaPath(const std::string& xmlFileName, const Version& version) const { using std::literals::string_literals::operator""s; auto range = getXmlFiles(xmlFileName); for (auto it = range.first; it != range.second; ++it) { const MatrixXmlFile& matrixXmlFile = it->second; if (matrixXmlFile.versionRange().contains(version)) { if (!matrixXmlFile.overriddenPath().empty()) { return matrixXmlFile.overriddenPath(); } return "/"s + (type() == SchemaType::DEVICE ? "vendor" : "system") + "/etc/" + xmlFileName + "_V" + std::to_string(matrixXmlFile.versionRange().majorVer) + "_" + std::to_string(matrixXmlFile.versionRange().maxMinor) + "." + to_string(matrixXmlFile.format()); } } return ""; } // Split existingHal into a HAL that contains only interface/instance and a HAL // that does not contain it. Return the HAL that contains only interface/instance. // - Return nullptr if existingHal does not contain interface/instance // - Return existingHal if existingHal contains only interface/instance // - Remove interface/instance from existingHal, and return a new MatrixHal (that is added // to "this") that contains only interface/instance. MatrixHal* CompatibilityMatrix::splitInstance(MatrixHal* existingHal, const std::string& interface, const std::string& instanceOrPattern, bool isRegex) { bool found = false; bool foundOthers = false; existingHal->forEachInstance([&](const auto& matrixInstance) { bool interfaceMatch = matrixInstance.interface() == interface; bool instanceMatch = false; if (matrixInstance.isRegex() && isRegex) { instanceMatch = (matrixInstance.regexPattern() == instanceOrPattern); } else if (!matrixInstance.isRegex() && !isRegex) { instanceMatch = (matrixInstance.exactInstance() == instanceOrPattern); } bool match = interfaceMatch && instanceMatch; found |= match; foundOthers |= (!match); return !found || !foundOthers; }); if (!found) { return nullptr; } if (!foundOthers) { return existingHal; } existingHal->removeInstance(interface, instanceOrPattern, isRegex); MatrixHal copy = *existingHal; copy.clearInstances(); copy.insertInstance(interface, instanceOrPattern, isRegex); return addInternal(std::move(copy)); } // Add all package@other_version::interface/instance as an optional instance. // If package@this_version::interface/instance is in this (that is, some instance // with the same package and interface and instance exists), then other_version is // considered a possible replacement to this_version. // See LibVintfTest.AddOptionalHal* tests for details. bool CompatibilityMatrix::addAllHalsAsOptional(CompatibilityMatrix* other, std::string* error) { if (other == nullptr || other->level() <= level()) { return true; } for (auto& pair : other->mHals) { const std::string& name = pair.first; MatrixHal& halToAdd = pair.second; std::set> insertedInstances; std::set> insertedRegex; auto existingHals = getHals(name); halToAdd.forEachInstance([&](const std::vector& versionRanges, const std::string& interface, const std::string& instanceOrPattern, bool isRegex) { for (auto* existingHal : existingHals) { MatrixHal* splitInstance = this->splitInstance(existingHal, interface, instanceOrPattern, isRegex); if (splitInstance != nullptr) { splitInstance->insertVersionRanges(versionRanges); if (isRegex) { insertedRegex.insert(std::make_pair(interface, instanceOrPattern)); } else { insertedInstances.insert(std::make_pair(interface, instanceOrPattern)); } } } return true; }); // Add the remaining instances. for (const auto& pair : insertedInstances) { halToAdd.removeInstance(pair.first, pair.second, false /* isRegex */); } for (const auto& pair : insertedRegex) { halToAdd.removeInstance(pair.first, pair.second, true /* isRegex */); } if (halToAdd.instancesCount() > 0) { halToAdd.setOptional(true); if (!add(std::move(halToAdd))) { if (error) { *error = "Cannot add HAL " + name + " for unknown reason."; } return false; } } } return true; } bool CompatibilityMatrix::addAllXmlFilesAsOptional(CompatibilityMatrix* other, std::string* error) { if (other == nullptr || other->level() <= level()) { return true; } for (auto& pair : other->mXmlFiles) { const std::string& name = pair.first; MatrixXmlFile& xmlFileToAdd = pair.second; xmlFileToAdd.mOptional = true; if (!addXmlFile(std::move(xmlFileToAdd))) { if (error) { *error = "Cannot add XML File " + name + " for unknown reason."; } return false; } } return true; } // Merge Kernel. // Add from exact "level", then optionally add from high levels to low levels. // For example, (each letter is a kernel version x.y.z) // 1.xml: A1, B1 // 2.xml: B2, C2, D2 // 3.xml: D3, E3 // Then the combined 1.xml should have // A1, B1 (from 1.xml, required), C2, D2, E3 (optional, use earliest possible). bool CompatibilityMatrix::addAllKernels(CompatibilityMatrix* other, std::string* error) { for (MatrixKernel& kernel : other->framework.mKernels) { KernelVersion ver = kernel.minLts(); if (!addKernel(std::move(kernel), error)) { if (error) { *error = "Cannot add kernel version " + to_string(ver) + ": " + *error; } return false; } } return true; } bool CompatibilityMatrix::addAllKernelsAsOptional(CompatibilityMatrix* other, std::string* error) { if (other == nullptr || other->level() <= level()) { return true; } for (MatrixKernel& kernelToAdd : other->framework.mKernels) { bool exists = std::any_of(this->framework.mKernels.begin(), this->framework.mKernels.end(), [&kernelToAdd](const MatrixKernel& existing) { return kernelToAdd.minLts().version == existing.minLts().version && kernelToAdd.minLts().majorRev == existing.minLts().majorRev; }); if (exists) { // Shouldn't retroactively add requirements to minLts(), so ignore this. // This happens even when kernelToAdd.conditions() != existing.conditions(). continue; } KernelVersion minLts = kernelToAdd.minLts(); if (!addKernel(std::move(kernelToAdd), error)) { if (error) { *error = "Cannot add " + to_string(minLts) + ": " + *error; } return false; } } return true; } template static bool mergeField(T* dst, T* src) { static const T kEmpty{}; if (*dst == *src) { return true; // no conflict } if (*src == kEmpty) { return true; } if (*dst == kEmpty) { *dst = std::move(*src); return true; } return false; } bool CompatibilityMatrix::addSepolicy(CompatibilityMatrix* other, std::string* error) { bool success = mergeField(&this->framework.mSepolicy, &other->framework.mSepolicy); if (!success && error) *error = " is already defined"; return success; } bool CompatibilityMatrix::addAvbMetaVersion(CompatibilityMatrix* other, std::string* error) { bool success = mergeField(&this->framework.mAvbMetaVersion, &other->framework.mAvbMetaVersion); if (!success && error) *error = " is already defined"; return success; } bool operator==(const CompatibilityMatrix &lft, const CompatibilityMatrix &rgt) { return lft.mType == rgt.mType && lft.mLevel == rgt.mLevel && lft.mHals == rgt.mHals && lft.mXmlFiles == rgt.mXmlFiles && (lft.mType != SchemaType::DEVICE || ( #pragma clang diagnostic push #pragma clang diagnostic ignored "-Wdeprecated-declarations" lft.device.mVndk == rgt.device.mVndk && #pragma clang diagnostic pop lft.device.mVendorNdk == rgt.device.mVendorNdk && lft.device.mSystemSdk == rgt.device.mSystemSdk)) && (lft.mType != SchemaType::FRAMEWORK || (lft.framework.mKernels == rgt.framework.mKernels && lft.framework.mSepolicy == rgt.framework.mSepolicy && lft.framework.mAvbMetaVersion == rgt.framework.mAvbMetaVersion)); } std::unique_ptr CompatibilityMatrix::combine( Level deviceLevel, std::vector>* matrices, std::string* error) { // Check type. for (const auto& e : *matrices) { if (e.object.type() != SchemaType::FRAMEWORK) { if (error) { *error = "File \"" + e.name + "\" is not a framework compatibility matrix."; return nullptr; } } } // Matrices with unspecified (empty) level are auto-filled with deviceLevel. for (auto& e : *matrices) { if (e.object.level() == Level::UNSPECIFIED) { e.object.mLevel = deviceLevel; } } // Add from low to high FCM version so that optional requirements are added correctly. // See comment in addAllAsOptional. std::sort(matrices->begin(), matrices->end(), [](const auto& x, const auto& y) { return x.object.level() < y.object.level(); }); auto baseMatrix = std::make_unique(); baseMatrix->mLevel = deviceLevel; baseMatrix->mType = SchemaType::FRAMEWORK; std::vector parsedFiles; for (auto& e : *matrices) { if (e.object.level() < deviceLevel) { continue; } bool success = false; if (e.object.level() == deviceLevel) { success = baseMatrix->addAll(&e, error); } else { success = baseMatrix->addAllAsOptional(&e, error); } if (!success) { if (error) { *error = "Conflict when merging \"" + e.name + "\": " + *error + "\n" + "Previous files:\n" + base::Join(parsedFiles, "\n"); } return nullptr; } parsedFiles.push_back(e.name); } return baseMatrix; } bool CompatibilityMatrix::addAll(Named* inputMatrix, std::string* error) { if (!addAllHals(&inputMatrix->object, error) || !addAllXmlFiles(&inputMatrix->object, error) || !addAllKernels(&inputMatrix->object, error) || !addSepolicy(&inputMatrix->object, error) || !addAvbMetaVersion(&inputMatrix->object, error)) { if (error) { *error = "File \"" + inputMatrix->name + "\" cannot be added: " + *error + "."; } } return true; } bool CompatibilityMatrix::addAllAsOptional(Named* inputMatrix, std::string* error) { if (!addAllHalsAsOptional(&inputMatrix->object, error) || !addAllXmlFilesAsOptional(&inputMatrix->object, error) || !addAllKernelsAsOptional(&inputMatrix->object, error)) { if (error) { *error = "File \"" + inputMatrix->name + "\" cannot be added: " + *error; } return false; } // ignore requirement from higher level // ignore requirement from higher level return true; } bool CompatibilityMatrix::forEachInstanceOfVersion( const std::string& package, const Version& expectVersion, const std::function& func) const { for (const MatrixHal* hal : getHals(package)) { bool cont = hal->forEachInstance([&](const MatrixInstance& matrixInstance) { if (matrixInstance.versionRange().contains(expectVersion)) { return func(matrixInstance); } return true; }); if (!cont) return false; } return true; } bool CompatibilityMatrix::matchInstance(const std::string& halName, const Version& version, const std::string& interfaceName, const std::string& instance) const { bool found = false; (void)forEachInstanceOfInterface(halName, version, interfaceName, [&found, &instance](const auto& e) { found |= (e.matchInstance(instance)); return !found; // if not found, continue }); return found; } std::string CompatibilityMatrix::getVendorNdkVersion() const { return type() == SchemaType::DEVICE ? device.mVendorNdk.version() : ""; } } // namespace vintf } // namespace android