summaryrefslogtreecommitdiffstats
blob: 3f058811c70434fd0120bf117e4123f545cbdec7 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
/*
 * Copyright (C) 2017 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include "CompatibilityMatrix.h"

#include <iostream>
#include <utility>

#include "parse_string.h"
#include "parse_xml.h"
#include "utils.h"

namespace android {
namespace vintf {

bool CompatibilityMatrix::add(MatrixHal &&hal) {
    return HalGroup<MatrixHal>::add(std::move(hal));
}

bool CompatibilityMatrix::add(MatrixKernel &&kernel) {
    if (mType != SchemaType::FRAMEWORK) {
        return false;
    }
    framework.mKernels.push_back(std::move(kernel));
    return true;
}

SchemaType CompatibilityMatrix::type() const {
    return mType;
}

Level CompatibilityMatrix::level() const {
    return mLevel;
}

Version CompatibilityMatrix::getMinimumMetaVersion() const {
    // TODO(b/62801658): this needs to depend on whether there are 1.1 requirements
    // (e.g. required <xmlfile> entry)
    return {1, 0};
}

status_t CompatibilityMatrix::fetchAllInformation(const std::string& path, std::string* error) {
    return details::fetchAllInformation(path, gCompatibilityMatrixConverter, this, error);
}

std::string CompatibilityMatrix::getXmlSchemaPath(const std::string& xmlFileName,
                                                  const Version& version) const {
    using std::literals::string_literals::operator""s;
    auto range = getXmlFiles(xmlFileName);
    for (auto it = range.first; it != range.second; ++it) {
        const MatrixXmlFile& matrixXmlFile = it->second;
        if (matrixXmlFile.versionRange().contains(version)) {
            if (!matrixXmlFile.overriddenPath().empty()) {
                return matrixXmlFile.overriddenPath();
            }
            return "/"s + (type() == SchemaType::DEVICE ? "vendor" : "system") + "/etc/" +
                   xmlFileName + "_V" + std::to_string(matrixXmlFile.versionRange().majorVer) +
                   "_" + std::to_string(matrixXmlFile.versionRange().maxMinor) + "." +
                   to_string(matrixXmlFile.format());
        }
    }
    return "";
}

// Add all package@other_version::interface/instance as an optional instance.
// If package@this_version::interface/instance is in this (that is, some instance
// with the same package and interface and instance exists), then other_version is
// considered a possible replacement to this_version.
// See LibVintfTest.AddOptionalHal* tests for details.
bool CompatibilityMatrix::addAllHalsAsOptional(CompatibilityMatrix* other, std::string* error) {
    if (other == nullptr || other->level() <= level()) {
        return true;
    }

    for (auto& pair : other->mHals) {
        const std::string& name = pair.first;
        MatrixHal& halToAdd = pair.second;

        bool added = false;
        for (auto* existingHal : getHals(name)) {
            if (existingHal->containsInstances(halToAdd)) {
                existingHal->insertVersionRanges(halToAdd);
                added = true;
                // Do not break here; try other <hal> with the same name as well.
            }
        }

        if (!added) {
            halToAdd.setOptional(true);
            if (!add(std::move(halToAdd))) {
                if (error) {
                    *error = "Cannot add HAL " + name + " for unknown reason.";
                }
                return false;
            }
        }
    }
    return true;
}

bool CompatibilityMatrix::addAllXmlFilesAsOptional(CompatibilityMatrix* other, std::string* error) {
    if (other == nullptr || other->level() <= level()) {
        return true;
    }
    for (auto& pair : other->mXmlFiles) {
        const std::string& name = pair.first;
        MatrixXmlFile& xmlFileToAdd = pair.second;

        xmlFileToAdd.mOptional = true;
        if (!addXmlFile(std::move(xmlFileToAdd))) {
            if (error) {
                *error = "Cannot add XML File " + name + " for unknown reason.";
            }
            return false;
        }
    }
    return true;
}

bool operator==(const CompatibilityMatrix &lft, const CompatibilityMatrix &rgt) {
    return lft.mType == rgt.mType && lft.mLevel == rgt.mLevel && lft.mHals == rgt.mHals &&
           lft.mXmlFiles == rgt.mXmlFiles &&
           (lft.mType != SchemaType::DEVICE ||
            (
#pragma clang diagnostic push
#pragma clang diagnostic ignored "-Wdeprecated-declarations"
                lft.device.mVndk == rgt.device.mVndk &&
#pragma clang diagnostic pop
                lft.device.mVendorNdk == rgt.device.mVendorNdk &&
                lft.device.mSystemSdk == rgt.device.mSystemSdk)) &&
           (lft.mType != SchemaType::FRAMEWORK ||
            (lft.framework.mKernels == rgt.framework.mKernels &&
             lft.framework.mSepolicy == rgt.framework.mSepolicy &&
             lft.framework.mAvbMetaVersion == rgt.framework.mAvbMetaVersion));
}

// Find compatibility_matrix.empty.xml (which has unspecified level) and use it
// as a base matrix.
CompatibilityMatrix* CompatibilityMatrix::findOrInsertBaseMatrix(
    std::vector<Named<CompatibilityMatrix>>* matrices, std::string* error) {
    bool multipleFound = false;
    CompatibilityMatrix* matrix = nullptr;
    for (auto& e : *matrices) {
        if (e.object.level() == Level::UNSPECIFIED) {
            if (!e.object.mHals.empty()) {
                if (error) {
                    *error = "Error: File \"" + e.name + "\" should not contain " + "HAL elements.";
                }
                return nullptr;
            }

            if (!e.object.mXmlFiles.empty()) {
                if (error) {
                    *error =
                        "Error: File \"" + e.name + "\" should not contain " + "XML File elements.";
                }
                return nullptr;
            }

            if (matrix != nullptr) {
                multipleFound = true;
            }

            matrix = &e.object;
            // continue to detect multiple files with "unspecified" levels
        }
    }

    if (multipleFound) {
        if (error) {
            *error =
                "Error: multiple framework compatibility matrix files have "
                "unspecified level; there should only be one such file.\n";
            for (auto& e : *matrices) {
                if (e.object.level() == Level::UNSPECIFIED) {
                    *error += "    " + e.name + "\n";
                }
            }
        }
        return nullptr;
    }

    if (matrix == nullptr) {
        matrix = &matrices->emplace(matrices->end())->object;
        matrix->mType = SchemaType::FRAMEWORK;
        matrix->mLevel = Level::UNSPECIFIED;
    }

    return matrix;
}

CompatibilityMatrix* CompatibilityMatrix::combine(Level deviceLevel,
                                                  std::vector<Named<CompatibilityMatrix>>* matrices,
                                                  std::string* error) {
    if (deviceLevel == Level::UNSPECIFIED) {
        if (error) {
            *error = "Error: device level is unspecified.";
        }
        return nullptr;
    }

    CompatibilityMatrix* matrix = findOrInsertBaseMatrix(matrices, error);
    if (matrix == nullptr) {
        return nullptr;
    }

    matrix->mLevel = deviceLevel;

    for (auto& e : *matrices) {
        if (&e.object != matrix && e.object.level() == deviceLevel) {
            if (!matrix->addAllHals(&e.object, error)) {
                if (error) {
                    *error = "File \"" + e.name + "\" cannot be added: HAL " + *error +
                             " has a conflict.";
                }
                return nullptr;
            }

            if (!matrix->addAllXmlFiles(&e.object, error)) {
                if (error) {
                    *error = "File \"" + e.name + "\" cannot be added: XML File entry " + *error +
                             " has a conflict.";
                }
                return nullptr;
            }
        }
    }

    for (auto& e : *matrices) {
        if (&e.object != matrix && e.object.level() != Level::UNSPECIFIED &&
            e.object.level() > deviceLevel) {
            if (!matrix->addAllHalsAsOptional(&e.object, error)) {
                if (error) {
                    *error = "File \"" + e.name + "\" cannot be added: " + *error +
                             ". See <hal> with the same name " +
                             "in previously parsed files or previously declared in this file.";
                }
                return nullptr;
            }

            if (!matrix->addAllXmlFilesAsOptional(&e.object, error)) {
                if (error) {
                    *error = "File \"" + e.name + "\" cannot be added: XML File entry " + *error +
                             " has a conflict.";
                }
                return nullptr;
            }
        }
    }

    for (auto& e : *matrices) {
        if (&e.object != matrix && e.object.level() == deviceLevel &&
            e.object.type() == SchemaType::FRAMEWORK) {
            for (MatrixKernel& kernel : e.object.framework.mKernels) {
                KernelVersion ver = kernel.minLts();
                if (!matrix->add(std::move(kernel))) {
                    if (error) {
                        *error = "Cannot add kernel version " + to_string(ver) +
                                 " from FCM version " + to_string(deviceLevel);
                    }
                    return nullptr;
                }
            }
        }
    }

    return matrix;
}

bool CompatibilityMatrix::forEachInstanceOfVersion(
    const std::string& package, const Version& expectVersion,
    const std::function<bool(const MatrixInstance&)>& func) const {
    for (const MatrixHal* hal : getHals(package)) {
        bool cont = hal->forEachInstance([&](const MatrixInstance& matrixInstance) {
            if (matrixInstance.versionRange().contains(expectVersion)) {
                return func(matrixInstance);
            }
            return true;
        });
        if (!cont) return false;
    }
    return true;
}

} // namespace vintf
} // namespace android