1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
|
/*
* Copyright (C) 2017 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef ANDROID_VINTF_COMPATIBILITY_MATRIX_H
#define ANDROID_VINTF_COMPATIBILITY_MATRIX_H
#include <map>
#include <string>
#include <utils/Errors.h>
#include "HalGroup.h"
#include "Level.h"
#include "MapValueIterator.h"
#include "MatrixHal.h"
#include "MatrixKernel.h"
#include "Named.h"
#include "SchemaType.h"
#include "Sepolicy.h"
#include "VendorNdk.h"
#include "Vndk.h"
#include "XmlFileGroup.h"
namespace android {
namespace vintf {
// Compatibility matrix defines what hardware does the framework requires.
struct CompatibilityMatrix : public HalGroup<MatrixHal>, public XmlFileGroup<MatrixXmlFile> {
// Create a framework compatibility matrix.
CompatibilityMatrix() : mType(SchemaType::FRAMEWORK) {};
SchemaType type() const;
Level level() const;
Version getMinimumMetaVersion() const;
// If the corresponding <xmlfile> with the given version exists, for the first match,
// - Return the overridden <path> if it is present,
// - otherwise the default value: /{system,vendor}/etc/<name>_V<major>_<minor-max>.<format>
// Otherwise if the <xmlfile> entry does not exist, "" is returned.
// For example, if the matrix says ["audio@1.0-5" -> "foo.xml", "audio@1.3-7" -> bar.xml]
// getXmlSchemaPath("audio", 1.0) -> foo.xml
// getXmlSchemaPath("audio", 1.5) -> foo.xml
// getXmlSchemaPath("audio", 1.7) -> bar.xml
// (Normally, version ranges do not overlap, and the only match is returned.)
std::string getXmlSchemaPath(const std::string& xmlFileName, const Version& version) const;
private:
bool add(MatrixHal &&hal);
bool add(MatrixKernel &&kernel);
// Add all HALs as optional HALs from "other". This function moves MatrixHal objects
// from "other".
// Require other->level() > this->level(), otherwise do nothing.
bool addAllHalsAsOptional(CompatibilityMatrix* other, std::string* error);
// Return the MatrixHal object with the given name and major version. Since all major
// version are guaranteed distinct when add()-ed, there should be at most 1 match.
// Return nullptr if none is found.
std::pair<MatrixHal*, VersionRange*> getHalWithMajorVersion(const std::string& name,
size_t majorVer);
// Similar to addAllHalsAsOptional but on <xmlfile> entries.
bool addAllXmlFilesAsOptional(CompatibilityMatrix* other, std::string* error);
status_t fetchAllInformation(const std::string& path, std::string* error = nullptr);
// Combine a subset of "matrices". For each CompatibilityMatrix in matrices,
// - If level() == UNSPECIFIED, use it as the base matrix (for non-HAL, non-XML-file
// requirements).
// - If level() < deviceLevel, ignore
// - If level() == deviceLevel, all HAL versions and XML files are added as is
// (optionality is kept)
// - If level() > deviceLevel, all HAL versions and XML files are added as optional.
// Return a pointer into one of the elements in "matrices".
static CompatibilityMatrix* combine(Level deviceLevel,
std::vector<Named<CompatibilityMatrix>>* matrices,
std::string* error);
static CompatibilityMatrix* findOrInsertBaseMatrix(
std::vector<Named<CompatibilityMatrix>>* matrices, std::string* error);
friend struct HalManifest;
friend struct RuntimeInfo;
friend struct CompatibilityMatrixConverter;
friend struct LibVintfTest;
friend class VintfObject;
friend class AssembleVintfImpl;
friend bool operator==(const CompatibilityMatrix &, const CompatibilityMatrix &);
SchemaType mType;
Level mLevel = Level::UNSPECIFIED;
// entries only for framework compatibility matrix.
struct {
std::vector<MatrixKernel> mKernels;
Sepolicy mSepolicy;
Version mAvbMetaVersion;
} framework;
// entries only for device compatibility matrix.
struct {
#pragma clang diagnostic push
#pragma clang diagnostic ignored "-Wdeprecated-declarations"
Vndk mVndk;
#pragma clang diagnostic pop
VendorNdk mVendorNdk;
} device;
};
} // namespace vintf
} // namespace android
#endif // ANDROID_VINTF_COMPATIBILITY_MATRIX_H
|