1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
|
/*
* Copyright (C) 2017 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef ANDROID_VINTF_HAL_GROUP_H
#define ANDROID_VINTF_HAL_GROUP_H
#include <map>
#include <set>
#include "MapValueIterator.h"
#include "Version.h"
namespace android {
namespace vintf {
// A HalGroup is a wrapped multimap from name to Hal.
// Hal.getName() must return a string indicating the name.
template <typename Hal>
struct HalGroup {
public:
virtual ~HalGroup() {}
// Move all hals from another HalGroup to this.
bool addAllHals(HalGroup* other, std::string* error = nullptr) {
for (auto& pair : other->mHals) {
if (!add(std::move(pair.second))) {
if (error) {
*error = pair.first;
}
return false;
}
}
return true;
}
// Add an hal to this HalGroup so that it can be constructed programatically.
virtual bool add(Hal&& hal) {
if (!shouldAdd(hal)) {
return false;
}
std::string name = hal.getName();
mHals.emplace(std::move(name), std::move(hal)); // always succeed
return true;
}
// Get all hals with the given name (e.g "android.hardware.camera").
// There could be multiple hals that matches the same given name.
std::vector<const Hal*> getHals(const std::string& name) const {
std::vector<const Hal*> ret;
auto range = mHals.equal_range(name);
for (auto it = range.first; it != range.second; ++it) {
ret.push_back(&it->second);
}
return ret;
}
// Get all hals with the given name (e.g "android.hardware.camera").
// There could be multiple hals that matches the same given name.
// Non-const version of the above getHals() method.
std::vector<Hal*> getHals(const std::string& name) {
std::vector<Hal*> ret;
auto range = mHals.equal_range(name);
for (auto it = range.first; it != range.second; ++it) {
ret.push_back(&it->second);
}
return ret;
}
// Get the hal that matches the given name and version (e.g.
// "android.hardware.camera@2.4")
// There should be a single hal that matches the given name and version.
const Hal* getHal(const std::string& name, const Version& version) const {
for (const Hal* hal : getHals(name)) {
if (hal->containsVersion(version)) return hal;
}
return nullptr;
}
// Get all instance names for hal that matches the given component name, version
// and interface name (e.g. "android.hardware.camera@2.4::ICameraProvider").
// * If the component ("android.hardware.camera@2.4") does not exist, return empty set.
// * If the component ("android.hardware.camera@2.4") does exist,
// * If the interface (ICameraProvider) does not exist, return empty set.
// * Else return the list hal.interface.instance.
std::set<std::string> getInstances(const std::string& halName, const Version& version,
const std::string& interfaceName) const {
const Hal* hal = getHal(halName, version);
if (hal == nullptr) {
return {};
}
return hal->getInstances(interfaceName);
}
protected:
// sorted map from component name to the component.
// The component name looks like: android.hardware.foo
std::multimap<std::string, Hal> mHals;
// override this to filter for add.
virtual bool shouldAdd(const Hal&) const { return true; }
// Return an iterable to all ManifestHal objects. Call it as follows:
// for (const auto& e : vm.getHals()) { }
ConstMultiMapValueIterable<std::string, Hal> getHals() const {
return ConstMultiMapValueIterable<std::string, Hal>(mHals);
}
// Get any HAL component based on the component name. Return any one
// if multiple. Return nullptr if the component does not exist. This is only
// for creating objects programatically.
// The component name looks like:
// android.hardware.foo
Hal* getAnyHal(const std::string& name) {
auto it = mHals.find(name);
if (it == mHals.end()) {
return nullptr;
}
return &(it->second);
}
};
} // namespace vintf
} // namespace android
#endif // ANDROID_VINTF_HAL_GROUP_H
|