summaryrefslogtreecommitdiffstats
blob: 033adf007d948be591f5ee891756887bbd22b963 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
/*
 * Copyright (C) 2017 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef ANDROID_VINTF_HAL_GROUP_H
#define ANDROID_VINTF_HAL_GROUP_H

#include <map>
#include <set>

#include "MapValueIterator.h"
#include "Version.h"

namespace android {
namespace vintf {

// A HalGroup is a wrapped multimap from name to Hal.
// Hal.getName() must return a string indicating the name.
template <typename Hal>
struct HalGroup {
    using InstanceType = typename Hal::InstanceType;

   public:
    virtual ~HalGroup() {}
    // Move all hals from another HalGroup to this.
    bool addAllHals(HalGroup* other, std::string* error = nullptr) {
        for (auto& pair : other->mHals) {
            if (!add(std::move(pair.second))) {
                if (error) {
                    *error = pair.first;
                }
                return false;
            }
        }
        return true;
    }

    // Add an hal to this HalGroup so that it can be constructed programatically.
    virtual bool add(Hal&& hal) {
        if (!shouldAdd(hal)) {
            return false;
        }
        std::string name = hal.getName();
        mHals.emplace(std::move(name), std::move(hal));  // always succeed
        return true;
    }

    // Get all hals with the given name (e.g "android.hardware.camera").
    // There could be multiple hals that matches the same given name.
    // TODO(b/74247301) Deprecated; use forEachInstanceOfPackage instead.
    std::vector<const Hal*> getHals(const std::string& name) const {
        std::vector<const Hal*> ret;
        auto range = mHals.equal_range(name);
        for (auto it = range.first; it != range.second; ++it) {
            ret.push_back(&it->second);
        }
        return ret;
    }

    // Get all hals with the given name (e.g "android.hardware.camera").
    // There could be multiple hals that matches the same given name.
    // Non-const version of the above getHals() method.
    // TODO(b/74247301) Deprecated; use forEachInstanceOfPackage instead.
    std::vector<Hal*> getHals(const std::string& name) {
        std::vector<Hal*> ret;
        auto range = mHals.equal_range(name);
        for (auto it = range.first; it != range.second; ++it) {
            ret.push_back(&it->second);
        }
        return ret;
    }

    // Apply func to all instances.
    bool forEachInstance(const std::function<bool(const InstanceType&)>& func) const {
        for (const auto& hal : getHals()) {
            bool cont = hal.forEachInstance(func);
            if (!cont) return false;
        }
        return true;
    }

    bool forEachInstanceOfPackage(const std::string& package,
                                  const std::function<bool(const InstanceType&)>& func) const {
        for (const auto* hal : getHals(package)) {
            if (!hal->forEachInstance(func)) {
                return false;
            }
        }
        return true;
    }

    // Apply func to all instances of package@expectVersion::*/*.
    // For example, if a.h.foo@1.1::IFoo/default is in "this" and getFqInstances
    // is called with a.h.foo@1.0, then a.h.foo@1.1::IFoo/default is returned.
    virtual bool forEachInstanceOfVersion(
        const std::string& package, const Version& expectVersion,
        const std::function<bool(const InstanceType&)>& func) const = 0;

    // Apply func to instances of package@expectVersion::interface/*.
    // For example, if a.h.foo@1.1::IFoo/default is in "this" and getFqInstances
    // is called with a.h.foo@1.0::IFoo, then a.h.foo@1.1::IFoo/default is returned.
    bool forEachInstanceOfInterface(const std::string& package, const Version& expectVersion,
                                    const std::string& interface,
                                    const std::function<bool(const InstanceType&)>& func) const {
        return forEachInstanceOfVersion(package, expectVersion,
                                        [&func, &interface](const InstanceType& e) {
                                            if (e.interface() == interface) {
                                                return func(e);
                                            }
                                            return true;
                                        });
    }

    // Alternative to forEachInstanceOfInterface if you need a vector instead.
    // If interface is empty, returns all instances of package@version;
    // else return all instances of package@version::interface.
    std::vector<InstanceType> getFqInstances(const std::string& package,
                                             const Version& expectVersion,
                                             const std::string& interface = "") const {
        std::vector<InstanceType> v;
        auto mapToVector = [&v](const auto& e) {
            v.push_back(e);
            return true;
        };
        if (interface.empty()) {
            (void)forEachInstanceOfVersion(package, expectVersion, mapToVector);
        } else {
            (void)forEachInstanceOfInterface(package, expectVersion, interface, mapToVector);
        }
        return v;
    }

    // Alternative to forEachInstance if you just need a set of instance names instead.
    std::set<std::string> getInstances(const std::string& halName, const Version& version,
                                       const std::string& interfaceName) const {
        std::set<std::string> ret;
        (void)forEachInstanceOfInterface(halName, version, interfaceName, [&ret](const auto& e) {
            ret.insert(e.instance());
            return true;
        });
        return ret;
    }

    // Return whether instance is in getInstances(...).
    bool hasInstance(const std::string& halName, const Version& version,
                     const std::string& interfaceName, const std::string& instance) const {
        bool found = false;
        (void)forEachInstanceOfInterface(halName, version, interfaceName,
                                         [&found, &instance](const auto& e) {
                                             found |= (instance == e.instance());
                                             return !found;  // if not found, continue
                                         });
        return found;
    }

   protected:
    // sorted map from component name to the component.
    // The component name looks like: android.hardware.foo
    std::multimap<std::string, Hal> mHals;

    // override this to filter for add.
    virtual bool shouldAdd(const Hal&) const { return true; }

    // Return an iterable to all ManifestHal objects. Call it as follows:
    // for (const auto& e : vm.getHals()) { }
    ConstMultiMapValueIterable<std::string, Hal> getHals() const {
        return ConstMultiMapValueIterable<std::string, Hal>(mHals);
    }

    // Get any HAL component based on the component name. Return any one
    // if multiple. Return nullptr if the component does not exist. This is only
    // for creating objects programatically.
    // The component name looks like:
    // android.hardware.foo
    Hal* getAnyHal(const std::string& name) {
        auto it = mHals.find(name);
        if (it == mHals.end()) {
            return nullptr;
        }
        return &(it->second);
    }
};

}  // namespace vintf
}  // namespace android

#endif  // ANDROID_VINTF_HAL_GROUP_H