summaryrefslogtreecommitdiffstats
blob: 50c1fedd2161f2a2c061e018ac65d1a053d38454 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
/*
 * Copyright (C) 2017 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef ANDROID_VINTF_VINTF_OBJECT_H_
#define ANDROID_VINTF_VINTF_OBJECT_H_

#include <memory>

#include "CheckFlags.h"
#include "CompatibilityMatrix.h"
#include "FileSystem.h"
#include "HalManifest.h"
#include "Named.h"
#include "RuntimeInfo.h"

namespace android {
namespace vintf {

namespace details {
class PartitionMounter;
template <typename T>
class ObjectFactory;
class PropertyFetcher;

template <typename T>
struct LockedSharedPtr {
    std::shared_ptr<T> object;
    std::mutex mutex;
    bool fetchedOnce = false;
};

struct LockedRuntimeInfoCache {
    std::shared_ptr<RuntimeInfo> object;
    std::mutex mutex;
    RuntimeInfo::FetchFlags fetchedFlags = RuntimeInfo::FetchFlag::NONE;
};
}  // namespace details

namespace testing {
class VintfObjectTestBase;
class VintfObjectRuntimeInfoTest;
class VintfObjectCompatibleTest;
}  // namespace testing

/*
 * The top level class for libvintf.
 * An overall diagram of the public API:
 * VintfObject
 *   + GetDeviceHalManfiest
 *   |   + getTransport
 *   |   + checkCompatibility
 *   + GetFrameworkHalManifest
 *   |   + getTransport
 *   |   + checkCompatibility
 *   + GetRuntimeInfo
 *       + checkCompatibility
 *
 * Each of the function gathers all information and encapsulate it into the object.
 * If no error, it return the same singleton object in the future, and the HAL manifest
 * file won't be touched again.
 * If any error, nullptr is returned, and Get will try to parse the HAL manifest
 * again when it is called again.
 * All these operations are thread-safe.
 * If skipCache, always skip the cache in memory and read the files / get runtime information
 * again from the device.
 */
class VintfObject {
   public:
    /**
     * A VintfObject that fetches from root and cache results, unless skipCache is specified.
     * Dependencies can be injected via arguments. If nullptr is provided, the default behavior
     * is used.
     * - FileSystem fetch from "/" for target and fetch no files for host
     * - PartitionMounter does nothing for both target and host
     * - ObjectFactory<RuntimeInfo> fetches default RuntimeInfo for target and nothing for host
     * - PropertyFetcher fetches properties for target and nothing for host
     */
    VintfObject(std::unique_ptr<FileSystem>&& = nullptr,
                std::unique_ptr<details::PartitionMounter>&& = nullptr,
                std::unique_ptr<details::ObjectFactory<RuntimeInfo>>&& = nullptr,
                std::unique_ptr<details::PropertyFetcher>&& = nullptr);

    /*
     * Return the API that access the device-side HAL manifest stored
     * in /vendor/manifest.xml.
     */
    std::shared_ptr<const HalManifest> getDeviceHalManifest(bool skipCache = false);

    /*
     * Return the API that access the framework-side HAL manifest stored
     * in /system/manfiest.xml.
     */
    std::shared_ptr<const HalManifest> getFrameworkHalManifest(bool skipCache = false);

    /*
     * Return the API that access the device-side compatibility matrix stored
     * in /vendor/compatibility_matrix.xml.
     */
    std::shared_ptr<const CompatibilityMatrix> getDeviceCompatibilityMatrix(bool skipCache = false);

    /*
     * Return the API that access the framework-side compatibility matrix stored
     * in /system/compatibility_matrix.xml.
     */
    std::shared_ptr<const CompatibilityMatrix> getFrameworkCompatibilityMatrix(
        bool skipCache = false);

    /*
     * Return the API that access device runtime info.
     *
     * {skipCache == true, flags == ALL}: re-fetch everything
     * {skipCache == false, flags == ALL}: fetch everything if not previously fetched
     * {skipCache == true, flags == selected info}: re-fetch selected information
     *                                if not previously fetched.
     * {skipCache == false, flags == selected info}: fetch selected information
     *                                if not previously fetched.
     *
     * @param skipCache do not fetch if previously fetched
     * @param flags bitwise-or of RuntimeInfo::FetchFlag
     */
    std::shared_ptr<const RuntimeInfo> getRuntimeInfo(
        bool skipCache = false, RuntimeInfo::FetchFlags flags = RuntimeInfo::FetchFlag::ALL);

    /**
     * Check compatibility, given a set of manifests / matrices in packageInfo.
     * They will be checked against the manifests / matrices on the device.
     *
     * @param packageInfo a list of XMLs of HalManifest /
     * CompatibilityMatrix objects.
     * @param error error message
     * @param flags flags to disable certain checks. See CheckFlags.
     *
     * @return = 0 if success (compatible)
     *         > 0 if incompatible
     *         < 0 if any error (mount partition fails, illformed XML, etc.)
     */
    int32_t checkCompatibility(const std::vector<std::string>& packageInfo,
                               std::string* error = nullptr,
                               CheckFlags::Type flags = CheckFlags::ENABLE_ALL_CHECKS);

    /**
     * A std::function that abstracts a list of "provided" instance names. Given package, version
     * and interface, the function returns a list of instance names that matches.
     * This function can represent a manifest, an IServiceManager, etc.
     * If the source is passthrough service manager, a list of instance names cannot be provided.
     * Instead, the function should call getService on each of the "hintInstances", and
     * return those instances for which getService does not return a nullptr. This means that for
     * passthrough HALs, the deprecation on <regex-instance>s cannot be enforced; only <instance>s
     * can be enforced.
     */
    using ListInstances = std::function<std::vector<std::pair<std::string, Version>>(
        const std::string& package, Version version, const std::string& interface,
        const std::vector<std::string>& hintInstances)>;
    /**
     * Check deprecation on framework matrices with a provided predicate.
     *
     * @param listInstances predicate that takes parameter in this format:
     *        android.hardware.foo@1.0::IFoo
     *        and returns {{"default", version}...} if HAL is in use, where version =
     *        first version in interfaceChain where package + major version matches.
     *
     * @return = 0 if success (no deprecated HALs)
     *         > 0 if there is at least one deprecated HAL
     *         < 0 if any error (mount partition fails, illformed XML, etc.)
     */
    int32_t checkDeprecation(const ListInstances& listInstances, std::string* error = nullptr);

    /**
     * Check deprecation on existing VINTF metadata. Use Device Manifest as the
     * predicate to check if a HAL is in use.
     *
     * @return = 0 if success (no deprecated HALs)
     *         > 0 if there is at least one deprecated HAL
     *         < 0 if any error (mount partition fails, illformed XML, etc.)
     */
    int32_t checkDeprecation(std::string* error = nullptr);

   private:
    const std::unique_ptr<FileSystem> mFileSystem;
    const std::unique_ptr<details::PartitionMounter> mPartitionMounter;
    const std::unique_ptr<details::ObjectFactory<RuntimeInfo>> mRuntimeInfoFactory;
    const std::unique_ptr<details::PropertyFetcher> mPropertyFetcher;

    details::LockedSharedPtr<HalManifest> mDeviceManifest;
    details::LockedSharedPtr<HalManifest> mFrameworkManifest;
    details::LockedSharedPtr<CompatibilityMatrix> mDeviceMatrix;

    // Parent lock of the following fields. It should be acquired before locking the child locks.
    std::mutex mFrameworkCompatibilityMatrixMutex;
    details::LockedSharedPtr<CompatibilityMatrix> mFrameworkMatrix;
    details::LockedSharedPtr<CompatibilityMatrix> mCombinedFrameworkMatrix;
    // End of mFrameworkCompatibilityMatrixMutex

    details::LockedRuntimeInfoCache mDeviceRuntimeInfo;

    // Expose functions for testing and recovery
    friend class VintfObjectRecovery;
    friend class testing::VintfObjectTestBase;
    friend class testing::VintfObjectRuntimeInfoTest;
    friend class testing::VintfObjectCompatibleTest;
    int32_t checkCompatibility(const std::vector<std::string>& xmls, bool mount, std::string* error,
                               CheckFlags::Type flags = CheckFlags::ENABLE_ALL_CHECKS);
    const std::unique_ptr<FileSystem>& getFileSystem();
    const std::unique_ptr<details::PartitionMounter>& getPartitionMounter();
    const std::unique_ptr<details::PropertyFetcher>& getPropertyFetcher();
    const std::unique_ptr<details::ObjectFactory<RuntimeInfo>>& getRuntimeInfoFactory();

   public:
    /*
     * Get global instance. By default, this fetches from root and cache results,
     * unless skipCache is specified.
     */
    static std::shared_ptr<VintfObject> GetInstance();

    // Static variants of member functions.

    /*
     * Return the API that access the device-side HAL manifest stored
     * in /vendor/manifest.xml.
     */
    static std::shared_ptr<const HalManifest> GetDeviceHalManifest(bool skipCache = false);

    /*
     * Return the API that access the framework-side HAL manifest stored
     * in /system/manfiest.xml.
     */
    static std::shared_ptr<const HalManifest> GetFrameworkHalManifest(bool skipCache = false);

    /*
     * Return the API that access the device-side compatibility matrix stored
     * in /vendor/compatibility_matrix.xml.
     */
    static std::shared_ptr<const CompatibilityMatrix> GetDeviceCompatibilityMatrix(
        bool skipCache = false);

    /*
     * Return the API that access the framework-side compatibility matrix stored
     * in /system/compatibility_matrix.xml.
     */
    static std::shared_ptr<const CompatibilityMatrix> GetFrameworkCompatibilityMatrix(
        bool skipCache = false);

    /*
     * Return the API that access device runtime info.
     *
     * {skipCache == true, flags == ALL}: re-fetch everything
     * {skipCache == false, flags == ALL}: fetch everything if not previously fetched
     * {skipCache == true, flags == selected info}: re-fetch selected information
     *                                if not previously fetched.
     * {skipCache == false, flags == selected info}: fetch selected information
     *                                if not previously fetched.
     *
     * @param skipCache do not fetch if previously fetched
     * @param flags bitwise-or of RuntimeInfo::FetchFlag
     */
    static std::shared_ptr<const RuntimeInfo> GetRuntimeInfo(
        bool skipCache = false, RuntimeInfo::FetchFlags flags = RuntimeInfo::FetchFlag::ALL);

    /**
     * Check compatibility, given a set of manifests / matrices in packageInfo.
     * They will be checked against the manifests / matrices on the device.
     *
     * @param packageInfo a list of XMLs of HalManifest /
     * CompatibilityMatrix objects.
     * @param error error message
     * @param flags flags to disable certain checks. See CheckFlags.
     *
     * @return = 0 if success (compatible)
     *         > 0 if incompatible
     *         < 0 if any error (mount partition fails, illformed XML, etc.)
     */
    static int32_t CheckCompatibility(const std::vector<std::string>& packageInfo,
                                      std::string* error = nullptr,
                                      CheckFlags::Type flags = CheckFlags::ENABLE_ALL_CHECKS);

    /**
     * Check deprecation on framework matrices with a provided predicate.
     *
     * @param listInstances predicate that takes parameter in this format:
     *        android.hardware.foo@1.0::IFoo
     *        and returns {{"default", version}...} if HAL is in use, where version =
     *        first version in interfaceChain where package + major version matches.
     *
     * @return = 0 if success (no deprecated HALs)
     *         > 0 if there is at least one deprecated HAL
     *         < 0 if any error (mount partition fails, illformed XML, etc.)
     */
    static int32_t CheckDeprecation(const ListInstances& listInstances,
                                    std::string* error = nullptr);

    /**
     * Check deprecation on existing VINTF metadata. Use Device Manifest as the
     * predicate to check if a HAL is in use.
     *
     * @return = 0 if success (no deprecated HALs)
     *         > 0 if there is at least one deprecated HAL
     *         < 0 if any error (mount partition fails, illformed XML, etc.)
     */
    static int32_t CheckDeprecation(std::string* error = nullptr);

   private:
    static details::LockedSharedPtr<VintfObject> sInstance;

    status_t getCombinedFrameworkMatrix(const std::shared_ptr<const HalManifest>& deviceManifest,
                                        CompatibilityMatrix* out, std::string* error = nullptr);
    std::vector<Named<CompatibilityMatrix>> getAllFrameworkMatrixLevels(
        std::string* error = nullptr);
    status_t addDirectoryManifests(const std::string& directory, HalManifest* manifests,
                                   std::string* error = nullptr);
    status_t fetchDeviceHalManifest(HalManifest* out, std::string* error = nullptr);
    status_t fetchDeviceMatrix(CompatibilityMatrix* out, std::string* error = nullptr);
    status_t fetchOdmHalManifest(HalManifest* out, std::string* error = nullptr);
    status_t fetchOneHalManifest(const std::string& path, HalManifest* out,
                                 std::string* error = nullptr);
    status_t fetchFrameworkHalManifest(HalManifest* out, std::string* error = nullptr);

    static bool IsHalDeprecated(const MatrixHal& oldMatrixHal,
                                const CompatibilityMatrix& targetMatrix,
                                const ListInstances& listInstances, std::string* error);
    static bool IsInstanceDeprecated(const MatrixInstance& oldMatrixInstance,
                                     const CompatibilityMatrix& targetMatrix,
                                     const ListInstances& listInstances, std::string* error);
};

enum : int32_t {
    COMPATIBLE = 0,
    INCOMPATIBLE = 1,

    NO_DEPRECATED_HALS = 0,
    DEPRECATED = 1,
};

// exposed for testing.
namespace details {

extern const std::string kSystemVintfDir;
extern const std::string kVendorVintfDir;
extern const std::string kOdmVintfDir;
extern const std::string kOdmLegacyVintfDir;
extern const std::string kOdmLegacyManifest;
extern const std::string kVendorManifest;
extern const std::string kSystemManifest;
extern const std::string kVendorMatrix;
extern const std::string kOdmManifest;
extern const std::string kVendorManifestFragmentDir;
extern const std::string kSystemManifestFragmentDir;
extern const std::string kOdmManifestFragmentDir;
extern const std::string kVendorLegacyManifest;
extern const std::string kVendorLegacyMatrix;
extern const std::string kSystemLegacyManifest;
extern const std::string kSystemLegacyMatrix;

// Convenience function to dump all files and directories that could be read
// by calling Get(Framework|Device)(HalManifest|CompatibilityMatrix). The list
// include files that may not actually be read when the four functions are called
// because some files have a higher priority than others. The list does NOT
// include "files" (including kernel interfaces) that are read when GetRuntimeInfo
// is called.
std::vector<std::string> dumpFileList();

} // namespace details

} // namespace vintf
} // namespace android

#endif // ANDROID_VINTF_VINTF_OBJECT_H_