blob: 6ce05477b3eeabeb731db73455a9b29e3d9d3fab (
plain) (
tree)
|
|
/*
* Copyright (C) 2016 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef WIFICOND_CLIENT_INTERFACE_IMPL_H_
#define WIFICOND_CLIENT_INTERFACE_IMPL_H_
#include <string>
#include <android-base/macros.h>
#include <utils/StrongPointer.h>
#include <wifi_system/interface_tool.h>
#include <wifi_system/supplicant_manager.h>
#include "android/net/wifi/IClientInterface.h"
#include "wificond/net/mlme_event_handler.h"
#include "wificond/net/netlink_utils.h"
#include "wificond/scanning/offload/offload_service_utils.h"
#include "wificond/scanning/scanner_impl.h"
namespace android {
namespace wificond {
class ClientInterfaceBinder;
class ClientInterfaceImpl;
class ScanUtils;
class MlmeEventHandlerImpl : public MlmeEventHandler {
public:
MlmeEventHandlerImpl(ClientInterfaceImpl* client_interface);
~MlmeEventHandlerImpl() override;
void OnConnect(std::unique_ptr<MlmeConnectEvent> event) override;
void OnRoam(std::unique_ptr<MlmeRoamEvent> event) override;
void OnAssociate(std::unique_ptr<MlmeAssociateEvent> event) override;
void OnDisconnect(std::unique_ptr<MlmeDisconnectEvent> event) override;
void OnDisassociate(std::unique_ptr<MlmeDisassociateEvent> event) override;
private:
ClientInterfaceImpl* client_interface_;
};
// Holds the guts of how we control network interfaces capable of connecting to
// access points via wpa_supplicant.
//
// Because remote processes may hold on to the corresponding
// binder object past the lifetime of the local object, we are forced to
// keep this object separate from the binder representation of itself.
class ClientInterfaceImpl {
public:
ClientInterfaceImpl(
uint32_t wiphy_index,
const std::string& interface_name,
uint32_t interface_index,
const std::vector<uint8_t>& interface_mac_addr,
android::wifi_system::InterfaceTool* if_tool,
android::wifi_system::SupplicantManager* supplicant_manager,
NetlinkUtils* netlink_utils,
ScanUtils* scan_utils);
virtual ~ClientInterfaceImpl();
// Get a pointer to the binder representing this ClientInterfaceImpl.
android::sp<android::net::wifi::IClientInterface> GetBinder() const;
bool EnableSupplicant();
bool DisableSupplicant();
bool GetPacketCounters(std::vector<int32_t>* out_packet_counters);
bool SignalPoll(std::vector<int32_t>* out_signal_poll_results);
const std::vector<uint8_t>& GetMacAddress();
const std::string& GetInterfaceName() const { return interface_name_; }
const android::sp<ScannerImpl> GetScanner() { return scanner_; };
bool requestANQP(
const ::std::vector<uint8_t>& bssid,
const ::android::sp<::android::net::wifi::IANQPDoneCallback>& callback);
virtual bool IsAssociated() const;
void Dump(std::stringstream* ss) const;
private:
bool RefreshAssociateFreq();
const uint32_t wiphy_index_;
const std::string interface_name_;
const uint32_t interface_index_;
const std::vector<uint8_t> interface_mac_addr_;
android::wifi_system::InterfaceTool* const if_tool_;
android::wifi_system::SupplicantManager* const supplicant_manager_;
NetlinkUtils* const netlink_utils_;
ScanUtils* const scan_utils_;
const std::shared_ptr<OffloadServiceUtils> offload_service_utils_;
const std::unique_ptr<MlmeEventHandlerImpl> mlme_event_handler_;
const android::sp<ClientInterfaceBinder> binder_;
android::sp<ScannerImpl> scanner_;
// Cached information for this connection.
bool is_associated_;
std::vector<uint8_t> bssid_;
uint32_t associate_freq_;
// Capability information for this wiphy/interface.
BandInfo band_info_;
ScanCapabilities scan_capabilities_;
WiphyFeatures wiphy_features_;
DISALLOW_COPY_AND_ASSIGN(ClientInterfaceImpl);
friend class MlmeEventHandlerImpl;
};
} // namespace wificond
} // namespace android
#endif // WIFICOND_CLIENT_INTERFACE_IMPL_H_
|