/* * Copyright (C) 2016 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #ifndef WIFICOND_AP_INTERFACE_IMPL_H_ #define WIFICOND_AP_INTERFACE_IMPL_H_ #include #include #include #include #include #include "wificond/net/netlink_manager.h" #include "android/net/wifi/IApInterface.h" namespace android { namespace wificond { class ApInterfaceBinder; class NetlinkUtils; // Holds the guts of how we control network interfaces capable of exposing an AP // via hostapd. Because remote processes may hold on to the corresponding // binder object past the lifetime of the local object, we are forced to // keep this object separate from the binder representation of itself. class ApInterfaceImpl { public: ApInterfaceImpl(const std::string& interface_name, uint32_t interface_index, NetlinkUtils* netlink_utils, wifi_system::InterfaceTool* if_tool, wifi_system::HostapdManager* hostapd_manager); ~ApInterfaceImpl(); // Get a pointer to the binder representing this ApInterfaceImpl. android::sp GetBinder() const; bool StartHostapd(); bool StopHostapd(); bool WriteHostapdConfig( const std::vector& ssid, bool is_hidden, int32_t channel, wifi_system::HostapdManager::EncryptionType encryption_type, const std::vector& passphrase); std::string GetInterfaceName() { return interface_name_; } int GetNumberOfAssociatedStations() const; void Dump(std::stringstream* ss) const; private: const std::string interface_name_; const uint32_t interface_index_; NetlinkUtils* const netlink_utils_; wifi_system::InterfaceTool* const if_tool_; wifi_system::HostapdManager* const hostapd_manager_; const android::sp binder_; // Number of associated stations. int number_of_associated_stations_; void OnStationEvent(StationEvent event, const std::vector& mac_address); DISALLOW_COPY_AND_ASSIGN(ApInterfaceImpl); }; } // namespace wificond } // namespace android #endif // WIFICOND_AP_INTERFACE_IMPL_H_