1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
|
/*
* Copyright (C) 2016 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#include "wificond/looper_backed_event_loop.h"
#include <android-base/logging.h>
#include <utils/Looper.h>
#include <utils/Timers.h>
namespace {
class EventLoopCallback : public android::MessageHandler {
public:
explicit EventLoopCallback(const std::function<void()>& callback)
: callback_(callback) {
}
~EventLoopCallback() override = default;
virtual void handleMessage(const android::Message& message) {
callback_();
}
private:
const std::function<void()> callback_;
DISALLOW_COPY_AND_ASSIGN(EventLoopCallback);
};
class WatchFdCallback : public android::LooperCallback {
public:
explicit WatchFdCallback(const std::function<void(int)>& callback)
: callback_(callback) {
}
~WatchFdCallback() override = default;
virtual int handleEvent(int fd, int events, void* data) {
callback_(fd);
// Returning 1 means Looper keeps watching this file descriptor after
// callback is called.
// See Looper.h for details.
return 1;
}
private:
const std::function<void(int)> callback_;
DISALLOW_COPY_AND_ASSIGN(WatchFdCallback);
};
} // namespace
namespace android {
namespace wificond {
LooperBackedEventLoop::LooperBackedEventLoop()
: should_continue_(true) {
looper_ = android::Looper::prepare(Looper::PREPARE_ALLOW_NON_CALLBACKS);
}
LooperBackedEventLoop::~LooperBackedEventLoop() {
}
void LooperBackedEventLoop::PostTask(const std::function<void()>& callback) {
sp<android::MessageHandler> event_loop_callback =
new EventLoopCallback(callback);
looper_->sendMessage(event_loop_callback, NULL);
}
void LooperBackedEventLoop::PostDelayedTask(
const std::function<void()>& callback,
int64_t delay_ms) {
sp<android::MessageHandler> looper_callback = new EventLoopCallback(callback);
looper_->sendMessageDelayed(ms2ns(delay_ms), looper_callback, NULL);
}
bool LooperBackedEventLoop::WatchFileDescriptor(
int fd,
ReadyMode mode,
const std::function<void(int)>& callback) {
sp<android::LooperCallback> watch_fd_callback = new WatchFdCallback(callback);
int event;
if (mode == kModeInput) {
event = Looper::EVENT_INPUT;
} else if (mode == kModeOutput) {
event = Looper::EVENT_OUTPUT;
} else {
LOG(ERROR) << "Invalid mode for WatchFileDescriptor().";
return false;
}
// addFd() returns 1 if descriptor was added, 0 if arguments were invalid.
// Since we are using non-NULL callback, the second parameter 'ident' will
// always be ignored. It is OK to use 0 for 'ident'.
// See Looper.h for more details.
if (looper_->addFd(fd, 0, event, watch_fd_callback, NULL) == 0) {
LOG(ERROR) << "Invalid arguments for Looper::addFd().";
return false;
}
return true;
}
bool LooperBackedEventLoop::StopWatchFileDescriptor(int fd) {
if (looper_->removeFd(fd) == 1) {
return true;
}
return false;
}
void LooperBackedEventLoop::Poll() {
while (should_continue_) {
looper_->pollOnce(-1);
}
}
void LooperBackedEventLoop::PollForOne(int timeout_millis) {
looper_->pollOnce(timeout_millis);
}
void LooperBackedEventLoop::TriggerExit() {
PostTask([this](){ should_continue_ = false; });
}
} // namespace wificond
} // namespace android
|