aboutsummaryrefslogtreecommitdiffstats
path: root/build
Commit message (Collapse)AuthorAgeFilesLines
* Using a python script to build sepolicyBowgo Tsai2018-02-053-0/+223
| | | | | | | | | | | | | Current sepolicy CIL files are built by several command-line tools in Android.mk. This change extracts some of the build logic into a python script to relief the effort in Android.mk. The first command is `build_sepolicy build_cil`. It's possible to add more sub-commands under the build_sepolicy script in the future. Bug: 64240127 Test: build bullhead/taimen Change-Id: Ie0ae4fc5256a550c72954cde5d5dd213a22d159a
* Revert "Using a python script to build sepolicy"Bowgo Tsai2018-02-013-223/+0
| | | | | | | | This reverts commit 3506ad3f310d46ace11ecb9f1a0b6d8abc4951c4. Fix angler/bullhead boot failure. Bug: 72787689 Test: build
* Using a python script to build sepolicyBowgo Tsai2018-01-313-0/+223
Current sepolicy CIL files are built by several command-line tools in Android.mk. This change extracts some of the build logic into a python script to relief the effort in Android.mk. The first command is `build_sepolicy build_cil`. It's possible to add more sub-commands under the build_sepolicy script in the future. Bug: 64240127 Test: build and boot a device Test: checks the content of $OUT/vendor/etc/selinux/vendor_sepolicy.cil is the same as before Change-Id: I0b64f1088f413172e97b579b4f7799fa392762df