With this approach, we don't need the UBL any more on DaVinci boards.
A "make boardname" will compile a u-boot.ubl, with UBL Header, which is
needed for the RBL to find the "UBL", which actually is a UBL-compatible
header, nand spl code and u-boot code.
As the RBL uses another read function as the "standard" u-boot,
we need a command, which switches between this two read/write
functions, so we can write the UBL header and the spl
code in a format, which the RBL can read. This is realize
(at the moment in board specific code) in the u-boot command
nandrbl
nandrbl without arguments returns actual mode (rbl or uboot).
with nandrbl mode (mode = "rbl" or "uboot") you can switch
between the two NAND read/write modes.
To set up mkimage you need a config file for mkimage, example:
board/ait/cam_enc_4xx/ublimage.cfg
For information about the configuration please see:
doc/README.ublimage
Example for the cam_enc_4xx board:
On the cam_enc_4xx board we have a NAND flash with blocksize = 0x20000 and
pagesize = 0x800, so the u-boot.ubl image (which you get with:
"make cam_enc_4xx") looks like this:
00000000 00 ed ac a1 20 00 00 00 06 00 00 00 05 00 00 00 |.... ...........|
00000010 00 00 00 00 20 00 00 00 ff ff ff ff ff ff ff ff |.... ...........|
00000020 ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff |................|
*
00000800 14 00 00 ea 14 f0 9f e5 10 f0 9f e5 0c f0 9f e5 |................|
00000810 08 f0 9f e5 04 f0 9f e5 00 f0 9f e5 04 f0 1f e5 |................|
00000820 00 01 00 00 78 56 34 12 78 56 34 12 78 56 34 12 |....xV4.xV4.xV4.|
[...]
*
00001fe0 00 00 00 00 00 00 00 00 ff ff ff ff ff ff ff ff |................|
00001ff0 ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff |................|
*
00003800 14 00 00 ea 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 |................|
00003810 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 |................|
00003820 80 01 08 81 e0 01 08 81 40 02 08 81 a0 02 08 81 |........@.......|
In the first "page" of the image, we have the UBL Header, needed for
the RBL to find the spl code.
The spl code starts in the second "page" of the image, with a size
defined by:
#define CONFIG_SYS_NROF_PAGES_NAND_SPL 6
After the spl code, there comes the "real" u-boot code
@ (6 + 1) * pagesize = 0x3800
------------------------------------------------------------------------
Setting up spl code:
/*
* RBL searches from Block n (n = 1..24)
* so we can define, how many UBL Headers
* we write before the real spl code
*/
#define CONFIG_SYS_NROF_UBL_HEADER 5
#define CONFIG_SYS_NROF_PAGES_NAND_SPL 6
#define CONFIG_SYS_NAND_U_BOOT_OFFS ((CONFIG_SYS_NROF_UBL_HEADER * \
CONFIG_SYS_NAND_BLOCK_SIZE) + \
(CONFIG_SYS_NROF_PAGES_NAND_SPL) * \
CONFIG_SYS_NAND_PAGE_SIZE)
------------------------------------------------------------------------
Burning into NAND:
step 1:
The RBL searches from Block n ( n = 1..24) on page 0 for valid UBL
Headers, so you have to burn the UBL header page from the u-boot.ubl
image to the blocks, you want to have the UBL header.
!! Don;t forget to switch to rbl nand read/write functions with
"nandrbl rbl"
step 2:
You need to setup in the ublimage.cfg, where the RBL can find the spl
code, and how big it is.
!! RBL always starts reading from page 0 !!
For the AIT board, we have:
PAGES 6
START_BLOCK 5
So we need to copy the spl code to block 5 page 0
!! Don;t forget to switch to rbl nand read/write functions with
"nandrbl rbl"
step 3:
You need to copy the u-boot image to the block/page
where the spl code reads it (CONFIG_SYS_NAND_U_BOOT_OFFS)
!! Don;t forget to switch to rbl nand read/write functions with
"nandrbl uboot", which is default.
On the cam_enc_4xx board it is:
#define CONFIG_SYS_NAND_U_BOOT_OFFS (0xc0000)
-> this results in following NAND usage on the cam_enc_4xx board:
addr
20000 possible UBL Header
40000 possible UBL Header
60000 possible UBL Header
80000 possilbe UBL Header
a0000 spl code
c0000 u-boot code
The above steps are executeed through the following environment vars:
(using 80000 as address for the UBL header)
pagesz=800
uboot=/tftpboot/cam_enc_4xx/u-boot.ubl
load=tftp 80000000 ${uboot}
writeheader nandrbl rbl;nand erase 80000 ${pagesz};nand write 80000000 80000 ${pagesz};nandrbl uboot
writenand_spl nandrbl rbl;nand erase a0000 3000;nand write 80000800 a0000 3000;nandrbl uboot
writeuboot nandrbl uboot;nand erase c0000 5d000;nand write 80003800 c0000 5d000
update=run load writeheader writenand_spl writeuboot
If you do a "run load update" u-boot, spl + ubl header
are magically updated ;-)
Note:
- There seem to be a bug in the RBL code (at least on my HW),
In the UBL block, I can set the page to values != 0, so it
is possible to burn step 1 and step 2 in one step into the
flash, but the RBL ignores the page settings, so I have to
burn the UBL Header to a page 0 and the spl code to
a page 0 ... :-(
- If we make the nand read/write functions in the RBL equal to
the functions in u-boot (as I have no RBL code, it is only
possible in u-boot), we could burn the complete image in
one step ... that would be nice ...