aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorMasahiro Yamada2014-07-16 03:49:44 -0500
committerTom Rini2014-07-22 06:44:27 -0500
commit8b90a11f7cf1d06812bc9a02e0bae20cfe40a564 (patch)
tree2566189ecebf6d98ed646518285a4f55c984e923 /.mailmap
parent3f9eb6e1095b791867975c236bd7ab8b0a51acf4 (diff)
downloadu-boot-8b90a11f7cf1d06812bc9a02e0bae20cfe40a564.tar.gz
u-boot-8b90a11f7cf1d06812bc9a02e0bae20cfe40a564.tar.xz
u-boot-8b90a11f7cf1d06812bc9a02e0bae20cfe40a564.zip
add .mailmap for proper git-shortlog output
This is the first version of .mailmap created by hand. Please see "man git-shortlog" for what this commit is trying to do. Without this file, for example, "git shortlog -n -s" shows as follows: 2693 Wolfgang Denk <------ 1002 Stefan Roese <------ 811 wdenk <------ 808 Mike Frysinger 806 Simon Glass [snip] 177 Matthias Fuchs 154 stroese <------ 153 Timur Tabi And then, with this file, it shows as follows: 3504 Wolfgang Denk <------ 1156 Stefan Roese <------ 808 Mike Frysinger 806 Simon Glass Signed-off-by: Masahiro Yamada <yamada.m@jp.panasonic.com> Cc: Stefan Roese <sr@denx.de> Cc: Wolfgang Denk <wd@denx.de>
Diffstat (limited to '.mailmap')
-rw-r--r--.mailmap12
1 files changed, 12 insertions, 0 deletions
diff --git a/.mailmap b/.mailmap
new file mode 100644
index 0000000000..9368e2d33e
--- /dev/null
+++ b/.mailmap
@@ -0,0 +1,12 @@
1#
2# This list is used by git-shortlog to fix a few botched name translations
3# in the git archive, either because the author's full name was messed up
4# and/or not always written the same way, making contributions from the
5# same person appearing not to be so or badly displayed.
6#
7# This file can be modified by hand or updated by the following command:
8# scripts/mailmapper > tmp; mv tmp .mailmap
9#
10
11Stefan Roese <stroese>
12Wolfgang Denk <wdenk>