aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorBin Meng2018-10-24 08:36:28 -0500
committerSimon Glass2018-11-14 11:16:28 -0600
commit4854ebc57e88f371963b5fa12587a3dd5e116e79 (patch)
treec8cbf6c6d7522c30f6877e5276826ed3e5e7932b
parent6f57c34473d37b8da5e6a3764d0d377d748aeef1 (diff)
downloadu-boot-4854ebc57e88f371963b5fa12587a3dd5e116e79.tar.gz
u-boot-4854ebc57e88f371963b5fa12587a3dd5e116e79.tar.xz
u-boot-4854ebc57e88f371963b5fa12587a3dd5e116e79.zip
arm: stm32mp: Remove DM_FLAG_PRE_RELOC flag
When a driver declares DM_FLAG_PRE_RELOC flag, it wishes to be bound before relocation. However due to a bug in the DM core, the flag only takes effect when devices are statically declared via U_BOOT_DEVICE(). This bug has been fixed recently by commit "dm: core: Respect drivers with the DM_FLAG_PRE_RELOC flag in lists_bind_fdt()", but with the fix, it has a side effect that all existing drivers that declared DM_FLAG_PRE_RELOC flag will be bound before relocation now. This may expose potential boot failure on some boards due to insufficient memory during the pre-relocation stage. To mitigate this potential impact, the following changes are implemented: - Remove DM_FLAG_PRE_RELOC flag in the driver, if the driver only supports configuration from device tree (OF_CONTROL) - Keep DM_FLAG_PRE_RELOC flag in the driver only if the device is statically declared via U_BOOT_DEVICE() - Surround DM_FLAG_PRE_RELOC flag with OF_CONTROL check, for drivers that support both statically declared devices and configuration from device tree Signed-off-by: Bin Meng <bmeng.cn@gmail.com> Reviewed-by: Simon Glass <sjg@chromium.org> Reviewed-by: Patrick Delaunay <patrick.delaunay@st.com>
-rw-r--r--arch/arm/mach-stm32mp/bsec.c1
1 files changed, 0 insertions, 1 deletions
diff --git a/arch/arm/mach-stm32mp/bsec.c b/arch/arm/mach-stm32mp/bsec.c
index 0e152efc04..d087a31389 100644
--- a/arch/arm/mach-stm32mp/bsec.c
+++ b/arch/arm/mach-stm32mp/bsec.c
@@ -417,7 +417,6 @@ U_BOOT_DRIVER(stm32mp_bsec) = {
417 .ofdata_to_platdata = stm32mp_bsec_ofdata_to_platdata, 417 .ofdata_to_platdata = stm32mp_bsec_ofdata_to_platdata,
418 .platdata_auto_alloc_size = sizeof(struct stm32mp_bsec_platdata), 418 .platdata_auto_alloc_size = sizeof(struct stm32mp_bsec_platdata),
419 .ops = &stm32mp_bsec_ops, 419 .ops = &stm32mp_bsec_ops,
420 .flags = DM_FLAG_PRE_RELOC,
421}; 420};
422 421
423/* bsec IP is not present in device tee, manage IP address by platdata */ 422/* bsec IP is not present in device tee, manage IP address by platdata */