diff options
author | Miquel Raynal | 2018-09-29 05:58:30 -0500 |
---|---|---|
committer | Jagan Teki | 2018-10-02 11:42:32 -0500 |
commit | 938db6fe5da3581ed2c17d64c7e016a7a8df5237 (patch) | |
tree | 59c94bddc4e864b80544cce6bb950aacde368e43 /cmd | |
parent | c58fb2cdb3e4abb8c2714b351b3856661573c747 (diff) | |
download | u-boot-938db6fe5da3581ed2c17d64c7e016a7a8df5237.tar.gz u-boot-938db6fe5da3581ed2c17d64c7e016a7a8df5237.tar.xz u-boot-938db6fe5da3581ed2c17d64c7e016a7a8df5237.zip |
cmd: mtdparts: describe as legacy
The 'mtdparts' command is not needed anymore. While the environment
variable is still valid (and useful, along with the 'mtdids' one), the
command has been replaced by 'mtd' which is much more close to the MTD
stack and do not add its own specific glue.
Signed-off-by: Miquel Raynal <miquel.raynal@bootlin.com>
Reviewed-by: Stefan Roese <sr@denx.de>
Reviewed-by: Boris Brezillon <boris.brezillon@bootlin.com>
Diffstat (limited to 'cmd')
-rw-r--r-- | cmd/Kconfig | 6 |
1 files changed, 5 insertions, 1 deletions
diff --git a/cmd/Kconfig b/cmd/Kconfig index b571e84cc1..12d19fd675 100644 --- a/cmd/Kconfig +++ b/cmd/Kconfig | |||
@@ -1699,7 +1699,11 @@ config CMD_MTDPARTS | |||
1699 | bool "MTD partition support" | 1699 | bool "MTD partition support" |
1700 | select MTD_DEVICE if (CMD_NAND || NAND) | 1700 | select MTD_DEVICE if (CMD_NAND || NAND) |
1701 | help | 1701 | help |
1702 | MTD partition support | 1702 | MTD partitioning tool support. |
1703 | It is strongly encouraged to avoid using this command | ||
1704 | anymore along with 'sf', 'nand', 'onenand'. One can still | ||
1705 | declare the partitions in the mtdparts environment variable | ||
1706 | but better use the MTD stack and the 'mtd' command instead. | ||
1703 | 1707 | ||
1704 | config MTDIDS_DEFAULT | 1708 | config MTDIDS_DEFAULT |
1705 | string "Default MTD IDs" | 1709 | string "Default MTD IDs" |