diff options
author | Petr Vorel | 2018-03-23 19:49:23 -0500 |
---|---|---|
committer | Heiko Schocher | 2018-03-24 00:37:10 -0500 |
commit | afb6fda2ae0b04f806a55fc5882df49a8eab572d (patch) | |
tree | bb1529056b10f19e4a016cfc170acf7695ac6390 /env | |
parent | e9951281585060a7ba9d9826e286ff3e7ed067bb (diff) | |
download | u-boot-afb6fda2ae0b04f806a55fc5882df49a8eab572d.tar.gz u-boot-afb6fda2ae0b04f806a55fc5882df49a8eab572d.tar.xz u-boot-afb6fda2ae0b04f806a55fc5882df49a8eab572d.zip |
Convert CONFIG_UBIFS_SILENCE_MSG to Kconfig
Introduce another difference from upstream (kernel) source in
fs/ubifs/super.c: adding preprocessor condition as y variable in
mount_ubifs() depends on CONFIG_UBIFS_SILENCE_MSG:
fs/ubifs/super.c:1337:15: error: variable ?y? set but not used [-Werror=unused-but-set-variable]
long long x, y;
Not setting CONFIG_UBIFS_SILENCE_MSG in am335x_igep003x_defconfig and
igep0032_defconfig. Although it was defined in their config headers, it
depends on CMD_UBIFS which is not set for them.
Signed-off-by: Petr Vorel <petr.vorel@gmail.com>
Cc: Joe Hershberger <joe.hershberger@ni.com>
Cc: Heiko Schocher <hs@denx.de>
Diffstat (limited to 'env')
-rw-r--r-- | env/Kconfig | 1 |
1 files changed, 0 insertions, 1 deletions
diff --git a/env/Kconfig b/env/Kconfig index a3c6298273..36d6e799fc 100644 --- a/env/Kconfig +++ b/env/Kconfig | |||
@@ -361,7 +361,6 @@ config ENV_IS_IN_UBI | |||
361 | It is assumed that both volumes are in the same MTD partition. | 361 | It is assumed that both volumes are in the same MTD partition. |
362 | 362 | ||
363 | - CONFIG_UBI_SILENCE_MSG | 363 | - CONFIG_UBI_SILENCE_MSG |
364 | - CONFIG_UBIFS_SILENCE_MSG | ||
365 | 364 | ||
366 | You will probably want to define these to avoid a really noisy system | 365 | You will probably want to define these to avoid a really noisy system |
367 | when storing the env in UBI. | 366 | when storing the env in UBI. |